Beacon

This section presents the user interactions and testing methods for the Beacon application.

Advertising data

The beacons are non-connectable advertising packets that are sent on the three advertising channels. The latter contains the following fields.

  • Company Identifier (2 bytes): 0x0025 (NXP ID as defined by the Bluetooth SIG).

  • Beacon Identifier (1 byte): 0xBC (Allows identifying an NXP Beacon alongside with Company Identifier).

  • UUID (16 bytes): Beacon sensor unique identifier.

  • A (2 bytes): Beacon application data.

  • B (2 bytes): Beacon application data.

  • C (2 bytes): Beacon application data.

  • RSSI at 1m (1 byte): Allows distance-based applications.

By default, the UUID value is a random value based on the unique identifier of the board.

Supported Boards

The Beacon application is supported on the following platform:

  • KW45B41Z-EVK

  • K32W148-EVK

  • FRDM-MCXW71

  • KW47-EVK

  • MCX-W72-EVK