Bluetooth LE FSCI Black Box

This section describes the functionality, user interactions, and testing methods for the Bluetooth LE FSCI Black Box demo application.

Demo functionality overview

The Bluetooth LE FSCI Black Box demo application gives access to the Bluetooth LE Host Stack via a serial interface using the FSCI protocol. See the FSCI (Framework Serial Communication Interface) manual for the format of the FSCI commands and a full list of supported commands.

The demo can be used with the Test Tool for Connectivity Products. Command Console application can be downloaded from the NXP website or using a custom application that supports the FSCI protocol and commands.

Supported Boards

The Bluetooth LE FSCI Black Box application is supported on the following platform:

  • KW45B41Z-EVK

  • K32W148-EVK

  • FRDM-MCXW71

  • KW47-EVK

  • MCX-W72-EVK