Low-power temperature sensor

This section describes the implemented profiles and services, user interactions, and testing methods for the temperature sensor application.

Implemented profiles and services

The Temperature Sensor application implements a GATT server, a custom profile and the following services.

  • Temperature Service (UUID: 01ff0200-ba5e-f4ee-5ca1-eb1e5e4b1ce0)

  • Battery Service v1.0

  • Device Information Service v1.1

The application behaves as a GAP peripheral node. It enters GAP General Discoverable Mode and waits for a GAP central node to connect and configure notifications for the temperature value.

The Temperature service is a custom service that implements the Temperature characteristic (UUID: 0x2A6E) with a Characteristic Presentation Format descriptor (UUID: 0x2904), both defined by the Bluetooth SIG.

The application uses pairing with bonding by default. When connected with the Low-Power Temperature Sensor application, the collector sends the 999999 passcode to the host stack by default.

Supported Boards

The Temperature Sensor application is supported by the following platforms:

  • KW45B41Z-EVK

  • K32W148-EVK

  • FRDM-MCXW71

  • KW47-EVK

  • MCX-W72-EVK