MCUXpresso SDK Documentation

pf5020

pf5020#

Overview#

The pf5020 driver example demonstrates the usage of pf5020 SDK component driver. The example shows the usage of pf5020 API to:

  1. Set regulator output voltages;

  2. Set Internal high speed clock;

  3. Set PF5020 to standby mode;

  4. Dump PF5020 register content.

To use this example, user need to pay attention the output voltage when update the regulator output and make sure the output voltage to set will not cause hardware damage.

Supported Boards#