MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-IMXRT1152 board

  • Personal Computer

  • RK055MHD091 panel or RK055AHD091 panel or RK055IQH091 panel or Raspberry Pi 7 inch panel

Board settings#

Connect the panel to J62. For Raspberry Pi 7 inch panel, connect the panel to J58, then connect the panel’s 5V pin to J56-1, GND pin to J56-2.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, the project uses Raspberry Pi 7 inch panel by default, to use other panels, change #define USE_MIPI_PANEL MIPI_PANEL_RASPI_7INCH to #define USE_MIPI_PANEL MIPI_PANEL_RK055IQH091 or #define USE_MIPI_PANEL MIPI_PANEL_RK055AHD091 or #define USE_MIPI_PANEL MIPI_PANEL_RK055MHD091 in lcdifv2_support.h.

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the example runs, the screen shows what described in overview.