Hardware requirements#
Type-C USB cable
MIMXRT2660-EVK board
Personal computer
Board settings#
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Note#
IAR EWARM cannot debug the RT2660 directly. Use SEGGER Ozone to download and debug the IAR-built image instead.