mc_pmsm_enc#
Overview#
This example demonstrates the control of the PMSM.
Supported Boards#
FRDM-MCXE32B
Hardware requirements
FRDMMCXE32B board
FRDM-MC-LVPMSM board
Power supply 24V
Mini/micro USB cable
Low-voltage 3-phase permanent magnet motor
Personal Computer
Overview
The 3-phase permanent magnet synchronous motor (PMSM) control reference application is intended to provide the example for 3-phase PMSM motor control solutions. The reference design uses a closed-loop field-oriented vector speed (FOC) control mechanism.
More information
Application web page with the board specific Application User’s guide and other documentation: http://www.nxp.com/sdkmotorcontrol
Board settings
Follow chapter “Hardware setup” in Application User’s guide.
In this example, the LCU is used as a PWM output, therefore some additional wiring is required. Please connect the FRDM-MC-LVPMSM to the FRDM-MCXE32B, and then connect the LCU outputs on J8 to the Freedom board using wires.
FRDM-MC-LVPMSM FRDM-MCXE32B J3-15 (PWM_AT) with J8-9 (PTB1) J3-13 (PWM_AB) with J8-11 (PTB0) J3-11 (PWM_BT) with J8-6 (PTC9) J3-9 (PWM_BB) with J8-8 (PTC8) J3-7 (PWM_CT) with J8-10 (PTC11) J3-5 (PWM_CB) with J8-12 (PTC10)
Running the demo
Follow chapter “User interface” in Application User’s guide.
FRDM-MCXN947T
Hardware requirements
FRDMMCXN947T board
FRDM-MC-LVPMSM board
Power supply 24V
Mini/micro USB cable
Low-voltage 3-phase permanent magnet motor
Personal Computer
Overview
The 3-phase permanent magnet synchronous motor (PMSM) control reference application is intended to provide the example for 3-phase PMSM motor control solutions. The reference design uses a closed-loop field-oriented vector speed (FOC) control mechanism.
More information
Application web page with the board specific Application User’s guide and other documentation: http://www.nxp.com/sdkmotorcontrol
Board settings
Follow chapter “Hardware setup” in Application User’s guide.
Running the demo
Follow chapter “User interface” in Application User’s guide.
FRDM-IMXRT1152
Hardware requirements
MIMXRT1150-EVK board
FRDM-MC-LVPMSM board
Power supply 24V
Type-C USB cable
Low-voltage 3-phase permanent magnet motor
Personal Computer
Overview
The 3-phase permanent magnet synchronous motor (PMSM) control reference application is intended to provide the example for 3-phase PMSM motor control solutions. The reference design uses a closed-loop field-oriented vector speed (FOC) control mechanism.
More information
Application web page with the board specific Application User’s guide and other documentation: http://www.nxp.com/sdkmotorcontrol
Board settings
Follow chapter “Hardware setup” in Application User’s guide.
Running the demo
Follow chapter “User interface” in Application User’s guide.
HVP-MCXA346
Hardware requirements
HVP-MCXA346 controller card
HVP-MC3PH high-voltage development platform
Power supply 240V
Type-C USB cable
High-voltage 3-phase permanent magnet motor
Personal Computer
Overview
The 3-phase permanent magnet synchronous motor (PMSM) control reference application is intended to provide the example for 3-phase PMSM motor control solutions. The reference design uses a closed-loop field-oriented vector speed (FOC) control mechanism.
More information
Application web page with the board specific Application User’s guide and other documentation: http://www.nxp.com/sdkmotorcontrol
Board settings
Follow chapter “Hardware setup” in Application User’s guide.
Running the demo
Follow chapter “User interface” in Application User’s guide.
MIMXRT2660-EVK
Hardware requirements
MIMXRT2660-EVK board
FRDM-MC-LVPMSM board
Power supply 24V
Mini/micro USB cable
Low-voltage 3-phase permanent magnet motor
Personal Computer
Overview
The 3-phase permanent magnet synchronous motor (PMSM) control reference application is intended to provide the example for 3-phase PMSM motor control solutions. The reference design uses a closed-loop field-oriented vector speed (FOC) control mechanism.
More information
Application web page with the board specific Application User’s guide and other documentation: http://www.nxp.com/sdkmotorcontrol
Board settings
Follow chapter “Hardware setup” in Application User’s guide.
Running the demo
Follow chapter “User interface” in Application User’s guide.
Notice
This example has not been tested on the target hardware. Only build testing was completed.