MCUXpresso SDK Documentation

enet_qos_txrx_multiring_transfer

enet_qos_txrx_multiring_transfer#

Overview#

The example shows the way to use ENET QOS driver to
receive and transmit frames supported multi-ring platforms. this example is only supported in multi-ring platform.

  1. This example shows how to initialize the ENET MAC.

  2. How to use ENET MAC to transmit frames in avb supported multiple-ring platforms.

The example transmits 20 number frames. For simple demo, we create frames with some special definition.

  1. Build transmission frames with broadcast mac address.

  2. Build frames with unicast mac address

  3. Send broadcast frames to ring 0 and unitcase frames to ring 1, then receive them back in associated rings.

Supported Boards#

MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • Loopback network cable RJ45 standard

  • EVK-MIMXRT1170 board

  • Personal Computer

Board settings

If Rx frame CRC error occurs, try to populate a suitable C66. The REV C/C1 boards populate 22pF which is high and may result in CRC errors on some of boards, if this is the case C66 may be removed or replaced by a smaller capacitor.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable to Ethernet RJ45 port(J4).

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Make loopback cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white

Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET multi-ring txrx example start.

30 frames will be sent in 3 queues, and frames will be received in queues. The frame transmitted from the ring 0, 1, 2 is 10, 10, 10! 30 frames transmitted succeed! The frames successfully received from the ring 0, 1, 2 is 10, 10, 10!

FRDM-IMXRT1152
Hardware requirements
  • Type-C USB cable

  • Loopback network cable RJ45 standard

  • FRDM-IMXRT1152 board

  • Personal Computer

Board settings
  • Use the 10/100 Ethernet RJ45 port (J55).

  • Set JP2 to position 1-2.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable to the 10/100 Ethernet RJ45 port (J55).

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Make loopback cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white

Connect J1 => J3, J2 => J6. 10/100M transfer only requires J1, J2, J3, and J6. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET multi-ring txrx example start.

30 frames will be sent in 3 queues, and frames will be received in queues. The frame transmitted from the ring 0, 1, 2 is 10, 10, 10! 30 frames transmitted succeed! The frames successfully received from the ring 0, 1, 2 is 10, 10, 10!

EVK-MIMX8MP
Hardware requirements
  • Micro USB cable

  • EVK-MIMX8M Plus board

  • J-Link Debug Probe

  • 12V power supply

  • Personal Computer

Board settings

Example uses phy looback. No need to connect any network cable on port.

Please note this application can’t support running with Linux BSP! This example aims to show the basic usage of the IP’s function, some of the used Pads/Resources are also used by Cortex-A core.

Prepare the Demo
  1. Connect 12V power supply and J-Link Debug Probe to the board.

  2. Connect a micro USB cable between the host PC and the J19 USB Debug Port on the CPU board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET multi-ring txrx example start.

30 frames will be sent in 3 queues, and frames will be received in 3 queues. The frame transmitted from the ring 0, 1, 2 is 10, 10, 10! 30 frames transmitted succeed! The frames successfully received from the ring 0, 1, 2 is 10, 10, 10!

MCIMX93-EVK
Hardware requirements
  • USB Type-C cable

  • Loopback network cable RJ45 standard

  • MCIMX93-EVK board

  • Personal Computer

Board settings

No special settings are required.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable to Ethernet RJ45 port(J501).

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Make loopback cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white

Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET multi-ring txrx example start.

30 frames will be sent in 3 queues, and frames will be received in queues. The frame transmitted from the ring 0, 1, 2 is 10, 10, 10! 30 frames transmitted succeed! The frames successfully received from the ring 0, 1, 2 is 10, 10, 10!

MCIMX93W-EVK
Hardware requirements
  • USB Type-C cable

  • Loopback network cable RJ45 standard

  • MCIMX93W-EVK board

  • Personal Computer

Board settings

No special settings are required.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable to Ethernet RJ45 port(J501).

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Make loopback cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white

Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET multi-ring txrx example start.

30 frames will be sent in 3 queues, and frames will be received in queues. The frame transmitted from the ring 0, 1, 2 is 10, 10, 10! 30 frames transmitted succeed! The frames successfully received from the ring 0, 1, 2 is 10, 10, 10!

MCIMX93-QSB
Hardware requirements
  • USB Type-C cable

  • Loopback network cable RJ45 standard

  • MCIMX93-QSB board

  • Personal Computer

Board settings

No special settings are required.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable to Ethernet RJ45 port(J501).

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Make loopback cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white

Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET multi-ring txrx example start.

30 frames will be sent in 3 queues, and frames will be received in queues. The frame transmitted from the ring 0, 1, 2 is 10, 10, 10! 30 frames transmitted succeed! The frames successfully received from the ring 0, 1, 2 is 10, 10, 10!

FRDM-MCXE31B
Hardware requirements
  • Type-C USB cable

  • Loopback network cable RJ45 standard

  • FRDM-MCXE31B board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable to Ethernet RJ45 port (J16).

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Make loopback cable:

    568B standard 	Unknowed standard
J1	orange+white    green+white
J2	orange          green
J3	green+white     orange+white
J4	blue            brown+white
J5	blue+white      brown
J6	green           orange
J7	brown+white     blue
J8	brown           blue+white

Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET multi-ring txrx example start.
Wait for PHY init...
Wait for PHY link up...

20 frames will be sent in 2 queue(s), and frames will be received in 2 queue(s).
The number of frames transmitted from the ring 0, 1 is 10, 10!
20 frames transmitted successfully!
The number of frames successfully received from the ring 0, 1 is 10, 10!
FRDM-MCXE32B
Hardware requirements
  • Type-C USB cable

  • Loopback network cable RJ45 standard

  • FRDM-MCXE32B board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable to Ethernet RJ45 port (J16).

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Make loopback cable:

    568B standard 	Unknowed standard
J1	orange+white    green+white
J2	orange          green
J3	green+white     orange+white
J4	blue            brown+white
J5	blue+white      brown
J6	green           orange
J7	brown+white     blue
J8	brown           blue+white

Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET multi-ring txrx example start.
Wait for PHY init...
Wait for PHY link up...

20 frames will be sent in 2 queue(s), and frames will be received in 2 queue(s).
The number of frames transmitted from the ring 0, 1 is 10, 10!
20 frames transmitted successfully!
The number of frames successfully received from the ring 0, 1 is 10, 10!
MIMXRT2660-EVK
Hardware requirements
  • USB-C cable

  • Loopback network cable RJ45 standard

  • MIMXRT2660-EVK board

  • Personal Computer

Board settings

Connect jumper J52 pins 2-3 to route the on-board analog mux to the external RGMII PHY. The COMM_ENET_QOS MAC then drives the on-board YT8531 gigabit PHY (RGMII, PHY address 0x00) which terminates at RJ45 port J57.

This example uses multiple TX/RX queues at gigabit speed, so the loopback cable goes on J57.

Prepare the Demo
  1. Connect a USB-C cable between the host PC and the debug USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable to Ethernet RJ45 port J57.

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Make loopback cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white

Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET multi-ring txrx example start.

30 frames will be sent in 3 queues, and frames will be received in queues. The frame transmitted from the ring 0, 1, 2 is 10, 10, 10! 30 frames transmitted succeed! The frames successfully received from the ring 0, 1, 2 is 10, 10, 10!

10BASE-T1S PHY support

This example supports the internal 10BASE-T1S PHY (TENBASET_PHY) as an alternative to the external RGMII PHY. To enable, define in board.h:

#define BOARD_NETWORK_USE_TENBASET_PHY (1U)

Hardware setup for 10BASE-T1S mode:

  • Set jumper J52 to position 1-2 to route the board analog mux to the T1S PHY.

  • Attach the T1S link to RJ45 port J40 (the T1S connector dedicated to COMM_ENET_QOS on this EVK).

Hardware setup for RGMII mode:

  • Set jumper J52 to position 2-3 to route the board analog mux to the external RGMII PHY.

  • Use RJ45 port J57 for the RGMII link.