MCUXpresso SDK Documentation

error_recording

error_recording#

Overview#

The ERM project is a simple demonstration program of the SDK ERM driver. It shows how to show error events using the ERM driver.

Supported Boards#

FRDM-MCXL255
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXL255 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

ERM error recording example.

Flipped bit was corrected.

ERM error recording address is 0x28001f00.

ERM error recording example finished successfully.