MCUXpresso SDK Documentation

flexio_mculcd_edma_transfer

flexio_mculcd_edma_transfer#

Overview#

This example shows how to use flexio mculcd edma driver to drive MCU LCD panel. Please focus on functions DEMO_LcdWriteCommand, DEMO_LcdWriteData, and DEMO_LcdWriteMemory to learn how to use the APIs. Note that the DEMO_LcdWriteCommand and DEMO_LcdWriteData still use blocking APIs, because the send data is very small, blocking API is faster in this case. It is still OK to use FLEXIO_MCULCD_TransferEDMA in this case.

In this project, the panel is devided into 4 windows, the project changes the color of each window one by one. The behavior is:

  1. Project starts with black screen.

  2. Fill window one by one as red, and delay 0.5s after fill each window.

  3. Fill window one by one as green, and delay 0.5s after fill each window.

  4. Fill window one by one as blue, and delay 0.5s after fill each window.

  5. Fill window one by one as white, and delay 0.5s after fill each window.

  6. Go to step 2.

+---------------------------+---------------------------+
|                           |                           |
|                           |                           |
|                           |                           |
|      window 0             |        window 1           |
|                           |                           |
|                           |                           |
+---------------------------+---------------------------+
|                           |                           |
|                           |                           |
|                           |                           |
|      window 2             |        window 3           |
|                           |                           |
|                           |                           |
+---------------------------+---------------------------+

Supported Boards#

FRDM-MCXA156
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA156 Board

  • Personal Computer

  • LCD-PAR-S035 board

Board settings

Connect the LCD panel to header J8.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J21.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

FRDM-MCXN236
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN236 board

  • Personal Computer

  • TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika.

Board settings

Connect the panel to header J8. Pin 1 match Pin 1.

Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

FRDM-MCXN947
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947 Board

  • Personal Computer

  • TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika.

Board settings

Connect the panel to header J8. Pin 1 match Pin 1.

Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J17.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

FRDM-MCXN947T
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947T Board

  • Personal Computer

  • TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika.

Board settings

Connect the panel to header J8. Pin 1 match Pin 1.

Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J17.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

MCX-N5XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N5XX-EVK board

  • Personal Computer

  • TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika.

Board settings

Connect the panel to header J20. Pin 1 match Pin 1.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

MCX-N9XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N9XX-EVK Board

  • Personal Computer

  • TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika.

Board settings

Connect the panel to header J20. Pin 1 match Pin 1.

Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J5.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

FRDM-MCXE31B
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXE31B board

  • Personal Computer

  • LCD-PAR-S035 board

Board settings

Connect the LCD panel to header J8.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

FRDM-MCXE32B
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXE32B board

  • Personal Computer

  • LCD-PAR-S035 board

Board settings

Connect the LCD panel to header J8.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

FRDM-MCXA266
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA266 Board

  • Personal Computer

  • LCD-PAR-S035 board

Board settings

Connect the LCD panel to header J8.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

FRDM-MCXA366
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA366 Board

  • Personal Computer

  • LCD-PAR-S035 board

Board settings

Connect the LCD panel to header J8.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

FRDM-MCXA577
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA577 Board

  • Personal Computer

  • LCD-PAR-S035 board

Board settings

Connect the LCD panel to header J8.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.

FRDM-MCXA287
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA287 Board

  • Personal Computer

  • LCD-PAR-S035 board

Board settings

Connect the LCD panel to header J8.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the project running, the panel shows as overview described.