MCUXpresso SDK Documentation

gdet

gdet#

Overview#

Running the demo#

When the demo runs successfully, the terminal displays similar information like the following:


GDET Peripheral Driver Example

GDET Init
GDET Enable
GDET Isolate
* Now VDD voltage can be adjusted *
GDET Change voltage mode
GDET Isolation off

End of example

## Supported Boards

````{container} board-selector

```{container} board-setup
:name: board-frdmmcxn947

##### FRDM-MCXN947

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXN947 board
- Personal Computer

##### Board settings

##### Prepare the Demo
1.  Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

```

```{container} board-setup
:name: board-frdmmcxn947t

##### FRDM-MCXN947T

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXN947T board
- Personal Computer

##### Board settings

##### Prepare the Demo
1.  Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

```

```{container} board-setup
:name: board-mcxn5xxevk

##### MCX-N5XX-EVK

##### Hardware requirements
- Mini/micro USB cable
- MCX-N5XX-EVK Board
- Personal Computer

##### Board settings

##### Prepare the Demo
1.  Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

```

```{container} board-setup
:name: board-mcxn9xxevk

##### MCX-N9XX-EVK

##### Hardware requirements
- Mini/micro USB cable
- MCX-N9XX-EVK board
- Personal Computer

##### Board settings

##### Prepare the Demo
1.  Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

```

```{container} board-setup
:name: board-mimxrt700evk

##### MIMXRT700-EVK

##### Hardware requirements
- Micro USB cable
- MIMXRT700-EVK board
- Personal Computer

##### Board settings

##### Prepare the Demo
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

```

```{container} board-setup
:name: board-frdmimxrt700

##### FRDM-IMXRT700

##### Hardware requirements
- Type-C USB cable
- FRDM-IMXRT700 board
- Personal Computer

##### Board settings

##### Prepare the Demo
1.  Connect a USB cable between the PC host and the CMSIS DAP USB port on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

```

```{container} board-setup
:name: board-frdmkw43

##### FRDM-KW43

##### Hardware requirements
- Type-C USB cable
- FRDM-KW43 Board
- Personal Computer

##### Board settings
No special settings are required.

##### Prepare the Demo
1. Connect a USB cable between the host PC and the FRDM board J28.
2. Open a serial terminal on PC for the serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running
   the demo.

##### Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.

GDET Peripheral Driver Example

GDET Init
GDET Enable
GDET Isolate
* Now VDD voltage can be adjusted *
GDET Change voltage mode
GDET Isolation off

End of example

```

```{container} board-setup
:name: board-frdmmcxw70

##### FRDM-MCXW70

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXW70 Board
- Personal Computer

##### Board settings
No special settings are required.

##### Prepare the Demo
1. Connect a USB cable between the host PC and the FRDM board J28.
2. Open a serial terminal on PC for the serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running
   the demo.

##### Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.

GDET Peripheral Driver Example

GDET Init
GDET Enable
GDET Isolate
* Now VDD voltage can be adjusted *
GDET Change voltage mode
GDET Isolation off

End of example

```

```{container} board-setup
:name: board-frdmmcxa287

##### FRDM-MCXA287

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA287 board
- Personal Computer

##### Board settings

##### Prepare the Demo
1.  Connect a type-c USB cable between the PC host and the MCU-Link USB port (J10) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.

GDET Peripheral Driver Example

GDET Init
GDET Enable
GDET Isolate
* Now VDD voltage can be adjusted *
GDET Change voltage mode
GDET Isolation off

End of example

```

```{container} board-setup
:name: board-frdmmcxa577

##### FRDM-MCXA577

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA577 board
- Personal Computer

##### Board settings

##### Prepare the Demo
1.  Connect a type-c USB cable between the PC host and the MCU-Link USB port (J10) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.

GDET Peripheral Driver Example

GDET Init
GDET Enable
GDET Isolate
* Now VDD voltage can be adjusted *
GDET Change voltage mode
GDET Isolation off

End of example

```

```{container} board-setup
:name: board-mcxw70loc

##### MCXW70-LOC

##### Hardware requirements
- Type-C USB cable
- MCXW70-LOC Board
- Personal Computer

##### Board settings
No special settings are required.

##### Prepare the Demo
1. Connect a USB cable between the host PC and the LOC board J7.
2. Open a serial terminal on PC for the serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running
   the demo.

##### Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.

GDET Peripheral Driver Example

GDET Init
GDET Enable
GDET Isolate
* Now VDD voltage can be adjusted *
GDET Change voltage mode
GDET Isolation off

End of example

```

````