hscmp_interrupt#
Overview#
The HSCMP interrupt Example shows how to use interrupt with HSCMP driver.
In this example, user should indicate an input channel to capture a voltage signal (can be controlled by user) as the HSCMP’s positive channel input. On the negative side, the internal 6-bit DAC is used to generate the fixed voltage about half value of reference voltage.
When running the project, change the input voltage of user-defined channel, then the comparator’s output would change between logic one and zero when the user-defined channel’s voltage crosses the internal DAC’s value. The change of comparator’s output would generate the falling and rising edge events with their interrupts enabled. When any HSCMP interrupt happens, the HSCMP’s ISR would turn on the LED light if detecting the output’s rising edge, or turn off it when detecting the output’s falling edge.
Supported Boards#
LPCXpresso55S36
Hardware requirements
Micro USB cable
Personal Computer
LPCXpresso55S36 board
Board settings
This example project uses HSCMP to compare the voltage signal input from channel 3(P1_5) with the voltage signal(half of VREF_OUT) output by HSCMP’s internal DAC and output different result. LED_RED will turn ON/OFF corresponding to different result. So the voltage signal input from P1_28 should be changed to observe the dynamical LED state.
Input signal to J9-9
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
HSCMP Interrupt Example.
FRDM-MCXC353
Hardware requirements
Type-C USB cable
FRDM-MCXC353 board
Personal Computer
Board settings
This example project uses HSCMP to compare the voltage signal input from CMP0_INP0 with the voltage signal(half of VREF_OUT) output by HSCMP’s internal DAC and output different result. LED_RED will turn ON/OFF corresponding to different result. So the voltage signal input from P1_11 should be changed to observe the dynamical LED state.
CMP0_INP0 input signal J1-13(P1_11).
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
HSCMP Interrupt Example.