MCUXpresso SDK Documentation

lpspi_interrupt_b2b_transfer_slave

lpspi_interrupt_b2b_transfer_slave#

Overview#

The lpspi_interrupt_b2b_transfer example shows how to use LPSPI driver in interrupt way.

In this example, we need two boards, one board used as LPSPI master and another board used as LPSPI slave. The file ‘lpspi_interrupt_b2b_transfer_slave.c’ includes the LPSPI slave code. This example uses the transactional API in LPSPI driver. The LPSPI master send/received data to/from LPSPI slave using interrupt (the LPSPI slave is using interrupt to receive/send the data).

Running the demo#

When the demo runs successfully, you will see output in the terminal like this:

LPSPI interrupt board to board (b2b) transfer slave example.

Slave example is running...

This is LPSPI slave transfer completed callback.
It's a successful transfer.

This is LPSPI slave transfer completed callback.
It's a successful transfer.

Slave received:
     0  1  2  3  4  5  6  7  8  9  A  B  C  D  E  F
    10 11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F
    20 21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F
    30 31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F

Slave example is running...

Supported Boards#

EVK9-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • two MIMX8ULP-EVK/EVK9 boards

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

Remove R139, R159 and populat R140, R158 on both base boards.

SPI two boards: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

INSTANCE0(SPI1)     CONNECTS TO         INSTANCE0(SPI1)
Pin Name   Board Location     Pin Name  Board Location
SPI1_SCK    J23 pin 4            SPI1_SCK  J23 pin 4
SPI1_SIN    J23 pin 2            SPI1_SOUT J23 pin 3
SPI1_SOUT   J23 pin 3            SPI1_SIN  J23 pin 2
SPI1_PCS0   J23 pin 1            SPI1_PCS0 J23 pin 1
GND                             GND
Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

IMX952LPD5EVK-19
Hardware requirements
  • Micro USB cable

  • two IMX952-EVK boards

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

set SW1 into 0000 on IMX952-EVK

Transfer data from one board instance to another board’s instance. SPI7 pins are connected with SPI7 pins of another board

INSTANCE0(SPI7)     CONNECTS TO         INSTANCE0(SPI7)
Pin Name   Board Location       Pin Name  Board Location
SPI_SCK    IMX952LPD5EVK-19   JP1   pin 5	  SPI7_SCK  IMX952LPD5EVK-19    JP1 pin 5
SPI_SIN    IMX952LPD5EVK-19   JP1   pin 3          SPI7_SOUT IMX952LPD5EVK-19    JP1 pin 4
SPI_SOUT   IMX952LPD5EVK-19   JP1   pin 4          SPI7_SIN  IMX952LPD5EVK-19    JP1 pin 3
SPI_PCS0   IMX952LPD5EVK-19   JP1   pin 2          SPI7_PCS0 IMX952LPD5EVK-19    JP1 pin 2
GND                             GND
Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

EVK-MCIMX7ULP
Hardware requirements
  • Micro USB cable

  • two MCIMX7ULP-EVK boards

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

Populate R188, R189, R190, R191 on both base boards.

SPI two boards: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

INSTANCE0(SPI1)     CONNECTS TO         INSTANCE0(SPI1)
Pin Name   Board Location     Pin Name  Board Location
SPI1_SCK    J8 pin 6            SPI1_SCK  J8 pin 6
SPI1_SIN    J8 pin 5            SPI1_SOUT J8 pin 4
SPI1_SOUT   J8 pin 4            SPI1_SIN  J8 pin 5
SPI1_PCS0   J8 pin 3            SPI1_PCS0 J8 pin 3
GND                             GND

Please note this application can’t support running with Linux BSP! Note

Because of the LPSPI signal pin allocating issue, you can not restart this demo/example by press the ResetButton(SW3):
The LPSPI1_SIN, LPSPI1_SOUT, LPSPI1_SCK and LPSPI1_PCS0 pins are connected to PTA12, PTA13, PTA14 and PTA15 pads.
These pins are also used as BOO_CFG12, BOO_CFG13, BOO_CFG14 and BOO_CFG15 when the i.MX SoC reboot. These signals are
driven by LPSPI1 pins on the other board, when user press ResetButton. This may cause M4 Core enter enter
incorrect boot modes and only re-powerup both boards can let the M4 core exit such modes.

##### Prepare the Demo
1.  Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
2.  Connect a micro USB cable between the host PC and the J6 USB port on the target board.
3.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
4.  Download the program to the target board.
5.  Either cold boot your board or launch the debugger in your IDE to begin running the example.
EVK-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • two MIMX8ULP-EVK/EVK9 boards

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

Remove R139, R159 and populat R140, R158 on both base boards.

SPI two boards: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

INSTANCE0(SPI1)     CONNECTS TO         INSTANCE0(SPI1)
Pin Name   Board Location     Pin Name  Board Location
SPI1_SCK    J23 pin 4            SPI1_SCK  J23 pin 4
SPI1_SIN    J23 pin 2            SPI1_SOUT J23 pin 3
SPI1_SOUT   J23 pin 3            SPI1_SIN  J23 pin 2
SPI1_PCS0   J23 pin 1            SPI1_PCS0 J23 pin 1
GND                             GND
Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

EVK-MIMXRT1010
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1010 board

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J57-10             SIN         J57-8
SIN        J57-8              SOUT        J57-10
SCK        J57-12             SCK         J57-12
PCS0       J57-6              PCS0        J57-6
GND        J57-14             GND         J57-14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1015
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1015 board

  • Personal Computer

Board settings

Remove R293 SPI two boards: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J19-4                SIN       J19-5
SIN        J19-5                SOUT      J19-4
SCK        J19-6                SCK       J19-6
PCS0       J19-3                PCS0      J19-3
GND        J19-7                GND       J19-7
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1020
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1020 board

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J19-4                SIN       J19-5
SIN        J19-5                SOUT      J19-4
SCK        J19-6                SCK       J19-6
PCS0       J19-3                PCS0      J19-3
GND        J19-7                GND       J19-7
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1024-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1024-EVK board

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J19-8                SIN       J19-10
SIN        J19-10               SOUT      J19-8
SCK        J19-12               SCK       J19-12
PCS0       J19-6                PCS0      J19-6
GND        J19-14               GND       J19-14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

FRDM-K32L2A4S
Hardware requirements
  • Mini USB cable

  • Two FRDM-K32L2A4S boards

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS0        J2 pin 6            PCS0      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-K32L3A6
Hardware requirements
  • Mini USB cable

  • Two FRDM-K32L3A6 boards

  • Personal Computer

Board settings

SPI two board: Transfer data from one board instance to another board’s instance. To make lpspi example work(M4), connections needed to be as follows: SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS2        J2 pin 6            PCS2      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14

To make lpspi example work(M0), connections needed to be as follows: SPI3 pins are connected with SPI3 pins of another board

INSTANCE3(SPI3)     CONNECTS TO         INSTANCE3(SPI3)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J1 pin 2            SIN       J1 pin 6
SIN         J1 pin 6            SOUT      J1 pin 2
SCK         J3 pin 5            SCK       J3 pin 5
PCS1        J3 pin 9            PCS1      J3 pin 9
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-KE15Z
Hardware requirements
  • Micro USB cable

  • Two FRDM-KE15Z boards

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS3        J2 pin 6            PCS3      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-KE16Z
Hardware requirements
  • Micro USB cable

  • Two FRDM-KE16Z boards

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J4 pin 7            SIN       J4 pin 5
SIN         J4 pin 5            SOUT      J4 pin 7
SCK         J4 pin 3            SCK       J4 pin 3
PCS3        J4 pin 6            PCS3      J4 pin 6
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-KE17Z
Hardware requirements
  • Micro USB cable

  • Two FRDM-KE17Z boards

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS1        J2 pin 6            PCS1      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-KE17Z512
Hardware requirements
  • Micro USB cable

  • Two FRDM-KE17Z512 boards

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS2        J2 pin 6            PCS2      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a USB cable between the PC host and the MCU-LINK USB port on the board.

  2. Open a serial terminal on PC for MCU-LINK serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-MCXA153
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA153 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI0)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J6-6                SIN       J2-10
SIN        J6-5                SOUT      J2-8
SCK        J6-4                SCK       J2-12
PCS0       J6-3                PCS1      J2-6
GND        J6-8                GND       J6-8
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA156
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA156 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI0)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J6-6                SIN       J3-9
SIN        J6-5                SOUT      J3-11
SCK        J6-4                SCK       J3-7
PCS0       J6-3                PCS1      J3-5
GND        J6-8                GND       J6-8
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA346
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA346 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXE247
Hardware requirements
  • USB-C cable

  • Two FRDM-MCXE247 boards

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J6 pin 6            SIN       J6 pin 5
SIN         J6 pin 5            SOUT      J6 pin 6
SCK         J6 pin 4            SCK       J6 pin 4
PCS2        J6 pin 3            PCS2      J6 pin 3
GND         J6 pin 8            GND       J6 pin 8
Prepare the Demo
  1. Connect a USB cable between the PC host and the MCU-LINK USB port on the board.

  2. Open a serial terminal on PC for MCU-LINK serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-MCXN236
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN236 board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Jumper setting:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 - 8           SIN         J2 - 10
SIN        J2 - 10          SOUT        J2 - 8
SCK        J2 - 12          SCK         J2 - 12
PCS0       J2 - 6           PCS0        J2 - 6
GND        J2 - 14          GND         J2 - 14

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXN947
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Jumper setting:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 - 8           SIN         J2 - 10
SIN        J2 - 10          SOUT        J2 - 8
SCK        J2 - 12          SCK         J2 - 12
PCS0       J2 - 6           PCS0        J2 - 6
GND        J2 - 14          GND         J2 - 14

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXN947T
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947T board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Jumper setting:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 - 8           SIN         J2 - 10
SIN        J2 - 10          SOUT        J2 - 8
SCK        J2 - 12          SCK         J2 - 12
PCS0       J2 - 6           PCS0        J2 - 6
GND        J2 - 14          GND         J2 - 14

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXW71
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW71 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Be sure to disconnect the 12V adapter on J9, otherwise the transmission will fail. Jumper setting:

MASTER(SPI0)                connect to      SLAVE(SPI0)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 9                         SIN         J1 pin 2
SIN        J1 pin 2                         SOUT        J2 pin 9
SCK        J1 pin 5                         SCK         J1 pin 5
PCS0       J1 pin 1                         PCS0        J1 pin 1

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCX-W71-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W71-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 13                        SIN         J2 pin 11
SIN        J2 pin 11                        SOUT        J2 pin 13
SCK        J2 pin 9                         SCK         J2 pin 9
PCS0       J2 pin 15                        PCS0        J2 pin 15

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXW72
Hardware requirements
  • Type-C USB cable

  • RDM-MCXW72 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 7                         SIN         J2 pin 6
SIN        J2 pin 6                         SOUT        J2 pin 7
SCK        J2 pin 5                         SCK         J2 pin 5
PCS0       J2 pin 8                         PCS0        J2 pin 8
GND        J2 pin 4                         GND         J2 pin 4

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

KW45B41Z-EVK
Hardware requirements
  • Mini/micro USB cable

  • KW45B41Z-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Be sure to disconnect the 12V adapter on J9, otherwise the transmission will fail. Jumper setting:

MASTER(SPI0)                connect to      SLAVE(SPI0)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 2                         SIN         J1 pin 2
SIN        J1 pin 2                         SOUT        J2 pin 2
SCK        J1 pin 5                         SCK         J1 pin 5
PCS0       J1 pin 1                         PCS0        J1 pin 1

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

KW47-EVK
Hardware requirements
  • Type-C USB cable

  • KW47-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 13                        SIN         J2 pin 11
SIN        J2 pin 11                        SOUT        J2 pin 13
SCK        J2 pin 9                         SCK         J2 pin 9
PCS0       J2 pin 15                        PCS0        J2 pin 15

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCIMX93AUTO-EVK
Hardware requirements
  • USB Type-C cable

  • two MCIMX93AUTO-EVK boards

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

Transfer data from one board instance to another board’s instance. SPI3 pins are connected with SPI3 pins of another board

INSTANCE0(SPI3)     CONNECTS TO         INSTANCE0(SPI3)
Pin Name   Board Location       Pin Name  Board Location
SPI3_SCK    J16  pin  23        SPI3_SCK  J16  pin  23
SPI3_SIN    J16  pin  21        SPI3_SOUT J16  pin  19
SPI3_SOUT   J16  pin  19        SPI3_SIN  J16  pin  21
SPI3_PCS0   J16  pin  24        SPI3_PCS0 J16  pin  24
GND                             GND
Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

MCIMX93-EVK
Hardware requirements
  • USB Type-C cable

  • two MCIMX93-EVK boards

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

Transfer data from one board instance to another board’s instance. SPI3 pins are connected with SPI3 pins of another board

INSTANCE0(SPI3)     CONNECTS TO         INSTANCE0(SPI3)
Pin Name   Board Location       Pin Name  Board Location
SPI3_SCK    J1001 pin 23        SPI3_SCK  J1001 pin 23
SPI3_SIN    J1001 pin 21        SPI3_SOUT J1001 pin 19
SPI3_SOUT   J1001 pin 19        SPI3_SIN  J1001 pin 21
SPI3_PCS0   J1001 pin 24        SPI3_PCS0 J1001 pin 24
GND                             GND
Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

MCIMX93W-EVK
Hardware requirements
  • USB Type-C cable

  • two MCIMX93W-EVK boards

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

Transfer data from one board instance to another board’s instance. SPI3 pins are connected with SPI3 pins of another board

INSTANCE0(SPI3)     CONNECTS TO         INSTANCE0(SPI3)
Pin Name   Board Location       Pin Name  Board Location
SPI3_SCK    J1001 pin 23        SPI3_SCK  J1001 pin 23
SPI3_SIN    J1001 pin 21        SPI3_SOUT J1001 pin 19
SPI3_SOUT   J1001 pin 19        SPI3_SIN  J1001 pin 21
SPI3_PCS0   J1001 pin 24        SPI3_PCS0 J1001 pin 24
GND                             GND
Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

MCIMX93-QSB
Hardware requirements
  • USB Type-C cable

  • two MCIMX93-QSB boards

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

Transfer data from one board instance to another board’s instance. SPI3 pins are connected with SPI3 pins of another board

INSTANCE0(SPI3)     CONNECTS TO         INSTANCE0(SPI3)
Pin Name   Board Location       Pin Name  Board Location
SPI3_SCK    J1401 pin 23        SPI3_SCK  J1401 pin 23
SPI3_SIN    J1401 pin 21        SPI3_SOUT J1401 pin 19
SPI3_SOUT   J1401 pin 19        SPI3_SIN  J1401 pin 21
SPI3_PCS0   J1401 pin 24        SPI3_PCS0 J1401 pin 24
GND                             GND
Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1708 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

MCX-N5XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N5xx-EVK board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Jumper setting:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 - 8           SIN         J2 - 10
SIN        J2 - 10          SOUT        J2 - 8
SCK        J2 - 12          SCK         J2 - 12
PCS0       J2 - 6           PCS0        J2 - 6
GND        J2 - 14          GND         J2 - 14

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCX-N9XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N9xx-EVK board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Jumper setting:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 - 8           SIN         J2 - 10
SIN        J2 - 10          SOUT        J2 - 8
SCK        J2 - 12          SCK         J2 - 12
PCS0       J2 - 6           PCS0        J2 - 6
GND        J2 - 14          GND         J2 - 14

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCX-W72-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W72-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 13                        SIN         J2 pin 11
SIN        J2 pin 11                        SOUT        J2 pin 13
SCK        J2 pin 9                         SCK         J2 pin 9
PCS0       J2 pin 15                        PCS0        J2 pin 15

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT700-EVK
Hardware requirements
  • Micro USB cable

  • Two MIMXRT700-EVK boards

  • Personal Computer

Board settings
  1. Make sure JP12 is installed

  2. SPI two boards: Transfer data from one board instance to another board’s instance. SPI14 pins are connected with SPI14 pins of another board

INSTANCE0(SPI14)     CONNECTS TO         INSTANCE0(SPI14)
Pin Name   Board Location           Pin Name  Board Location
SOUT        J20 pin 3                   SIN       J20 pin 5
SIN         J20 pin 5                   SOUT      J20 pin 3
SCK         J20 pin 7                   SCK       J20 pin 7
PCS0        J20 pin 1                   PCS0      J20 pin 1
GND         J20 pin 9                   GND       J20 pin 9
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-IMXRT700
Hardware requirements
  • Type-C USB cable

  • Two FRDM-IMXRT700 boards

  • Personal Computer

Board settings
  1. SPI two boards: Transfer data from one board instance to another board’s instance. SPI16 pins are connected with SPI16 pins of another board

INSTANCE0(SPI16)     CONNECTS TO         INSTANCE0(SPI16)
Pin Name   Board Location           Pin Name  Board Location
SOUT        J22 pin 6                   SIN       J22 pin 5
SIN         J22 pin 5                   SOUT      J22 pin 6
SCK         J22 pin 4                   SCK       J22 pin 4
PCS0        J22 pin 3                   PCS0      J22 pin 3
GND         J22 pin 8                   GND       J22 pin 8
Prepare the Demo
  1. Connect a USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-MCXE31B
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXE31B board

  • Personal Computer

Board settings

LPSPI:

INSTANCE1(LPSPI_1)     CONNECTS TO         INSTANCE1(LPSPI_1)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J6 pin 6           SIN       J6 pin 5
SIN         J6 pin 5           SOUT      J6 pin 6
SCK         J6 pin 4           SCK       J6 pin 4
PCS0        J6 pin 3           PCS0      J6 pin 3 
GND         J6 pin 8           GND       J6 pin 8
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXE32B
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXE32B board

  • Personal Computer

Board settings

LPSPI:

INSTANCE1(LPSPI_1)     CONNECTS TO         INSTANCE1(LPSPI_1)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J6 pin 6           SIN       J6 pin 5
SIN         J6 pin 5           SOUT      J6 pin 6
SCK         J6 pin 4           SCK       J6 pin 4
PCS0        J6 pin 3           PCS0      J6 pin 3 
GND         J6 pin 8           GND       J6 pin 8
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXL255
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXL255 board

  • Personal Computer

Board settings

LPSPI:

            MASTER(SPI1)        connect to      SLAVE(SPI1)
Pin Name    Board Location      Pin Name        Board Location
SOUT        J2-8                SIN             J2-10
SIN         J2-10               SOUT            J2-8
SCK         J2-12               SCK             J2-12
PCS0        J2-6                PCS1            J2-6
GND         J2-14               GND             J2-14

Make sure you have solder bridges SJ1 and SJ2 set to

  • 2-1 for the main core (cm33)

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA174
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA174 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA344
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA344 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

KW47-LOC
Hardware requirements
  • Type-C USB cable

  • KW47-LOC Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 6                         SIN         J1 pin 5
SIN        J1 pin 5                         SOUT        J1 pin 6
SCK        J1 pin 4                         SCK         J1 pin 4
PCS0       J1 pin 3                         PCS0        J1 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCXW72-LOC
Hardware requirements
  • Type-C USB cable

  • MCXW72-LOC Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 6                         SIN         J1 pin 5
SIN        J1 pin 5                         SOUT        J1 pin 6
SCK        J1 pin 4                         SCK         J1 pin 4
PCS0       J1 pin 3                         PCS0        J1 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA266
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA266 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA366
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA366 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA577
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA577 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXC162
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXC162 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI0)      connect to        SLAVE(SPI0)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-KW43
Hardware requirements
  • Type-C USB cable

  • FRDM-KW43 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J19 pin 5                        SIN         J19 pin 4
SIN        J19 pin 4                        SOUT        J19 pin 5
SCK        J19 pin 6                        SCK         J19 pin 6
PCS0       J19 pin 3                        PCS0        J19 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a Type-C USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXW70
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW70 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J19 pin 5                        SIN         J19 pin 4
SIN        J19 pin 4                        SOUT        J19 pin 5
SCK        J19 pin 6                        SCK         J19 pin 6
PCS0       J19 pin 3                        PCS0        J19 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a Type-C USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA287
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA287 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

frdmimx952
Hardware requirements
  • Micro USB cable

  • two IMX952-EVK boards

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

Connection as below:

MASTER(LPSPI7)                connect to        SLAVE(LPSPI7)
Pin Name    Board Location                      Pin Name    Board Location
PCS0        J18 pin 7                           PCS0        J18 pin 7
SCK         J18 pin 26                          SCK         J18 pin 26
SOUT        J18 pin 31                          SIN         J18 pin 29
SIN         J18 pin 29                          SOUT        J18 pin 31
GND         J18 pin 6                           GND         J18 pin 6

IMPORTANT: SOUT/SIN (MOSI/MISO) lines MUST be crossed as shown above.

Note: J18 is the 40-PIN GPIO HDR expansion connector. - J18-Pin7: LPSPI7_PCS0 (GPIO_IO04) - Chip Select - J18-Pin26: LPSPI7_SCK (GPIO_IO07) - Clock - J18-Pin31: LPSPI7_SOUT (GPIO_IO06) - MOSI (connects to slave SIN) - J18-Pin29: LPSPI7_SIN (GPIO_IO05) - MISO (connects to slave SOUT) - J18-Pin6: Common Ground (any GND pin on J18 can be used) - Each board must be powered independently - No IO expander configuration required for this example

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

FRDM-IMX95
Hardware requirements
  • Micro USB cable

  • one FRDM-IMX95 board and MCIMX93EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

Transfer data from one board instance to another board’s instance. SPI3 pins are connected with SPI3 pins of another board

INSTANCE0(SPI3)     CONNECTS TO         INSTANCE0(SPI3)
Pin Name   Board Location       Pin Name  Board Location
SPI3_SCK   FRDMIMX95    J19 pin 23	  SPI3_SCK  FRDMIMX95    J19 pin 23
SPI3_SIN   FRDMIMX95    J19 pin 21          SPI3_SOUT FRDMIMX95    J19 pin 19
SPI3_SOUT  FRDMIMX95    J19 pin 19          SPI3_SIN  FRDMIMX95    J19 pin 21
SPI3_PCS0  FRDMIMX95    J19 pin 24          SPI3_PCS0 FRDMIMX95    J19 pin 24
GND                             GND
Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

FRDM-IMX937
Hardware requirements
  • Micro USB cable

  • two FRDM-IMX937 boards

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

Connection as below:

MASTER(LPSPI7)                connect to        SLAVE(LPSPI7)
Pin Name    Board Location                      Pin Name    Board Location
PCS0        J18 pin 7                           PCS0        J18 pin 7
SCK         J18 pin 26                          SCK         J18 pin 26
SOUT        J18 pin 31                          SIN         J18 pin 29
SIN         J18 pin 29                          SOUT        J18 pin 31
GND         J18 pin 6                           GND         J18 pin 6

IMPORTANT: SOUT/SIN (MOSI/MISO) lines MUST be crossed as shown above.

Note: J18 is the 40-PIN GPIO HDR expansion connector. - J18-Pin7: LPSPI7_PCS0 (GPIO_IO04) - Chip Select - J18-Pin26: LPSPI7_SCK (GPIO_IO07) - Clock - J18-Pin31: LPSPI7_SOUT (GPIO_IO06) - MOSI (connects to slave SIN) - J18-Pin29: LPSPI7_SIN (GPIO_IO05) - MISO (connects to slave SOUT) - J18-Pin6: Common Ground (any GND pin on J18 can be used) - Each board must be powered independently - No IO expander configuration required for this example

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.