MCUXpresso SDK Documentation

lpuart_edma_transfer

lpuart_edma_transfer#

Overview#

The lpuart_edma Example project is to demonstrate usage of the KSDK lpuart driver. In the example, you can send characters to the console back and they will be printed out onto console in a group of 8 characters.

Supported Boards#

EVK9-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!

Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download flash.bin for single boot type: a. Download to emmc(for single boot type) with uuu

    uuu -b emmc imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 flash.bin (Need download the file imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 from linux bsp)

    for low power boot type/dual boot type: a. Download to flexspi nor flash of m33 with uboot console(pls refer to the doc Getting Started with MCUXpresso SDK for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf) b. Download to flexspi nor flash of m33(for low power boot type/dual boot type) with jlink(pls refer to the doc Getting Started with MCUXpresso SDK for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf) c. Download to flexspi nor flash of m33 with uuu(write a uuu script to write flash.bin to flexspi nor flash of m33, pls refer to uuu manual)

  5. Power Off board and Power on board

  6. Note: Pls not running the demo that use TRDC with debugger(jlink or others)

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
IMX952LPD5EVK-19
Hardware requirements
  • Micro USB cable

  • IMX952-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!
Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
EVKB-IMXRT1050
Hardware requirements
  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKB board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-IMXRT1152
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1152 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
EVK-MCIMX7ULP
Hardware requirements
  • Micro USB cable

  • MCIMX7ULP-EVK board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!

Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.

  2. Connect a micro USB cable between the host PC and the J6 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
EVK-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!

Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download flash.bin for single boot type: a. Download to emmc(for single boot type) with uuu

    uuu -b emmc imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 flash.bin (Need download the file imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 from linux bsp)

    for low power boot type/dual boot type: a. Download to flexspi nor flash of m33 with uboot console(pls refer to the doc Getting Started with MCUXpresso SDK for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf) b. Download to flexspi nor flash of m33(for low power boot type/dual boot type) with jlink(pls refer to the doc Getting Started with MCUXpresso SDK for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf) c. Download to flexspi nor flash of m33 with uuu(write a uuu script to write flash.bin to flexspi nor flash of m33, pls refer to uuu manual)

  5. Power Off board and Power on board

  6. Note: Pls not running the demo that use TRDC with debugger(jlink or others)

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
EVK-MIMXRT1010
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1010 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1015
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1015 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1020
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1020 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1024-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1024-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1040-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
EVK-MIMXRT1064
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1064 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MIMXRT1160-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MIMXRT1180-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-K22F
Hardware requirements
  • Mini/Micro USB cable

  • FRDM-K22F board

  • Personal Computer

  • USB to Com Converter

Board settings

Connect pin:

  • RX of USB2COM to J1-4

  • TX of USB2COM to J1-2

  • GND of USB2COM to J2-14

Prepare the Demo
  1. Connect USB to Com Converter between the PC host and the port on the board.

  2. Open a serial terminal on PC for serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the LPUART Terminal port which connected to the USB2COM like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-K32L2A4S
Hardware requirements
  • Mini USB cable

  • FRDM-K32L2A4S board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-K32L3A6
Hardware requirements
  • Mini/Micro USB cable

  • FRDM-K32L3A6 board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-KE15Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE15Z board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-KE17Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE17Z board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-KE17Z512
Hardware requirements
  • Micro USB cable

  • FRDM-KE17Z512 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXA153
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA153 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXA156
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA156 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXA346
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA346 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXE247
Hardware requirements
  • USB-C cable

  • FRDM-MCXE247 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXN236
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN236 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXN947
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXN947T
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947T board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXW71
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW71 Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MCX-W71-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W71-EVK Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
IMX95LPD5EVK-19
Hardware requirements
  • Micro USB cable

  • IMX95LPD5-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-IMX95
Hardware requirements
  • Micro USB cable

  • FRDM-IMX95 board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-IMX952
Hardware requirements
  • Micro USB cable

  • IMX952-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!
Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-IMX937
Hardware requirements
  • Micro USB cable

  • FRDM-IMX937 board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
KW45B41Z-EVK
Hardware requirements
  • Mini/micro USB cable

  • KW45B41Z-EVK Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
KW47-EVK
Hardware requirements
  • Type-C USB cable

  • KW47-EVK Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MCIMX93AUTO-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93AUTO-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Boot Linux BSP to u-boot, and load M core image from SD card to run. (Put the image into SD card before.) => load mmc 1:1 0x80000000 /sdk20-app.bin => cp.b 0x80000000 0x201e0000 0x20000 => bootaux 0x1ffe0000 0

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
MCIMX93-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Boot Linux BSP to u-boot, and load M core image from SD card to run. (Put the image into SD card before.) => load mmc 1:1 0x80000000 /sdk20-app.bin => cp.b 0x80000000 0x201e0000 0x20000 => bootaux 0x1ffe0000 0

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
MCIMX93W-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93W-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Boot Linux BSP to u-boot, and load M core image from SD card to run. (Put the image into SD card before.) => load mmc 1:1 0x80000000 /sdk20-app.bin => cp.b 0x80000000 0x201e0000 0x20000 => bootaux 0x1ffe0000 0

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
MCIMX93-QSB
Hardware requirements
  • USB Type-C cable

  • MCIMX93-QSB board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Boot Linux BSP to u-boot, and load M core image from SD card to run. (Put the image into SD card before.) => load mmc 1:1 0x80000000 /sdk20-app.bin => cp.b 0x80000000 0x201e0000 0x20000 => bootaux 0x1ffe0000 0

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
IMX943-EVK
Hardware requirements
  • Micro USB cable

  • IMX943-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!
Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.

  2. Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
MCX-N5XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N5XX-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MCX-N9XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MCX-W72-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W72-EVK Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MIMXRT700-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

  • USB to serial converter

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the DEBUG PORT(J54) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-LINK terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-IMXRT700
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT700 board

  • Personal Computer

  • USB to serial converter

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the DEBUG PORT(J54) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-LINK terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXL255
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXL255 board

  • Personal Computer

Board settings

Make sure you have solder bridges SJ1 and SJ2 set to

  • 2-1 for the main core (cm33)

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXA174
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA174 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXA344
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA344 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
KW47-LOC
Hardware requirements
  • Type-C USB cable

  • KW47-LOC Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MCXW72-LOC
Hardware requirements
  • Type-C USB cable

  • MCXW72-LOC Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-IMXRT1186
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXA266
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA266 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXA366
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA366 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXW72
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW72 Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXA577
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA577 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXC162
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXC162 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-KW43
Hardware requirements
  • Type-C USB cable

  • FRDM-KW43 Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J28.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXW70
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW70 Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J28.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
FRDM-MCXA287
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA287 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the MCU-Link terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
IMX943-ORANGEBOX
Hardware requirements
  • Micro USB cable

  • IMX943-ORANGEBOX board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No need special setting.

Please note this application can’t support running with Linux BSP!
Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.

  2. Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPUART EDMA example
Send back received data
Echo every 8 characters
MIMXRT2660-EVK
Hardware requirements
  • Type-C USB cable

  • MIMXRT2660-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters
MCXW70-LOC
Hardware requirements
  • Type-C USB cable

  • MCXW70-LOC Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the host PC and the LOC board J7.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART EDMA example
Send back received data
Echo every 8 characters