lpuart_polling_seven_bits#
Overview#
The lpuart_polling_seven_bits Example project is to demonstrate usage of the KSDK lpuart driver with seven data bits feature enabled. In the example, you can send characters to the console back and they will be printed out onto console instantly. NOTE: Please set com port format to “7 data bits without parity bit” in PC’s com port tool
Supported Boards#
EVKB-IMXRT1050
Hardware requirements
Mini/micro USB cable
EVKB-IMXRT1050 board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J22-2
TX of USB2COM to J22-1
GND of USB2COM to J24-7
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
MIMXRT1060-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J16-2
TX of USB2COM to J16-1
GND of USB2COM to J17-7
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J25-15
TX of USB2COM to J25-13
GND of USB2COM to J25-14
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
MIMXRT1060-EVKC
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKC board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J16-2
TX of USB2COM to J16-1
GND of USB2COM to J17-7
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-IMXRT1152
Hardware requirements
Type-C USB cable
FRDM-IMXRT1152 board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J11-8
TX of USB2COM to J11-10
GND of USB2COM to J11-14
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
EVK-MIMXRT1010
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1010 board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J26-12
TX of USB2COM to J26-10
GND of USB2COM to J60-14
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart interrupt example with seven data bits
Board receives 8 characters then sends them out
Now please input:
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
EVK-MIMXRT1015
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1015 board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J17-2
TX of USB2COM to J17-1
GND of USB2COM to J19-7
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
EVK-MIMXRT1020
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1020 board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J17-2
TX of USB2COM to J17-1
GND of USB2COM to J19-7
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
MIMXRT1024-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1024-EVK board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J17-4
TX of USB2COM to J17-2
GND of USB2COM to J19-14
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
MIMXRT1040-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1040-EVK board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J16-2
TX of USB2COM to J16-1
GND of USB2COM to J17-7
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
EVK-MIMXRT1064
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1064 board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J22-2
TX of USB2COM to J22-1
GND of USB2COM to J24-7
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
MIMXRT1160-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1160-EVK board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J25-15
TX of USB2COM to J25-13
GND of USB2COM to J25-14
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
MIMXRT1180-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
TX of USB2COM to J44-20
RX of USB2COM to J44-18
GND of USB2COM to J44-14
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-K32L3A6
Hardware requirements
Micro USB cable
FRDM-K32L3A6 board
Personal Computer
USB to Com converter
Board settings
PTA25(J1-2) connect to TxD of the USB to Com converter . PTA26(J1-4) connect to RxD of the USB to Com converter. GND(J2-14) connect to GND of the USB to Com converter.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
When the example runs successfully, the following message is displayed in the terminal:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-KE15Z
Hardware requirements
Micro USB cable
FRDM-KE15Z board
Personal Computer
USB to Com converter
Board settings
PTA2(J4-10) connect to TxD of the USB to Com converter. PTA3(J4-12) connect to RxD of the USB to Com converter. GND(J3-14) connect to GND of the USB to Com converter.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-KE16Z
Hardware requirements
Micro USB cable
FRDM-KE16Z board
Personal Computer
USB to Com converter
Board settings
PTD6(J2-11) connect to TxD of the USB to Com converter . PTD7(J4-9) connect to RxD of the USB to Com converter. GND(J2-14) connect to GND of the USB to Com converter.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-KE17Z
Hardware requirements
Micro USB cable
FRDM-KE17Z board
Personal Computer
USB to Com converter
Board settings
PTA2(J1-2) connect to TxD of the USB to Com converter. PTA3(J1-4) connect to RxD of the USB to Com converter. GND(J3-14) connect to GND of the USB to Com converter.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-KE17Z512
Hardware requirements
Micro USB cable
FRDM-KE17Z512 board
Personal Computer
USB to Com converter
Board settings
PTA2(J1-2) connect to TxD of the USB to Com converter. PTA3(J1-4) connect to RxD of the USB to Com converter. GND(J3-14) connect to GND of the USB to Com converter.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXA153
Hardware requirements
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA153 board. FRDM-MCXA153 UART pins:
TX of USB2COM to J2-4(P3_14)
RX of USB2COM to J2-2(P3_15)
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXA156
Hardware requirements
Type-C USB cable
FRDM-MCXA156 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA156 board.
TX of USB2COM to J5-3(P3_20)
RX of USB2COM to J5-4(P3_21)
GND of the USB2COM to J5-8(GND)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXA346
Hardware requirements
Type-C USB cable
FRDM-MCXA346 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA346 board.
TX of USB2COM to J5-3(P4_2)
RX of USB2COM to J5-4(P4_5)
GND of the USB2COM to J5-8(GND)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXE247
Hardware requirements
USB-C cable
FRDM-MCXE247 board
Personal Computer
USB to COM converter
Board settings
PTC9(J5-4) connect to RxD of the USB to COM converter. PTC8(J5-3) connect to TxD of the USB to COM converter. GND(J5-8) connect to GND of the USB to COM converter.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXL255
Hardware requirements
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXL255 board.
CM33:
TX of USB2COM to SJ1-1(P2_10)
RX of USB2COM to SJ2-1(P2_11)
AON (CM0+):
TX of USB2COM to SJ1-3(P0_7)
RX of USB2COM to SJ2-3(P0_6)
Make sure you have solder bridges SJ1 and SJ2 set to
2-1 for the main core (cm33)
2-3 for AON core (cm0+)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXN236
Hardware requirements
Type-C USB cable
FRDM-MCXN236 board
Personal Computer
USB to TTL converter
Board settings
Connect the USB to TTL converter to FRDM-MCXN236 board. MCX-N9XX-EVK UART pins:
TX of USB2COM to J8-4(P4_0)
RX of USB2COM to J8-3(P4_1)
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J10) on the board
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
USB to TTL converter
Board settings
Connect the USB to TTL converter to FRDM-MCXN947 board. FRDM-MCXN947 UART pins:
TX of USB2COM to J8-9(P0_12)
RX of USB2COM to J8-12(P0_13)
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T board
Personal Computer
USB to TTL converter
Board settings
Connect the USB to TTL converter to FRDM-MCXN947T board. FRDM-MCXN947T UART pins:
TX of USB2COM to J8-9(P0_12)
RX of USB2COM to J8-12(P0_13)
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXW71
Hardware requirements
Type-C USB cable
FRDM-MCXW71 Board
USB to Serial Converter
Personal Computer
Board settings
The connection should be set as following:
J1-1(PTA16), TX of USB2COM connected
J1-2(PTA17), RX of USB2COM connected
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal on PC for USB2COM serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the USB2COM terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
MCX-W71-EVK
Hardware requirements
Type-C USB cable
MCX-W71-EVK Board
USB to Serial Converter
Personal Computer
Board settings
The connection should be set as following:
J1-1(PTA16), TX of USB2COM connected
J1-3(PTA17), RX of USB2COM connected
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for USB2COM serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the USB2COM terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
KW45B41Z-EVK
Hardware requirements
Mini/micro USB cable
KW45B41Z-EVK Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
KW47-EVK
Hardware requirements
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
Note: Only the MCU-Link with CMSIS-DAP debugger protocol firmware supports the seven bits transfer. Please check the getting started guide on how to update the MCU-Link debugger firmware.
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
USB to TTL converter
Board settings
Connect the USB to TTL converter to MCX-N5XX-EVK board. MCX-N5XX-EVK UART pins:
TX of USB2COM to J20-9(P0_12)
RX of USB2COM to J20-12(P0_13)
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
USB to TTL converter
Board settings
Connect the USB to TTL converter to MCX-N9XX-EVK board. MCX-N9XX-EVK UART pins:
TX of USB2COM to J20-9(P0_12)
RX of USB2COM to J20-12(P0_13)
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
MCX-W72-EVK
Hardware requirements
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
Note: Only the MCU-Link with CMSIS-DAP debugger protocol firmware supports the seven bits transfer. Please check the getting started guide on how to update the MCU-Link debugger firmware.
MIMXRT700-EVK
Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
USB to Com Converter
Board settings
Remove Jumper JP22.
Connect pin:
RX of USB2COM to JP13-4
TX of USB2COM to JP13-5
GND of USB2COM to JP13-1
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the DEBUG PORT on the board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-LINK terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXE31B
Hardware requirements
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
TX of USB2COM to J1-2
RX of USB2COM to J1-4
GND of USB2COM to J2-14
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXE32B
Hardware requirements
Type-C USB cable
FRDM-MCXE32B board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
TX of USB2COM to J1-2
RX of USB2COM to J1-4
GND of USB2COM to J2-14
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXA174
Hardware requirements
Type-C USB cable
FRDM-MCXA174 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA174 board.
TX of USB2COM to J5-3(P4_2)
RX of USB2COM to J5-4(P4_5)
GND of the USB2COM to J5-8(GND)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXA344
Hardware requirements
Type-C USB cable
FRDM-MCXA344 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA344 board.
TX of USB2COM to J5-3(P4_2)
RX of USB2COM to J5-4(P4_5)
GND of the USB2COM to J5-8(GND)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
KW47-LOC
Hardware requirements
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
Note: Only the MCU-Link with CMSIS-DAP debugger protocol firmware supports the seven bits transfer. Please check the getting started guide on how to update the MCU-Link debugger firmware.
MCXW72-LOC
Hardware requirements
Type-C USB cable
MCXW72-LOC Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
Note: Only the MCU-Link with CMSIS-DAP debugger protocol firmware supports the seven bits transfer. Please check the getting started guide on how to update the MCU-Link debugger firmware.
FRDM-IMXRT1186
Hardware requirements
Type-C USB cable
FRDM-IMXRT1186 board
Personal Computer
USB to Com Converter
Board settings
Change Jumper J41 from 1-2 to 2-3, Jumper J43 from 1-2 to 2-3. Connect pin:
TX of USB2COM to J1-2
RX of USB2COM to J1-4
GND of USB2COM to J1-15
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXA266
Hardware requirements
Type-C USB cable
FRDM-MCXA266 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA266 board.
TX of USB2COM to J5-3(P4_2)
RX of USB2COM to J5-4(P4_5)
GND of the USB2COM to J5-8(GND)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXA366
Hardware requirements
Type-C USB cable
FRDM-MCXA366 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA366 board.
TX of USB2COM to J5-3(P4_2)
RX of USB2COM to J5-4(P4_5)
GND of the USB2COM to J5-8(GND)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXW72
Hardware requirements
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
Note: Only the MCU-Link with CMSIS-DAP debugger protocol firmware supports the seven bits transfer. Please check the getting started guide on how to update the MCU-Link debugger firmware.
FRDM-MCXA577
Hardware requirements
Type-C USB cable
FRDM-MCXA577 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA577 board.
TX of USB2COM to J5-3(P0_24)
RX of USB2COM to J5-4(P0_25)
GND of the USB2COM to J5-8(GND)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXC162
Hardware requirements
Type-C USB cable
FRDM-MCXC162 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXC162 board.
TX of USB2COM to J5-3(P3_13)
RX of USB2COM to J5-4(P3_12)
GND of the USB2COM to J5-8(GND)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-KW43
Hardware requirements
Type-C USB cable
FRDM-KW43 Board
Personal Computer
USB to serial (UART) converter
Board settings
Using instance 0 of LPUART interface to transfer data to USB to serial (UART) converter.
LPUART0 CONNECTS TO USB to serial (UART) converter Pin Name Board Location Pin Name TXD JP19-1 RXD RXD J19-1 TXD
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal on PC for USB to serial (UART) converter serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the USB to serial (UART) converter terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXW70
Hardware requirements
Type-C USB cable
FRDM-MCXW70 Board
Personal Computer
USB to serial (UART) converter
Board settings
Using instance 0 of LPUART interface to transfer data to USB to serial (UART) converter.
LPUART0 CONNECTS TO USB to serial (UART) converter Pin Name Board Location Pin Name TXD JP19-1 RXD RXD J19-1 TXD
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal on PC for USB to serial (UART) converter serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the USB to serial (UART) converter terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
FRDM-MCXA287
Hardware requirements
Type-C USB cable
FRDM-MCXA287 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA287 board.
TX of USB2COM to J5-3(P0_24)
RX of USB2COM to J5-4(P0_25)
GND of the USB2COM to J5-8(GND)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart polling example with seven data bits
Board will send back received characters
MIMXRT2660-EVK
Hardware requirements
Type-C USB cable
MIMXRT2660-EVK board
Personal Computer
USB to Com Converter
Board settings
HSP_LPUART1_TXD (PIO3_8, J94-21), RX of USB2COM connected
HSP_LPUART1_RXD (PIO3_9, J94-22), TX of USB2COM connected
Ground connection
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
MCXW70-LOC
Hardware requirements
Type-C USB cable
MCXW70-LOC Board
Personal Computer
USB to serial (UART) converter
Board settings
Using instance 0 of LPUART interface to transfer data to USB to serial (UART) converter.
LPUART0 CONNECTS TO USB to serial (UART) converter Pin Name Board Location Pin Name TXD JS6-3 RXD RXD JS5-3 TXD
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J7.
Open a serial terminal on PC for USB to serial (UART) converter serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the USB to serial (UART) converter terminal like:
Lpuart polling example with seven data bits
Board will send back received characters