mcx_enet_txrx_ptp1588_transfer#
Overview#
The enet_rxtx_ptp1588_transfer example shows the way to use ENET driver to
receive and transmit frame in the 1588 feature required cases.
This example shows how to initialize the ENET.
How to get the time stamp of the PTP 1588 timer.
How to use Get the ENET transmit and receive frame time stamp.
The example transmits 20 number PTP event frame, shows the timestamp of the transmitted frame. The length, source MAC address and destination MAC address of the received frame will be print. The time stamp of the received timestamp will be print when the PTP message frame is received(the outside loopback cable can be used to see the right rx time-stamping log since we send the ptp message).
Supported Boards#
FRDM-MCXA577
Hardware requirements
Type-C USB cable
FRDM-MCXA577 board
Personal Computer
Loopback network cable RJ45 standard
Board settings
Short position 2-3 on J29.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The example uses external PHY over MII by default (ERR053383: A0 silicon has an ENET RMII RX issue). If you want to use the internal 10BASE-T1S digital PHY, redefine BOARD_NETWORK_USE_TENBASET_PHY from board.h to 1 and rebuild. Loopback cable is not needed in that case.
Note: In the default MII configuration the ENET TX bus uses P1_8/P1_9, which are the same pins as the MCU-Link VCOM debug console (LPUART1). Therefore this example routes its debug console to LPUART2 on the Arduino header (D1/TX = P2_10, D0/RX = P2_11) instead of the VCOM port. Connect an external USB-to-UART module to those Arduino-header pins (module RX to D1/P2_10, module TX to D0/P2_11, GND to GND) and open the serial terminal on that module’s COM port. When using the internal 10BASE-T1S PHY (BOARD_NETWORK_USE_TENBASET_PHY = 1), the console stays on the MCU-Link VCOM port.
Make loopback network cable:
Pin |
568B standard |
Unknown standard |
|---|---|---|
J1 |
orange+white |
green+white |
J2 |
orange |
green |
J3 |
green+white |
orange+white |
J4 |
blue |
brown+white |
J5 |
blue+white |
brown |
J6 |
green |
orange |
J7 |
brown+white |
blue |
J8 |
brown |
blue+white |
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not shown in the list, please connect J1~J8 based on your situation.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Get the 1-th time 0 second, 18208 nanosecond
Get the 2-th time 0 second, 199772858 nanosecond
Get the 3-th time 0 second, 399893806 nanosecond
Get the 4-th time 0 second, 600016650 nanosecond
Get the 5-th time 0 second, 800141079 nanosecond
Get the 6-th time 1 second, 276075 nanosecond
Get the 7-th time 1 second, 200136436 nanosecond
Get the 8-th time 1 second, 400272188 nanosecond
Get the 9-th time 1 second, 600404401 nanosecond
Get the 10-th time 1 second, 800540642 nanosecond
Transmission start now!
The 1 frame transmitted success!
the timestamp is 2 second, 3333631 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 3334569 nanosecond
The 2 frame transmitted success!
the timestamp is 2 second, 19654509 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 19655448 nanosecond
The 3 frame transmitted success!
the timestamp is 2 second, 36150233 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 36151172 nanosecond
The 4 frame transmitted success!
the timestamp is 2 second, 52657575 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 52658513 nanosecond
The 5 frame transmitted success!
the timestamp is 2 second, 69153651 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 69154590 nanosecond
The 6 frame transmitted success!
the timestamp is 2 second, 85660875 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 85661814 nanosecond
The 7 frame transmitted success!
the timestamp is 2 second, 102156951 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 102157890 nanosecond
The 8 frame transmitted success!
the timestamp is 2 second, 118851226 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 118852164 nanosecond
The 9 frame transmitted success!
the timestamp is 2 second, 135534234 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 135535173 nanosecond
The 10 frame transmitted success!
the timestamp is 2 second, 152227453 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 152228391 nanosecond
The 11 frame transmitted success!
the timestamp is 2 second, 169003400 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 169004339 nanosecond
The 12 frame transmitted success!
the timestamp is 2 second, 185790964 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 185791903 nanosecond
The 13 frame transmitted success!
the timestamp is 2 second, 202566442 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 202567381 nanosecond
The 14 frame transmitted success!
the timestamp is 2 second, 219353537 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 219354476 nanosecond
The 15 frame transmitted success!
the timestamp is 2 second, 236128898 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 236129837 nanosecond
The 16 frame transmitted success!
the timestamp is 2 second, 252915876 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 252916814 nanosecond
The 17 frame transmitted success!
the timestamp is 2 second, 269691588 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 269692527 nanosecond
The 18 frame transmitted success!
the timestamp is 2 second, 286478331 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 286479270 nanosecond
The 19 frame transmitted success!
the timestamp is 2 second, 303253457 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 303254396 nanosecond
The 20 frame transmitted success!
the timestamp is 2 second, 320040435 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 320041374 nanosecond
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Loopback network cable RJ45 standard
Board settings
Set JP13 2-3 on. Populate R274 to sync reference clock.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Make loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Get the 1-th time 0 second, 18208 nanosecond
Get the 2-th time 0 second, 199772858 nanosecond
Get the 3-th time 0 second, 399893806 nanosecond
Get the 4-th time 0 second, 600016650 nanosecond
Get the 5-th time 0 second, 800141079 nanosecond
Get the 6-th time 1 second, 276075 nanosecond
Get the 7-th time 1 second, 200136436 nanosecond
Get the 8-th time 1 second, 400272188 nanosecond
Get the 9-th time 1 second, 600404401 nanosecond
Get the 10-th time 1 second, 800540642 nanosecond
Transmission start now!
The 1 frame transmitted success!
the timestamp is 2 second, 3333631 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 3334569 nanosecond
The 2 frame transmitted success!
the timestamp is 2 second, 19654509 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 19655448 nanosecond
The 3 frame transmitted success!
the timestamp is 2 second, 36150233 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 36151172 nanosecond
The 4 frame transmitted success!
the timestamp is 2 second, 52657575 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 52658513 nanosecond
The 5 frame transmitted success!
the timestamp is 2 second, 69153651 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 69154590 nanosecond
The 6 frame transmitted success!
the timestamp is 2 second, 85660875 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 85661814 nanosecond
The 7 frame transmitted success!
the timestamp is 2 second, 102156951 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 102157890 nanosecond
The 8 frame transmitted success!
the timestamp is 2 second, 118851226 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 118852164 nanosecond
The 9 frame transmitted success!
the timestamp is 2 second, 135534234 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 135535173 nanosecond
The 10 frame transmitted success!
the timestamp is 2 second, 152227453 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 152228391 nanosecond
The 11 frame transmitted success!
the timestamp is 2 second, 169003400 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 169004339 nanosecond
The 12 frame transmitted success!
the timestamp is 2 second, 185790964 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 185791903 nanosecond
The 13 frame transmitted success!
the timestamp is 2 second, 202566442 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 202567381 nanosecond
The 14 frame transmitted success!
the timestamp is 2 second, 219353537 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 219354476 nanosecond
The 15 frame transmitted success!
the timestamp is 2 second, 236128898 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 236129837 nanosecond
The 16 frame transmitted success!
the timestamp is 2 second, 252915876 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 252916814 nanosecond
The 17 frame transmitted success!
the timestamp is 2 second, 269691588 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 269692527 nanosecond
The 18 frame transmitted success!
the timestamp is 2 second, 286478331 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 286479270 nanosecond
The 19 frame transmitted success!
the timestamp is 2 second, 303253457 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 303254396 nanosecond
The 20 frame transmitted success!
the timestamp is 2 second, 320040435 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 320041374 nanosecond
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T board
Personal Computer
Loopback network cable RJ45 standard
Board settings
Set JP13 2-3 on. Populate R274 to sync reference clock.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Make loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Get the 1-th time 0 second, 18208 nanosecond
Get the 2-th time 0 second, 199772858 nanosecond
Get the 3-th time 0 second, 399893806 nanosecond
Get the 4-th time 0 second, 600016650 nanosecond
Get the 5-th time 0 second, 800141079 nanosecond
Get the 6-th time 1 second, 276075 nanosecond
Get the 7-th time 1 second, 200136436 nanosecond
Get the 8-th time 1 second, 400272188 nanosecond
Get the 9-th time 1 second, 600404401 nanosecond
Get the 10-th time 1 second, 800540642 nanosecond
Transmission start now!
The 1 frame transmitted success!
the timestamp is 2 second, 3333631 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 3334569 nanosecond
The 2 frame transmitted success!
the timestamp is 2 second, 19654509 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 19655448 nanosecond
The 3 frame transmitted success!
the timestamp is 2 second, 36150233 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 36151172 nanosecond
The 4 frame transmitted success!
the timestamp is 2 second, 52657575 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 52658513 nanosecond
The 5 frame transmitted success!
the timestamp is 2 second, 69153651 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 69154590 nanosecond
The 6 frame transmitted success!
the timestamp is 2 second, 85660875 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 85661814 nanosecond
The 7 frame transmitted success!
the timestamp is 2 second, 102156951 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 102157890 nanosecond
The 8 frame transmitted success!
the timestamp is 2 second, 118851226 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 118852164 nanosecond
The 9 frame transmitted success!
the timestamp is 2 second, 135534234 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 135535173 nanosecond
The 10 frame transmitted success!
the timestamp is 2 second, 152227453 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 152228391 nanosecond
The 11 frame transmitted success!
the timestamp is 2 second, 169003400 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 169004339 nanosecond
The 12 frame transmitted success!
the timestamp is 2 second, 185790964 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 185791903 nanosecond
The 13 frame transmitted success!
the timestamp is 2 second, 202566442 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 202567381 nanosecond
The 14 frame transmitted success!
the timestamp is 2 second, 219353537 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 219354476 nanosecond
The 15 frame transmitted success!
the timestamp is 2 second, 236128898 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 236129837 nanosecond
The 16 frame transmitted success!
the timestamp is 2 second, 252915876 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 252916814 nanosecond
The 17 frame transmitted success!
the timestamp is 2 second, 269691588 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 269692527 nanosecond
The 18 frame transmitted success!
the timestamp is 2 second, 286478331 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 286479270 nanosecond
The 19 frame transmitted success!
the timestamp is 2 second, 303253457 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 303254396 nanosecond
The 20 frame transmitted success!
the timestamp is 2 second, 320040435 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 320041374 nanosecond
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
Loopback network cable RJ45 standard
Board settings
Set JP13 2-3 on. Populate R274 to sync reference clock.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Make loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Get the 1-th time 0 second, 18208 nanosecond
Get the 2-th time 0 second, 199772858 nanosecond
Get the 3-th time 0 second, 399893806 nanosecond
Get the 4-th time 0 second, 600016650 nanosecond
Get the 5-th time 0 second, 800141079 nanosecond
Get the 6-th time 1 second, 276075 nanosecond
Get the 7-th time 1 second, 200136436 nanosecond
Get the 8-th time 1 second, 400272188 nanosecond
Get the 9-th time 1 second, 600404401 nanosecond
Get the 10-th time 1 second, 800540642 nanosecond
Transmission start now!
The 1 frame transmitted success!
the timestamp is 2 second, 3333631 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 3334569 nanosecond
The 2 frame transmitted success!
the timestamp is 2 second, 19654509 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 19655448 nanosecond
The 3 frame transmitted success!
the timestamp is 2 second, 36150233 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 36151172 nanosecond
The 4 frame transmitted success!
the timestamp is 2 second, 52657575 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 52658513 nanosecond
The 5 frame transmitted success!
the timestamp is 2 second, 69153651 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 69154590 nanosecond
The 6 frame transmitted success!
the timestamp is 2 second, 85660875 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 85661814 nanosecond
The 7 frame transmitted success!
the timestamp is 2 second, 102156951 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 102157890 nanosecond
The 8 frame transmitted success!
the timestamp is 2 second, 118851226 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 118852164 nanosecond
The 9 frame transmitted success!
the timestamp is 2 second, 135534234 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 135535173 nanosecond
The 10 frame transmitted success!
the timestamp is 2 second, 152227453 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 152228391 nanosecond
The 11 frame transmitted success!
the timestamp is 2 second, 169003400 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 169004339 nanosecond
The 12 frame transmitted success!
the timestamp is 2 second, 185790964 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 185791903 nanosecond
The 13 frame transmitted success!
the timestamp is 2 second, 202566442 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 202567381 nanosecond
The 14 frame transmitted success!
the timestamp is 2 second, 219353537 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 219354476 nanosecond
The 15 frame transmitted success!
the timestamp is 2 second, 236128898 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 236129837 nanosecond
The 16 frame transmitted success!
the timestamp is 2 second, 252915876 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 252916814 nanosecond
The 17 frame transmitted success!
the timestamp is 2 second, 269691588 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 269692527 nanosecond
The 18 frame transmitted success!
the timestamp is 2 second, 286478331 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 286479270 nanosecond
The 19 frame transmitted success!
the timestamp is 2 second, 303253457 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 303254396 nanosecond
The 20 frame transmitted success!
the timestamp is 2 second, 320040435 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 320041374 nanosecond
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Loopback network cable RJ45 standard
Board settings
Set JP13 2-3 on. Populate R274 to sync reference clock.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Make loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Get the 1-th time 0 second, 18208 nanosecond
Get the 2-th time 0 second, 199772858 nanosecond
Get the 3-th time 0 second, 399893806 nanosecond
Get the 4-th time 0 second, 600016650 nanosecond
Get the 5-th time 0 second, 800141079 nanosecond
Get the 6-th time 1 second, 276075 nanosecond
Get the 7-th time 1 second, 200136436 nanosecond
Get the 8-th time 1 second, 400272188 nanosecond
Get the 9-th time 1 second, 600404401 nanosecond
Get the 10-th time 1 second, 800540642 nanosecond
Transmission start now!
The 1 frame transmitted success!
the timestamp is 2 second, 3333631 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 3334569 nanosecond
The 2 frame transmitted success!
the timestamp is 2 second, 19654509 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 19655448 nanosecond
The 3 frame transmitted success!
the timestamp is 2 second, 36150233 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 36151172 nanosecond
The 4 frame transmitted success!
the timestamp is 2 second, 52657575 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 52658513 nanosecond
The 5 frame transmitted success!
the timestamp is 2 second, 69153651 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 69154590 nanosecond
The 6 frame transmitted success!
the timestamp is 2 second, 85660875 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 85661814 nanosecond
The 7 frame transmitted success!
the timestamp is 2 second, 102156951 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 102157890 nanosecond
The 8 frame transmitted success!
the timestamp is 2 second, 118851226 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 118852164 nanosecond
The 9 frame transmitted success!
the timestamp is 2 second, 135534234 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 135535173 nanosecond
The 10 frame transmitted success!
the timestamp is 2 second, 152227453 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 152228391 nanosecond
The 11 frame transmitted success!
the timestamp is 2 second, 169003400 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 169004339 nanosecond
The 12 frame transmitted success!
the timestamp is 2 second, 185790964 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 185791903 nanosecond
The 13 frame transmitted success!
the timestamp is 2 second, 202566442 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 202567381 nanosecond
The 14 frame transmitted success!
the timestamp is 2 second, 219353537 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 219354476 nanosecond
The 15 frame transmitted success!
the timestamp is 2 second, 236128898 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 236129837 nanosecond
The 16 frame transmitted success!
the timestamp is 2 second, 252915876 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 252916814 nanosecond
The 17 frame transmitted success!
the timestamp is 2 second, 269691588 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 269692527 nanosecond
The 18 frame transmitted success!
the timestamp is 2 second, 286478331 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 286479270 nanosecond
The 19 frame transmitted success!
the timestamp is 2 second, 303253457 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 303254396 nanosecond
The 20 frame transmitted success!
the timestamp is 2 second, 320040435 nanosecond
One frame received. the length 1014
the timestamp is 2 second, 320041374 nanosecond