mcx_enet_txrx_transfer_rxpoll#
Overview#
The enet_rxtx_rxinterrupt example shows the simplest way to use ENET transactional tx/rx API for simple frame receive and transmit.
This example shows how to initialize the ENET.
How to use ENET to receive frame in polling and to transmit frame.
The example transmits 20 number broadcast frame, print the number and the mac address of the recieved frames.
Supported Boards#
FRDM-MCXA577
Hardware requirements
Type-C USB cable
FRDM-MCXA577 board
Personal Computer
Loopback network cable RJ45 standard
Board settings
The Ethernet uses the external PHY over the MII bus. Rework the following solder jumpers so the MII signals reach the PHY (this rework is not applicable to 10BASE-T1S mode):
Short 2-3 (and disconnect 1-2) of SJ13 (TXD2), SJ14 (TXD3), SJ16 (RXD2), SJ17 (RXD3), SJ18 (COL), SJ19 (CRS).
Disconnect 1-2 and 2-3 of SJ15 (RX_CLK) and SJ44 (RXER).
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The example uses external PHY over MII by default (ERR053383: A0 silicon has an ENET RMII RX issue). If you want to use the internal 10BASE-T1S digital PHY, redefine BOARD_NETWORK_USE_TENBASET_PHY from board.h to 1 and rebuild. Loopback cable is not needed in that case.
Note: In the default MII configuration the ENET TX bus uses P1_8/P1_9, which are the same pins as the MCU-Link VCOM debug console (LPUART1). Therefore this example routes its debug console to LPUART2 on the Arduino header (D1/TX = P2_10, D0/RX = P2_11) instead of the VCOM port. Connect an external USB-to-UART module to those Arduino-header pins (module RX to D1/P2_10, module TX to D0/P2_11, GND to GND) and open the serial terminal on that module’s COM port. When using the internal 10BASE-T1S PHY (BOARD_NETWORK_USE_TENBASET_PHY = 1), the console stays on the MCU-Link VCOM port.
Make loopback network cable:
Pin |
568B standard |
Unknown standard |
|---|---|---|
J1 |
orange+white |
green+white |
J2 |
orange |
green |
J3 |
green+white |
orange+white |
J4 |
blue |
brown+white |
J5 |
blue+white |
brown |
J6 |
green |
orange |
J7 |
brown+white |
blue |
J8 |
brown |
blue+white |
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not shown in the list, please connect J1~J8 based on your situation.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Transmission start now!
The 1 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 2 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 3 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 4 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 5 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 6 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 7 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 8 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 9 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 10 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 11 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 12 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 13 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 14 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 15 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 16 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 17 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 18 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 19 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 20 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
Optionally, you may use a loop back cable
Make a loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to the 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Set CONFIG_APP_USES_LOOPBACK_CABLE=y in .config (or add/change #define APP_USES_LOOPBACK_CABLE 1 in mcux_config.h if you don’t use Kconfig) and rebuild the example.
Insert loopback network cable to Ethernet RJ45 port.
Run the demo in the same way as described earlier.
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Loopback network cable RJ45 standard (optional)
Board settings
Set JP13 2-3 on. Populate R274 to sync reference clock.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Transmission start now!
The 1 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 2 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 3 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 4 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 5 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 6 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 7 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 8 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 9 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 10 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 11 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 12 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 13 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 14 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 15 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 16 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 17 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 18 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 19 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 20 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
Optionally, you may use a loop back cable
Make a loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to the 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Set CONFIG_APP_USES_LOOPBACK_CABLE=y in .config (or add/change #define APP_USES_LOOPBACK_CABLE 1 in mcux_config.h if you don’t use Kconfig) and rebuild the example.
Insert loopback network cable to Ethernet RJ45 port.
Run the demo in the same way as described earlier.
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T board
Personal Computer
Loopback network cable RJ45 standard (optional)
Board settings
Set JP13 2-3 on. Populate R274 to sync reference clock.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Transmission start now!
The 1 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 2 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 3 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 4 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 5 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 6 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 7 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 8 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 9 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 10 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 11 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 12 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 13 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 14 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 15 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 16 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 17 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 18 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 19 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 20 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
Optionally, you may use a loop back cable
Make a loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to the 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Set CONFIG_APP_USES_LOOPBACK_CABLE=y in .config (or add/change #define APP_USES_LOOPBACK_CABLE 1 in mcux_config.h if you don’t use Kconfig) and rebuild the example.
Insert loopback network cable to Ethernet RJ45 port.
Run the demo in the same way as described earlier.
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
Loopback network cable RJ45 standard (optional)
Board settings
Set JP13 2-3 on. Populate R274 to sync reference clock.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Transmission start now!
The 1 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 2 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 3 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 4 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 5 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 6 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 7 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 8 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 9 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 10 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 11 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 12 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 13 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 14 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 15 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 16 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 17 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 18 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 19 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 20 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
Optionally, you may use a loop back cable
Make a loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to the 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Set CONFIG_APP_USES_LOOPBACK_CABLE=y in .config (or add/change #define APP_USES_LOOPBACK_CABLE 1 in mcux_config.h if you don’t use Kconfig) and rebuild the example.
Insert loopback network cable to Ethernet RJ45 port.
Run the demo in the same way as described earlier.
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Loopback network cable RJ45 standard (optional)
Board settings
Set JP13 2-3 on. Populate R274 to sync reference clock.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
Transmission start now!
The 1 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 2 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 3 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 4 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 5 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 6 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 7 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 8 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 9 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 10 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 11 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 12 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 13 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 14 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 15 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 16 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 17 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 18 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 19 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 20 frame transmitted success!
One frame received. the length 1014
Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
Optionally, you may use a loop back cable
Make a loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to the 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Set CONFIG_APP_USES_LOOPBACK_CABLE=y in .config (or add/change #define APP_USES_LOOPBACK_CABLE 1 in mcux_config.h if you don’t use Kconfig) and rebuild the example.
Insert loopback network cable to Ethernet RJ45 port.
Run the demo in the same way as described earlier.