MCUXpresso SDK Documentation

qtmr_inputcapture_outputpwm_dma

qtmr_inputcapture_outputpwm_dma#

Overview#

The QTMR project is a demonstration program of the SDK QTMR driver’s input capture and output pwm feature by DMA. The example sets up a QTMR channel for input capture. Once the input signal is received, this example will print the capture value. The example also sets up one QTMR channel to output pwm. The example enables DMA and input edge flag setting will trigger DMA read request for CAPT register. The user should probe a 50Khz PWM signal output with 50% dutycycle with a oscilloscope. The user can enter a value to update the Duty cycle, when 5 is entered, the duty cycle will be set to 50%.

Supported Boards#

EVKB-IMXRT1050
Hardware requirements
  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

  • Oscilloscope

Board settings
  • Connect input signal to J23-6.

  • Use oscilloscope to measure output the signal pin at J23-5.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time = 1000 us (±5%)

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKB board

  • Personal Computer

  • Oscilloscope

Board settings
  • Connect input signal to J33-6.

  • Use oscilloscope to measure output the signal pin at J33-5.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time = 1000 us (±5%)

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

  • Oscilloscope

Board settings
  • Remove R414.

  • Connect input signal to J9-8.

  • Use oscilloscope to measure output the signal pin at J9-12.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Input Captured value=80c

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

  • Oscilloscope

Board settings
  • Connect input signal to J33-6.

  • Use oscilloscope to measure output the signal pin at J33-5.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time = 1000 us (±5%)

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
FRDM-IMXRT1152
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1152 board

  • Personal Computer

  • Oscilloscope

Board settings
  • Connect input signal to J10-8.

  • Use oscilloscope to measure output the signal pin at J10-10.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Input Captured value=80c

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
EVK-MIMXRT1015
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1015 board

  • Personal Computer

  • Oscilloscope

Board settings
  • Connect input signal to J17-2.

  • Use oscilloscope to measure output the signal pin at J17-1.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time = 1ms

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

Note:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
3. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
4. Start debugging in IDE.
   - Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.
EVK-MIMXRT1020
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1020 board

  • Personal Computer

  • Oscilloscope

Board settings
  • Connect input signal to J16-13.

  • Use oscilloscope to measure output the signal pin at J17-5.

  • Remove the R116 on the board when use pin J16-13 as input or output.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time = 1000 us (±5%)

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

Note:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
3. Start debugging in IDE.
   - Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.
MIMXRT1024-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1024-EVK board

  • Personal Computer

  • Oscilloscope

Board settings
  • Connect input signal to J55-6.

  • Use oscilloscope to measure output the signal pin at J17-10.

  • Remove the R116 on the board when use pin J55-6 as input or output.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time = 1000 us (±5%)

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

Note:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
3. Start debugging in IDE.
   - Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.
MIMXRT1040-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

  • Oscilloscope

Board settings
  • Connect input signal to J17-10.

  • Use oscilloscope to measure output the signal pin at J17-9.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time = 1000 us (±5%)

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
EVK-MIMXRT1064
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1064 board

  • Personal Computer

  • Oscilloscope

Board settings
  • Connect input signal to J23-6.

  • Use oscilloscope to measure output the signal pin at J23-5.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Input Captured value=80c

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MIMXRT1160-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

  • Oscilloscope

Board settings
  • Remove R414.

  • Connect input signal to J9-8.

  • Use oscilloscope to measure output the signal pin at J9-12.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Input Captured value=80c

****Output PWM dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MIMXRT1180-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

  • Oscilloscope

Board settings
  1. Input PWM signal to J45-15. PWM signal: 0-3.3V, default 1KHz.

  2. Use oscilloscope to monitor the signal at J45-13.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Press the reset button on your board to begin running the demo.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time=1000 us

****Output pwm dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50% duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
FRDM-IMXRT1186
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

  • Oscilloscope

Board settings
  1. Input PWM signal to J53-12. PWM signal: 0-3.3V, default 1KHz.

  2. Use oscilloscope to monitor the signal at J1-8.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Press the reset button on your board to begin running the demo.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time=1000 us

****Output pwm dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50% duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MIMXRT2660-EVK
Hardware requirements
  • Type-C USB cable

  • MIMXRT2660-EVK board

  • Personal Computer

  • Oscilloscope

Board settings
  1. Input capture: connect PWM signal (0-1.8V, 1 kHz) to J94-13 (PIO3_0). Signal path: PIO3_0 (GPIO1_GPIO0) -> GPIO1_TrigOut0 -> XBAR2 -> XBAR0 -> QTMR0_IN0.

  2. Output PWM: use oscilloscope to monitor J94-14 (PIO3_1). Signal path: QTMR0_OUT1 -> XBAR2 -> XBAR0 -> PIO3_1 (XBAR0_INOUT01, mux=A).

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Press the reset button on your board to begin running the demo.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

****Input capture dma example start.****

****Provide a signal input to the QTMR pin****

Captured Period time=1000 us

****Output pwm dma example.****

*********Make sure to connect an oscilloscope.*********

****A 50% duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:3
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~