sinc_adc#
Overview#
The sinc adc example shows how to use SINC driver to configure SINC module as single conversion mode to convert an external ADC sigma-delta modulator bitstream to a data stream. For this example, the over sample ratio is set as 128, the order is 3, and the SINC result data is signed. Theoretically, When ADCin = 0V, ADC output 50% duty of MBIT, sinc result is 0x0(If unsigned mode, sinc result is 128^3/2 = 0x10_0000); when ADCin = + maximum input voltage, ADC output always output 1(100% duty), SINC output is 128^3 = 0x20_0000. when ADCin = - maximum input voltage, ADC output always output 0(0% duty), SINC output is -128^3 = 0xE0_0000(If unsigned mode, sinc result is 0x0). For ADCin between -maximum input voltage and +maximum input voltage, the SINC result is ADCin/maximum * 0x20_0000.
Supported Boards#
MIMXRT1180-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings
Please check ADC chip(U45) on EVK board, if it is AMC1106M05 please connect TP41 to U45’s pin 7.
Connect input voltage to J49(If ADC chip is AMC1106M05, intput voltage ranges from -50mV to +50mV; If ADC chip is AD7402, input voltage ranges from -200mV to +200mV).
If using the AMC1106M05, note that a differential input of 50 mV will produce a stream of ones and zeros that are high 89.06% of the time, not 100%. So result can be verified based on equation: SINC result =(ADCin / 64mV) * (128^3 )
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the SINC ADC demo in the terminal window:
SINC ADC Example.
Press any key to trigger conversion!
Adc Result: 1193
MIMXRT2660-EVK
Hardware requirements
Type-C USB cable
MIMXRT2660-EVK board
Personal Computer
Board settings
connections required:
R328 1-3
R330 1-3
Connect differential input voltage to J99 (input range: -320mV ~ +320mV). note that a differential input of 50 mV will produce a stream of ones and zeros that are high 89.06% of the time, not 100%. So result can be verified based on equation: SINC result =(ADCin / 64mV) * (128^3 )
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Complete the wiring described in Board settings above.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
SINC ADC Example.
Press any key to trigger conversion!
Adc Result: 1193