MCUXpresso SDK Documentation

tpm_combine_pwm

tpm_combine_pwm#

Overview#

The TPM project is a demonstration program of generating a combined PWM signal by the SDK TPM driver. It sets up the TPM hardware block to output PWM signals(24kHZ) on two TPM channels. The example also show’s the complementary mode of operation and deadtime insertion. The PWM duty cycle is manually updated and is initially 10%. On boards that have 2 LEDs connected to the TPM pins, the user will see a change in LED brightness if user enter different values. And if the board do not support LEDs to show, the outputs can be observed by oscilloscope.

Supported Boards#

EVK9-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

  • Oscilloscope

Board settings

CM33: Connect J11-3 and J11-5(GND) to Oscilloscope

Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
IMX952LPD5EVK-19
Hardware requirements
  • Micro USB cable

  • IMX952-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings

CM7: Connect TP86 and (GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
EVK-MCIMX7ULP
Hardware requirements
  • Micro USB cable

  • MCIMX7ULP-EVK board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

  • Oscilloscope

Board settings

Connect TP86(PTB0) to Oscilloscope channel 1. Connect J9-4 to Oscilloscope channel 2. Please note both sides of R149 should be short-circuited.

Please note this application can’t support running with Linux BSP!

Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.

  2. Connect a micro USB cable between the host PC and the J6 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see information from the terminal as below.

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
EVK-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

  • Oscilloscope

Board settings

CM33: Connect J11-3 and J11-5(GND) to Oscilloscope

Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
FRDM-K32L2A4S
Hardware requirements
  • Mini/micro USB cable

  • FRDM-K32L2A4S board

  • Personal Computer

Board settings

This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see information from the terminal as below.

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

At this example you will see the changes of RGB led in brightness. the status of each led is opposite with another.

FRDM-K32L3A6
Hardware requirements
  • Mini/micro USB cable

  • FRDM-K32L3A6 board

  • Personal Computer

  • Oscilloscope

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see information from the terminal as below.

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

M0 core: Use oscilloscope to measure output signal pin at PTB13(J1-8),PTB14(J1-10) pin of FRDM-K32L3A6 board. M4 core: Use oscilloscope to measure output signal pin at PTB2(J2-2),PTB3(J2-4) pin of FRDM-K32L3A6 board.

FRDM-MCXW71
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW71 Board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
MCX-W71-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W71-EVK Board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
IMX95LPD5EVK-19
Hardware requirements
  • Micro USB cable

  • IMX95LPD5-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings

CM7: Connect R881 and (GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
FRDM-IMX95
Hardware requirements
  • Micro USB cable

  • FRDM-IMX95 board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings

CM7: Connect J19-32 and (GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
FRDM-IMX952
Hardware requirements
  • Micro USB cable

  • IMX952-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings

CM7: Connect GPIO_IO13(J18-33) and (GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
FRDM-IMX937
Hardware requirements
  • Micro USB cable

  • FRDM-IMX937 board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings

CM7: Connect GPIO_IO13(J18-33) and (GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
KW45B41Z-EVK
Hardware requirements
  • Mini/micro USB cable

  • KW45B41Z-EVK Board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
KW47-EVK
Hardware requirements
  • Type-C USB cable

  • KW47-EVK Board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
MCIMX93AUTO-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93AUTO-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings
  • CM33: connect J17-16(TPM2_CHN0), J17-29(GND) to Oscilloscope

  • CM33: connect J17-18(TPM2_CHN1), J17-29(GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J26 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
MCIMX93-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings
  • CM33: connect J1005-3(TPM2_CHN0), J1005-7(GND) to Oscilloscope

  • CM33: connect J1005-5(TPM2_CHN1), J1005-7(GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
MCIMX93W-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93W-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings
  • CM33: connect J1005-3(TPM2_CHN0), J1005-7(GND) to Oscilloscope

  • CM33: connect J1005-5(TPM2_CHN1), J1005-7(GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
MCIMX93-QSB
Hardware requirements
  • USB Type-C cable

  • MCIMX93-QSB board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings

CM33: Connect J1406-3 and J1406-7(GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1708 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
IMX943-EVK
Hardware requirements
  • Micro USB cable

  • IMX943-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

  • Oscilloscope

Board settings

Connect J47-6 and J47-14(GND) to Oscilloscope

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.

  2. Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
MCX-W72-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W72-EVK Board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
KW47-LOC
Hardware requirements
  • Type-C USB cable

  • KW47-LOC Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the host PC and the LOC board J3.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
MCXW72-LOC
Hardware requirements
  • Type-C USB cable

  • MCXW72-LOC Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the host PC and the LOC board J3.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
FRDM-MCXW72
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW72 Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
FRDM-KW43
Hardware requirements
  • Type-C USB cable

  • FRDM-KW43 Board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J28.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

Please monitor the PWM waveform on connector J19, pin 3 (PTB0) using an oscilloscope. Additionally, observe the blue LED for visual confirmation of the PWM signal.

FRDM-MCXW70
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW70 Board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J28.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

Please monitor the PWM waveform on connector J19, pin 3 (PTB0) using an oscilloscope. Additionally, observe the blue LED for visual confirmation of the PWM signal.