MCUXpresso SDK Documentation

Overview - ExecuTorch ModelRunner example project#

This example turns the board into a generic ExecuTorch model runner / benchmark tool: instead of hard-coding one model in firmware, the PC uploads any .pte model over UART at runtime, loads it with the ExecuTorch runtime, and runs inference on uploaded input tensors. Both pure-CPU models (portable kernels) and Neutron NPU models (delegate) are supported.

After each inference the board returns the raw output tensor bytes together with the inference time measured with the DWT cycle counter (pure inference time — UART transfer is not included), so the same firmware serves as a latency benchmark for any compatible model.

Serial protocol (binary, 115200 baud)#

Each frame is [0x55][0xAA][CMD][LEN:4B LE][PAYLOAD][CRC16:2B LE] (CRC-16/CCITT-FALSE over CMD+LEN+PAYLOAD). Commands:

Command

Payload

Response

LOAD_MODEL

raw .pte bytes

OK / ERROR

GET_INFO

-

input/output tensor specs (dtype/shape/dim_order/nbytes)

LOAD_INPUT

raw input tensor bytes

OK / ERROR

RUN

-

RESULT: timing_us (u64 LE) + raw output tensor bytes

The layout is implemented in protocol.h (frame and error codes) and executorch_engine.cpp (INFO / RESULT payload serialization); the Python implementation is scripts/run.py. Error frames carry a 1-byte code (see protocol.h), e.g. 0x03 model too big, 0x14 missing operator registration.

PC-side tool: scripts/run.py#

run.py implements the frame codec and provides both an interactive shell and a one-shot mode. It needs pyserial:

pip install -r scripts/requirements.txt

Interactive shell#

python scripts/run.py --port /dev/ttyACM0 --baud 115200
(modelrunner|no model)> model cifarnet_int8.pte
  >> uploading model cifarnet_int8.pte (111240 bytes)
  [OK] model upload success (111240 bytes)

  model spec:
    inputs : 1
      [0] dtype=Char shape=[1, 3, 32, 32] dim_order=[0, 2, 3, 1] nbytes=3072
    outputs: 1
      [0] dtype=Char shape=[1, 10] nbytes=10

(modelrunner|model loaded)> input img0.bin
  >> uploading input img0.bin (3072 bytes)
  [OK] input upload success (3072 bytes)

(modelrunner|input ready)> run
  >> running inference...
  [OK] inference time: 848 us

  output[0]: dtype=Char shape=[1, 10]
    values: [-128, -128, -128, 127, ...]

Commands: model <file> load a .pte, input <file> load an input tensor, info re-query the model spec, run run inference, status, reconnect [<port>], help, quit.

One-shot mode (script friendly)#

With the model (and optionally an input) given as positional arguments the tool runs once and exits; the exit code reflects success (0) or failure (1). It prints the inference time plus the raw output tensor values:

python scripts/run.py --port /dev/ttyACM0 model.pte input.bin

Input tensor files#

.bin inputs are header-less raw dumps of the model’s input tensor: the byte count must equal the input spec reported by GET_INFO (nbytes), and the data must already match the model’s dtype, shape, memory layout (dim_order) and quantization — the board copies the bytes straight into the input tensor with no preprocessing. For quantized models the quantization parameters can be read from the GET_INFO spec.

Model placement: SRAM vs PSRAM#

Models up to 384 KB are received into an on-chip NonCacheable SRAM buffer and run entirely from SRAM — the fastest path, since the Neutron NPU reads the weights directly. Larger models are streamed into the board’s XSPI2 HyperRAM (PSRAM, 16 MB model window at 0x60000000) and parsed in place; only weight segments are copied into SRAM while the model runs.

NPU models that live in PSRAM MUST be converted with the Neutron compiler option --fetch_constants_to_sram: the Neutron NPU cannot read PSRAM directly, so the compiler emits microcode that prefetches each layer’s weights from PSRAM into an SRAM scratch buffer while the previous layer is computing. A PSRAM-resident NPU model converted without this option still loads, but the NPU cannot reach its weights and inference produces garbage. CPU-only (portable-kernel) models have no such requirement — the CPU reads PSRAM through the XSPI2 AHB window like ordinary memory.

The SRAM/PSRAM switchover threshold (384 KB by default) can be overridden at build time by adding -DPTE_SRAM_THRESHOLD=65536 to the compiler flags in the board reconfig (_boards/<board>/eiq_examples/executorch_modelrunner/cm33_core0/reconfig.cmake), e.g. to force the PSRAM path for a small model while testing.

Kernel registry#

RegisterKernels.cpp is a hand-written registration table (the generated “Everything” table does not link against the shipped libexecutorch.a). It covers the op set of common vision and keyword-spotting models; when a new .pte reports load error 0x14 (load_method), diff its operators against this table (strings -n 2 <model>.pte shows the operator names) and add the missing entries, following the unboxing pattern of the existing entries.

Build#

Currently supported board: MIMXRT700-EVK (CM33 core0). From the SDK root (with west and the GNU Arm toolchain in PATH):

west build -p always -b mimxrt700evk examples/eiq_examples/executorch_modelrunner --toolchain armgcc -Dcore_id=cm33_core0 --config flash_release -d build_dir

The resulting firmware is build_dir/executorch_modelrunner_cm33_core0.elf.