tflm_kws#
Overview#
This is a keyword spotting example based on the Keyword spotting for Microcontrollers (ARM-software/ML-KWS-for-MCU) project. It demonstrates how to run a TensorFlow Lite Micro model on NXP MCUs for audio keyword detection.
In this example, static audio samples (“off”, “right”) are evaluated for classification into one of 12 keyword classes.
Key Features#
Model Architecture: Depthwise Separable Convolutional Neural Network (DS-CNN) based on MobileNet
Input: 1-second audio sample (pre-processed to MFCC spectrogram: 49×10 matrix)
Output: Classification into 12 classes (silence, unknown, yes, no, up, down, left, right, on, off, stop, go)
Detection Threshold: 95%
Audio Preprocessing: 40 ms sliding window with 20 ms stride, FFT-based MFCC feature extraction (10 coefficients)
Neutron Software Version: MCU SDK 26.09.00 comes with a default Neutron Software Version of 3.2.2
Input Data Preprocessing#
Raw audio data is pre-processed by calculating a spectrogram:
A 40 ms window slides over a one-second audio sample with a 20 ms stride
For each window, audio frequency strengths are computed using FFT
The results are transformed into Mel-Frequency Cepstral Coefficients (MFCC)
Only the first 10 coefficients are taken into account
The window slides over a sample 49 times, creating a matrix with 49 rows and 10 columns
Classification#
The spectrogram is fed into a neural network for classification:
The neural network is a depthwise separable convolutional neural network based on MobileNet (MobileNets: Efficient Convolutional Neural Networks for Mobile Vision Applications)
The model produces a probability vector for the following 12 classes:
“Silence”
“Unknown”
“yes”, “no”, “up”, “down”, “left”, “right”
“on”, “off”
“stop”, “go”
Quantization#
The neural network model is quantized to optimize performance on MCUs:
The model takes quantized input and produces quantized output
Input spectrogram scaling: from range
[-247, 30]to range[0, 255], rounded to integersValues lower than zero are set to zero
Values exceeding 255 are set to 255
Output: a vector with components in the interval
(0, 255)that add up to 255
Model Source#
The pre-trained model is sourced from:
https://github.com/ARM-software/ML-KWS-for-MCU/blob/master/Pretrained_models/DS_CNN/DS_CNN_S.pb
For details on model quantization and conversion, refer to the eIQ TensorFlow Lite User’s Guide included in the MCUXpresso SDK package.
Audio Data Source#
The static audio samples are from the Speech Commands Dataset:
https://storage.cloud.google.com/download.tensorflow.org/data/speech_commands_v0.02.tar.gz
speech_commands_test_set_v0.02/off/0ba018fc_nohash_2.wavspeech_commands_test_set_v0.02/right/0a2b400e_nohash_1.wav
Audio Data Conversion#
Waveform files can be converted to C arrays using Python with Scipy:
from scipy.io import wavfile
rate, data = wavfile.read('yes.wav')
with open('wav_data.h', 'w') as fout:
print('#define WAVE_DATA {', file=fout)
data.tofile(fout, ',', '%d')
print('}\n', file=fout)
Project Files#
File/Directory |
Description |
|---|---|
|
Example main function |
|
Waveform audio file for the word “off” |
|
Waveform audio file for the word “right” |
|
Waveform audio files converted to C language array |
|
Model training script based on TensorFlow audio tutorial |
|
Timer source code |
|
Audio capture and pre-processing code |
|
MFCC feature extraction matching TensorFlow MFCC operation |
|
Audio buffer handling for MFCC feature extraction |
|
Top results retrieval |
|
Model data converted to C language array |
|
NPU TensorFlow Lite model |
|
Model initialization and inference code |
|
Model operations registration |
|
Model output processing |
Project Structure in MCU SDK#
Only primary files are listed here:
Path_to_MCUSDK/mcuxsdk/examples/
├── eiq_examples/
│ ├── common/
│ │ └── audio/*
│ └── tflm_kws/
│ ├── CMakeLists.txt
│ ├── audio_data.h
│ ├── demo_config.h
│ ├── dsp
│ │ └── main.c
│ ├── labels.h
│ ├── main.cpp
│ ├── off.wav
│ ├── output_postproc.cpp
│ ├── readme.md
│ └── train.py
└── _boards/
└── <board_name>/
└── eiq_examples/
└── tflm_kws/
├── example_board_readme.md
├── npu # NPU version of the model files
│ ├── ds_cnn_s_npu.tflite
│ ├── model_data.h
│ └── model_ds_cnn_ops_npu.cpp
└── reconfig.cmake
(For the boards without NPU hardware, the CPU version of the model files is located in the cpu/ folder.)
Project Structure in IDE#
(1) Project Structure in MCUXpresso IDE
Only primary files are listed here:
.
├── eiq
│ ├── neutron # Neutron-Software files
│ │ ├── common
│ │ │ └── include
│ │ │ └── NeutronErrors.h
│ │ ├── driver
│ │ │ └── include
│ │ │ └── NeutronDriver.h
│ │ └── rt700
│ │ └── cm33
│ │ ├── libNeutronDriver.a
│ │ └── libNeutronFirmware.a
│ └── tensorflow-lite/
├── source
│ ├── audio/
│ ├── board_init.h
│ ├── demo_info.cpp
│ ├── demo_info.h
│ ├── labels.h
│ ├── main.cpp
│ ├── mcux_config.h
│ ├── mcuxsdk_version.h
│ ├── model
│ │ ├── get_top_n.cpp
│ │ ├── get_top_n.h
│ │ ├── model.cpp
│ │ ├── model.h
│ │ ├── model_data.h # Model data file
│ │ ├── model_ds_cnn_ops_npu.cpp
│ │ └── output_postproc.h
│ ├── output_postproc.cpp
│ ├── pmic_support.c
│ ├── pmic_support.h
│ ├── semihost_hardfault.c
│ ├── timer.c
│ ├── timer.h
│ └── train.py
└── doc/ # Documentation
└── readme.md
The library files and header files in the eiq/neutron/ folder are Neutron-Software related files.
Users can update the Neutron-Software version in this project by replacing these four files in the eiq/neutron/ folder: NeutronDriver.h, NeutronErrors.h, libNeutronDriver.a, and libNeutronFirmware.a.
(2) Project Structure in MCUXpresso for VScode
Please select the following two options in the MCUXpresso for VS Code extension settings:
[✓] Mcuxpresso > Experimental: Enable Add Files To Project
[✓] Mcuxpresso > Experimental: Enable Freestanding Copy Board
After importing a Freestanding project from the MCU SDK, the project structure is as follows (only primary files are listed here):
.
├── CMakeLists.txt
├── audio/*
├── audio_data.h
├── common
│ ├── timer.c
│ ├── timer.h
│ └── timer_xtensa.h
├── labels.h
├── main.cpp
├── model
│ ├── get_top_n.cpp
│ ├── get_top_n.h
│ ├── model.h
│ └── output_postproc.h
├── npu # NPU version of the model files
│ ├── ds_cnn_s_npu.tflite
│ ├── model_data.h # Model data file
│ └── model_ds_cnn_ops_npu.cpp
├── <board_name_folder> (e.g. mimxrt700evk_cm33_core0)
│ └── middleware_eiq_neutron # Neutron-Software files
│ ├── NeutronDriver.h
│ ├── NeutronErrors.h
│ └── cm33
│ ├── libNeutronDriver.a
│ └── libNeutronFirmware.a
├── off.wav
├── output_postproc.cpp
└── train.py
For the boards with NPU hardware, the NPU model file is located in the npu/ folder. (For the boards without NPU hardware, the CPU version of the model file is located in the cpu/ folder.)
The header files and library files in the <board_name_folder>/middleware_eiq_neutron folder are Neutron-Software related files.
Users can update the Neutron-Software version in this project by replacing these four files: NeutronDriver.h, NeutronErrors.h, libNeutronDriver.a, and libNeutronFirmware.a.
Replace the model file#
If you need to replace the model file with your own model, please follow two main steps:
Step 1: Modify the
model_data.hfile.Step 2: Modify the
model_ds_cnn_ops_npu.cppfile.
Step 1: Modify the model_data.h file.#
(1) Use NPU model
For NPU boards, you can use the Neutron Converter tool to convert your .tflite model into an NPU-optimized version, which simultaneously generates an NPU-specific .tflite file and a corresponding .h header file.
You can obtain the Neutron Converter tool from the eIQ Neutron SDK.
After downloading and extracting the Neutron SDK Zip package, you can find the Neutron Converter tool at the following path:
/eiq-neutron-sdk-linux-x.x.x/bin/neutron-converter.
# Set environment variables
export NEUTRON_SDK_PATH="/path/to/eiq-neutron-sdk-linux-x.x.x"
export LD_LIBRARY_PATH="${NEUTRON_SDK_PATH}/lib:${LD_LIBRARY_PATH}"
export PATH="${NEUTRON_SDK_PATH}/bin:${PATH}"
# Convert for mcxn94x target
neutron-converter --input model_name.tflite --output model_name_mcxn94x.tflite --target mcxn94x --dump-header-file-output
# Convert for imxrt700 target
neutron-converter --input model_name.tflite --output model_name_rt700.tflite --target imxrt700 --dump-header-file-output
Neutron Converter Target Platforms:
Target |
Description |
Boards |
|---|---|---|
|
MCXN94x series |
frdmmcxn947, mcxn5xxevk, mcxn9xxevk |
|
i.MX RT700 series |
mimxrt700evk |
Modify the model_data.h file in the project:
Replace the original model data with
model_dataarray andmodel_data_lenfrom your model’s.hfile.Refer to the “Total data” value for graph “main” shown in the terminal output of neutron converter, and adjust the
kTensorArenaSizevalue in themodel_data.hfile accordingly. Typically,kTensorArenaSizeshould be set to 105% or more of the “Total data” value.
# Example terminal output from neutron converter:
# The "Total data" value for graph "main" is 16,512 (bytes), so the kTensorArenaSize should be set to about 17,338 (bytes) (16,512 * 1.05)
Overall statistics for graph "main":
Operators:
...<operator details>...
Memory:
Total data = 16,512 (bytes) (Inputs + Outputs + Intermediate Variable Tensors)
Total weights = 30,400 (bytes) (Weights)
Total size = 46,912 (bytes) (All)
// Modify the model_data.h file:
constexpr int kTensorArenaSize = <Total data * 1.05>; // TensorArenaSize in (bytes)
static const uint8_t model_data[] __ALIGNED(16) __PLACEMENT = {
...<your model array>...
}
static const unsigned int model_data_len = <your model length>;
If the following error occurs while running the example, it is caused by the kTensorArenaSize being too small. Please increase the kTensorArenaSize accordingly.
Failed to resize buffer. Requested:16544, available 15928, missing:616
AllocateTensors() failed
(2) Use CPU model
You can use the following workflow to run a CPU-version model in this example.
The xxd tool can convert your .tflite model file into a .h header file. The command is as follows:
xxd -i model_name.tflite > model_name.h
Or you can also use Neutron Converter (Recommend) to generate the .h file by using the --dump-header-file-input option. This will convert your input CPU-version .tflite model into a CPU-version .h file.
neutron-converter --input model_name.tflite --output model_name_imxrt700.tflite --target imxrt700 --dump-header-file-input
Modify the model_data.h file in the project: replace the original model data with model_data array and model_data_len from your model’s .h file.
# Modify the model_data.h file:
static const uint8_t model_data[] __ALIGNED(16) __PLACEMENT = {
...<your model array>...
}
static const unsigned int model_data_len = <your model length>;
Step 2: Modify the model_ds_cnn_ops_npu.cpp file.#
In step 2, you need to refer to the .h file generated by the Neutron Converter in step 1 and modify the model operators in the model_ds_cnn_ops_npu.cpp file.
Typically, the .h file output by the Neutron Converter contains content similar to the following:
/*
// Register operators for TFLite Micro.
static tflite::MicroMutableOpResolver<4> s_microOpResolver;
s_microOpResolver.AddQuantize();
s_microOpResolver.AddSoftmax();
s_microOpResolver.AddDequantize();
s_microOpResolver.AddCustom(tflite::GetString_NEUTRON_GRAPH(), tflite::Register_NEUTRON_GRAPH());
*/
Copy the operator registration code from the .h file generated by the Neutron Converter into the model_ds_cnn_ops_npu.cpp file.
Running the Demo#
Run result on MIMXRT700-EVK board with ARM GCC toolchain (NPU version):
Keyword spotting example using a TensorFlow Lite Micro model.
Detection threshold: 95%
Model: ds_cnn_s_npu
Core/NPU Frequency: 324 MHz
TensorArena Addr: 0x20000000 - 0x20020000
TensorArena Size: Total 0x20000 (131072 B); Used 0x4390 (17296 B)
Model Addr: 0x20400000 - 0x20407d50
Model Size: 0x7d50 (32080 B)
Total Size Used: 49376 B (Model (32080 B) + TensorArena (17296 B))
Static data processing:
----------------------------------------
Inference time: 595 us
Detected: off (99%)
----------------------------------------
----------------------------------------
Inference time: 576 us
Detected: right (99%)
----------------------------------------
Supported Boards with NPU#
FRDM-IMXRT1152
MIMXRT1180-EVK
EVKB-IMXRT1050
MIMXRT1040-EVK
FRDM-IMXRT1186
MIMXRT1060-EVKC
MIMXRT1060-EVKB
MIMXRT1170-EVKB
EVK-MIMXRT1064
MIMXRT1160-EVK
Supported Boards with CPU Only#
MIMXRT1040-EVK
EVKB-IMXRT1050
MIMXRT1060-EVKB
MIMXRT1060-EVKC
EVK-MIMXRT1064
MIMXRT1160-EVK
MIMXRT1170-EVKB
MIMXRT1180-EVK
FRDM-IMXRT1186
EVK-MIMXRT595
EVK-MIMXRT685
MIMXRT685-AUD-EVK