lwip_httpsrv_freertos#
Overview#
The lwip_httpsrv_freertos demo application demonstrates an HTTP server on the lwIP TCP/IP stack with FreeRTOS. The user uses an internet browser to send a request for connection. The board acts as an HTTP server and sends a web page back to the PC.
The example supports both IPv4 and IPv6 protocols. But some combinations of boards or build configurations may have only IPv4 enabled due to memory constraints. If it fits into memory, it is possible for the example to be compiled with both IPv4 and IPv6 (LWIP_IPV4=1 and LWIP_IPV6=1 in lwipopts.h), IPv4 only (LWIP_IPV4=1 and LWIP_IPV6=0 in lwipopts.h) or IPv6 only (LWIP_IPV4=0 and LWIP_IPV6=1 in lwipopts.h). If IPv6 is enabled, the board will assign a link-local IPv6 address to its interface, but this is often not enough as web browsers tend to not support link-local address with zone index in URL (e.g. http://[FE80::5627:8DFF:FE46:29F8%eth0]). So if the board is connected directly to the host PC, the PC should be configured to send ICMPv6 Router Advertisement messages with Prefix option, which the board could use to assign itself a routable address using the Stateless Address Autoconfiguration mechanism. If the board and the host PC are connected through a router, sending of Router Advertisement messages could be configured on that router (if it supports IPv6). Instructions how to set the IPv6 network correctly can be different on each system and it is out of scope of this readme. It can take a couple of seconds until the addresses are validated and assigned to the board’s ethernet interface, so the board will print “IPv6 address update” messages followed by all valid IPv6 addresses anytime there is a change. The assigned unique local or global unique addresses could be typed into the web browser’s address bar in a form like “http://[FD00:AABB:CCDD:EEFF:5627:8DFF:FE46:29F8]” to access the web server over IPv6.
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA(or USB to Serial) USB port on the target board.
Open a serial terminal on PC for OpenSDA serial(or USB to Serial) device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert the Ethernet Cable into the target board’s RJ45 port and connect it to your PC network adapter.
Configure the host PC IP address to 192.168.0.100.
Configure the host PC to advertise IPv6 address prefix.
Open a web browser.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, the terminal will display the following: Initializing PHY…
*********************************************************** HTTP Server example *********************************************************** IPv4 Address : 192.168.0.102 IPv4 Subnet mask : 255.255.255.0 IPv4 Gateway : 192.168.0.100 IPv6 Address0 : - IPv6 Address1 : - IPv6 Address2 : - mDNS hostname : lwip-http *********************************************************** IPv6 address update, valid addresses: IPv6 Address0 : FE80::5627:8DFF:FE46:29F8 IPv6 Address1 : - IPv6 Address2 : - IPv6 address update, valid addresses: IPv6 Address0 : FE80::5627:8DFF:FE46:29F8 IPv6 Address1 : FD00:AABB:CCDD:EEFF:5627:8DFF:FE46:29F8 IPv6 Address2 : -
If the example has been compiled with IPv4 enabled (LWIP_IPV4=1), type 192.168.0.102 (IP address of the board) into the browser address bar. The browser should show a web page. The board also advertises itself using mDNS so that it can be accessed using URL http://lwip-http.local. Please note that your system may not support mDNS out-of-the-box as it is necessary to have an mDNS resolver installed. For instance Bonjour Print Services for Windows contain such resolver. In case of Linux nss-mdns serves this purpose. Username admin and password admin is required to access “Authorization example” section of the web page.
If the example has been compiled with IPv6 enabled (LWIP_IPV6=1), wait for the unique local or global unique IPv6 address to appear in the list of valid addresses in the console output. Then the server could be reached over IPv6. For the example output above, http://[FD00:AABB:CCDD:EEFF:5627:8DFF:FE46:29F8] could be typed into the browser’s address bar to make it show the web page and communicate with the board over IPv6.
If the example has been compiled with IPv6 only and no IPv4 (LWIP_IPV6=1 and LWIP_IPV4=0), the board will still have the mDNS responder enabled. But some web browsers seem to send mDNS queries for IPv4 address only, so it might not be possible to access the board using http://lwip-http.local URL. Still, some utilities (like avahi-resolve on Linux) could be used to resolve the name to IPv6 address using mDNS.
Modifying content of static web pages#
To modify content available through the web server you must complete following steps:
Modify, add or delete files in folder “boards/<board_name>/lwip_examples/lwip_httpsrv_freertos/webpage”.
Run the script file “middleware/lwip/src/apps/httpsrv/mkfs/mkfs.pl <directory name>” to generate new “httpsrv_fs_data.c”. Make sure to execute it from a folder where the file “httpsrv_fs_data.c” is. For example:
C:\sdk\boards\<board_name>\lwip_examples\lwip_httpsrv_freertos> C:\sdk\middleware\lwip\src\apps\httpsrv\mkfs\mkfs.pl webpage Processing file webpage/auth.html Processing file webpage/cgi.html Processing file webpage/favicon.ico Processing file webpage/help.html Processing file webpage/httpsrv.css Processing file webpage/index.html Processing file webpage/NXP_logo.png Processing file webpage/poll.html Processing file webpage/request.js Processing file webpage/ssi.shtml Processing file webpage/welcome.html Done.
Make sure the “httpsrv_fs_data.c” file has been overwritten with the newly generated content.
Re-compile the HTTP server application example and download it to your board.
Supported Boards#
EVKB-IMXRT1050
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
EVKB-IMXRT1050 board
Personal Computer
Board settings
No special settings are required.
MIMXRT1060-EVKB
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
MIMXRT1060-EVKB board
Personal Computer
Board settings
No special settings are required.
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
MIMXRT1170-EVKB board
Personal Computer
Board settings
This example uses 1G port(J4) as default. If want to test 100M port(J3), please set the macro BOARD_NETWORK_USE_100M_ENET_PORT to 1.
MIMXRT1060-EVKC
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
MIMXRT1060-EVKC board
Personal Computer
Board settings
No special settings are required.
FRDM-IMXRT1152
Hardware requirements
FRDM-IMXRT1152 board
USB Type-C cable
RJ45 network cable
Personal Computer
Board settings
Connect the USB Type-C cable to the FRDM-IMXRT1152 USB debug connector.
Use the Gigabit Ethernet RJ45 port (J45).
Set JP2 to position 1-2.
EVK-MIMXRT1020
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
EVK-MIMXRT1020 board
Personal Computer
Board settings
No special settings are required.
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
MIMXRT1024-EVK
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
MIMXRT1024-EVK board
Personal Computer
Board settings
No special settings are required.
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
MIMXRT1040-EVK
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
MIMXRT1040-EVK board
Personal Computer
Board settings
No special settings are required.
EVK-MIMXRT1064
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
EVK-MIMXRT1064 board
Personal Computer
Board settings
No special settings are required.
MIMXRT1160-EVK
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
MIMXRT1160-EVK board
Personal Computer
Board settings
This example uses 1G port(J4) as default. If want to test 100M port(J3), please set the macro BOARD_NETWORK_USE_100M_ENET_PORT to 1.
MIMXRT1180-EVK
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
MIMXRT1180-EVK board
Personal Computer
Board settings
This example uses Ethernet RJ45 port J32.
FRDM-MCXA577
Hardware requirements
Type-C USB cable
RJ45 Network cable (for 100BASE-TX mode)
10BASE-T1S network adapter and cable (optional for 10BASE-T1S mode)
FRDM-MCXA577 board
Personal Computer
Board settings
Short position 2-3 on J29.
Note: In the default MII configuration the debug console is on LPUART2 (Arduino header: D1/TX = P2_10, D0/RX = P2_11), because MII uses the VCOM pins P1_8/P1_9. Attach an external USB-to-UART module (115200-8-N-1). With the internal 10BASE-T1S PHY the console stays on VCOM.
Use with 10BASE-T1S Ethernet
The example uses 100BASE-TX Ethernet over RJ45 by default. If you want to use the internal 10BASE-T1S digital PHY, redefine BOARD_NETWORK_USE_TENBASET_PHY from board.h to 1 and rebuild. Connect to a PC with a 10BASE-T1S network adapter instead of RJ45 and enable PLCA on a PC with the following parameters: - node ID: 0 (PLCA coordinator) - node count: 8 - TO timer: 32 BT - burst count: 0 - burst timer: 128 BT
FRDM-MCXE247
Hardware requirements
USB-C cable
Network cable RJ45 standard
FRDM-MCXE247 board
Personal Computer
Board settings
No special settings are required.
FRDM-MCXN947
Hardware requirements
Type-C USB cable
RJ45 Network cable
FRDM-MCXN947 board
Personal Computer
Board settings
Connect JP13 2-3 pin. Populate R274 to sync reference clock.
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
RJ45 Network cable
FRDM-MCXN947T board
Personal Computer
Board settings
Connect JP13 2-3 pin. Populate R274 to sync reference clock.
FRDM-RW612
Hardware requirements
USB-C cable
Network cable RJ45 standard
FRDM-RW612 board
Personal Computer
Board settings
Make sure SJ21 and SJ22 have positions 1 and 2 soldered (default).
LPCXpresso54628
Hardware requirements
Mini/micro USB cable
RJ45 Network cable
LPCXpresso54628 board
Personal Computer
Board settings
For LPCXpresso54628 V2.0:JP11 and JP12 1-2 on.
LPCXpresso54S018
Hardware requirements
Mini/micro USB cable
RJ45 Network cable
LPCXpresso54S018 board
Personal Computer
Board settings
LPCXpresso54S018M
Hardware requirements
Mini/micro USB cable
RJ45 Network cable
LPCXpresso54S018M board
Personal Computer
Board settings
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
RJ45 Network cable
MCX-N5XX-EVK board
Personal Computer
Board settings
Connect JP13 2-3 pin. Populate R274 to sync reference clock.
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
RJ45 Network cable
MCX-N9XX-EVK board
Personal Computer
Board settings
Connect JP13 2-3 pin. Populate R274 to sync reference clock.
RD-RW612-BGA
Hardware requirements
Micro USB cable
Network cable RJ45 standard
RD-RW612-BGA board
Personal Computer
Board settings
Connect JP54. Load R520, R508, R505 Remove R518, R507, R506
IMX943-ORANGEBOX
Hardware requirements
Micro USB cable
IMX943-ORANGEBOX board
12V~20V power supply
Personal Computer
Board settings
This example uses NETC ENETC0 1G port in default. To choose other port, configure in lwip_netc_port.h.
FRDM-IMXRT1186
Hardware requirements
Type-C USB cable
Network cable RJ45 standard
FRDM-IMXRT1186 board
Personal Computer
Board settings
Short jumpers J12 (1-2) and J13 (2-3) and connect network cable to J56A.
IMX943-EVK
Hardware requirements
Micro USB cable
IMX943-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
This example uses NETC ENETC0 (ETH2/J25) 1G port in default. To choose other port, configure in lwip_netc_port.h.
MIMXRT2660-EVK
Hardware requirements
USB Type-C cable for debug console
Network cable RJ45 standard
MIMXRT2660-EVK board
Personal Computer
Board settings
This example uses the on-board COMM_ENET port (gigabit YT8531 PHY, RGMII), which terminates at RJ45 port J71. No board rework or jumper action is required for COMM_ENET.
10BASE-T1S PHY support
This example supports the internal 10BASE-T1S PHY (TENBASET_PHY) as an alternative to the external RGMII PHY. To enable, define in board.h:
#define BOARD_NETWORK_USE_TENBASET_PHY (1U)
Hardware setup for 10BASE-T1S mode:
Set jumper J52 to position 1-2 to route the board analog mux to the T1S PHY.
Attach the T1S link to RJ45 port J47 (the T1S connector dedicated to COMM_ENET on this EVK).
Hardware setup for RGMII mode (default):
Use RJ45 port J71 for the RGMII link (no jumper action required for COMM_ENET).