rpmsg_lite_pingpong_rtos#
Overview#
The Multicore RPMsg-Lite pingpong FreeRTOS project is a simple demonstration program that uses the MCUXpresso SDK software and the RPMsg-Lite library and shows how to implement the inter-core communication between cores of the multicore system.
The primary core releases the secondary core from the reset and then the inter-core communication is established.
Once the RPMsg is initialized and endpoints are created the message exchange starts, incrementing a virtual counter that is part of the message payload.
The message pingpong finishes when the counter reaches the value of 100. Then the RPMsg-Lite is deinitialized and the procedure of the data exchange is repeated again.
Building the application#
This shows example how to build application for evkbmimxrt1170 board with cm7 core_id.
Change the -b <board> parameter based on board you want to build.
Change the -Dcore_id=<core_id> parameter based on board core you want to build.
For these parameters please see attribute boards: in primary/example.yml.
west build --sysbuild examples/multicore_examples/rpmsg_lite_pingpong_rtos/primary --toolchain armgcc --config debug -b evkbmimxrt1170 -Dcore_id=cm7
Supported Boards#
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Copy CORE1 image to address: 0x20200000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
Note: To download and debug IAR EW project using J-Link (replacing the default CMSIS-DAP debug probe), following steps are needed:
Remove J6 and J7 jumpers.
Attach the J-Link probe (J-Link Plus / J-Trace) to the board using the J1 connector.
Set “J-Link / J-Trace” in CM7 project options -> Debugger -> Setup panel (replacing CMSIS-DAP option).
Unselect the “Use macro file(s)” in CM7 project options -> Debugger -> Setup panel.
Enable “Use command line options” in CM7 project options -> Debugger -> Extra Options panel (–jlink_script_file=$PROJ_DIR$/../evkbmimxrt1170_connect_cm4_cm7side.jlinkscript command line option is applied).
Click on “Download and Debug” button. During the loading process you can be asked by J-Link sw to select the proper device name (MIMXRT1176XXXA_M7 is unknown). Click O.K. and choose the MIMXRT1176xxxxA device.
It is not possible to attach to the CM4 core when using the J-Link. Also, the multicore debugging does not work with that probe.
Note: To download and debug Keil MDK project using J-Link (replacing the default CMSIS-DAP debug probe), following steps are needed:
Remove J6 and J7 jumpers.
Attach the J-Link probe (J-Link Plus / J-Trace) to the board using the J1 connector.
Set “J-LINK / J-TRACE Cortex” in CM7 project options -> Debug panel (replacing CMSIS-DAP Debugger option).
After the CM7 application build click on Download/F8 button (menu Flash -> Download).
Power off and power on the board.
Multicore example starts running, one can start debugging the CM7 side by clicking on Start/Stop Debug Session (Ctrl + F5).
It is not possible to attach to the CM4 core when using the J-Link.
MIMXRT1160-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1160-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Copy CORE1 image to address: 0x20200000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
Note: To download binary of cm7 core into qspiflash and boot from qspiflash directly, following steps are needed:
Compile flash target of the project, and get the binaray file “hello_world.bin”.
Set the SW1: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J11.
Drop the binaray into disk “RT1160-EVK” on PC.
Wait for the disk disappear and appear again which will take couple of seconds.
Reset the board by pressing SW3 or power off and on the board. (If default boot core is cm4, binary of cm4 could be downloaded and boot according to steps above.)
Note: To download and debug IAR EW project using J-Link (replacing the default CMSIS-DAP debug probe), following steps are needed:
Remove J6 and J7 jumpers.
Attach the J-Link probe (J-Link Plus / J-Trace) to the board using the J1 connector.
Set “J-Link / J-Trace” in CM7 project options -> Debugger -> Setup panel (replacing CMSIS-DAP option).
Unselect the “Use macro file(s)” in CM7 project options -> Debugger -> Setup panel.
Enable “Use command line options” in CM7 project options -> Debugger -> Extra Options panel (–jlink_script_file=$PROJ_DIR$/../evkmimxrt1160_connect_cm4_cm7side.jlinkscript command line option is applied).
Click on “Download and Debug” button. During the loading process you can be asked by J-Link sw to select the proper device name (MIMXRT1166XXXA_M7 is unknown). Click O.K. and choose the MIMXRT1166xxxxA device.
It is not possible to attach to the CM4 core when using the J-Link. Also, the multicore debugging does not work with that probe.
Note: To download and debug Keil MDK project using J-Link (replacing the default CMSIS-DAP debug probe), following steps are needed:
Remove J6 and J7 jumpers.
Attach the J-Link probe (J-Link Plus / J-Trace) to the board using the J1 connector.
Set “J-LINK / J-TRACE Cortex” in CM7 project options -> Debug panel (replacing CMSIS-DAP Debugger option).
After the CM7 application build click on Download/F8 button (menu Flash -> Download).
Power off and power on the board.
Multicore example starts running, one can start debugging the CM7 side by clicking on Start/Stop Debug Session (Ctrl + F5).
It is not possible to attach to the CM4 core when using the J-Link.
MIMXRT1180-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Copy CORE1 image to address: 0x303C0000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
FRDM-K32L3A6
Hardware requirements
Mini/micro USB cable
FRDM-K32L3A6 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the PC host and the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
.
.
.
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
The Multicore RPMsg-Lite pingpong RTOS project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
For detailed instructions, see the appropriate board User’s Guide.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Copy CORE1 image to address: 0x2004e000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T board
Personal Computer
Board settings
The Multicore RPMsg-Lite pingpong RTOS project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
For detailed instructions, see the appropriate board User’s Guide.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Copy CORE1 image to address: 0x2004e000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
FRDM-MCXW72
Hardware requirements
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the host PC and the board J10.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
KW47-EVK
Hardware requirements
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
KW47-LOC
Hardware requirements
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
LPCXpresso55S69
Hardware requirements
Mini/micro USB cable
LPCXpresso55s69 board
Personal Computer
Board settings
The Multicore RPMsg-Lite pingpong RTOS project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
For detailed instructions, see the appropriate board User’s Guide.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Copy CORE1 image to address: 0x20033000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings
The Multicore RPMsg-Lite pingpong RTOS project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
For detailed instructions, see the appropriate board User’s Guide.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Copy CORE1 image to address: 0x2004e000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings
The Multicore RPMsg-Lite pingpong RTOS project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
For detailed instructions, see the appropriate board User’s Guide.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Copy CORE1 image to address: 0x2004e000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
MCX-W72-EVK
Hardware requirements
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
MIMXRT700-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the PC host and the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
.
.
.
MCXW72-LOC
Hardware requirements
Type-C USB cable
MCXW72-LOC Board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
FRDM-IMXRT1186
Hardware requirements
Type-C USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Copy CORE1 image to address: 0x303C0000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
FRDM-IMXRT700
Hardware requirements
Type-C USB cable
FRDM-IMXRT700 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the PC host and the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
.
.
.
FRDM-MCXE32B
Hardware requirements
Type-C USB cable
FRDM-MCXE32B board
Personal Computer
Board settings
The Multicore RPMsg-Lite pingpong RTOS project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:
RPMsg demo starts
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
RPMsg demo ends
Note: The secondary core (M7_1) image is embedded into the primary core (M7_0) image and programmed to flash at address 0x005C0000. The primary core releases the secondary core through the MC_ME interface and the secondary core runs in place directly from flash. No copy-to-RAM step is performed.