MCUXpresso SDK Documentation

Encrypted XIP using IPED#

This document extends the documentation of MCUBoot and encrypted XIP in OTA examples and provides an additional information related to the IPED module.

Note: The extension currently supports only IPED module based on GCM algorithm in RW61x devices.

1. Introduction#

IPED (Inline Prince Encryption/Decryption for off-chip flash) is encryption unit for external flash specific for NXP RW61x, RT700 and MCXN MCUs.

The IPED engine generates an 8-byte authentication tag for each 32-byte block of encrypted data. When storing this encrypted data in Flash memory, the FlexSPI controller organizes it in a specific pattern:

  • Each block of 32 bytes of ciphertext is followed by 8 bytes of authentication tag data (total: 40 bytes per unit)

  • The authentication tags are stored physically in flash but are hidden from the CPU’s logical address space (AHB read, fetch) - the CPU only sees the decrypted payload

  • Due to this interleaving scheme, the actual physical flash consumption is (5/4)× the logical address space visible to the CPU

Following image shows an example of a valid IPED regions configuration - logical to physical address mapping

Image

There are several points to be aware when utilizing IPED in an OTA process

  • Resulting consumption of physical memory

    • range of IPED region is defined in terms of logical address but the physical memory consumption is 1.25× the logical memory consumption

    • OTA process must ensure that installed OTA image doesn’t overlap the maximal size of IPED region, for example by adjusting the output binary size in linker file and/or doing checks of the image size before the encryption process

  • Flash operations have to satisfy boundaries of the flash page/sector size and encryption unit size

    • due internal software arbitration only ROM IAP for flash writes can be used

    • size of data chunk must be aligned to 4 * page size, no partial writes are allowed - last data chunk must be padded with dummy bytes

The whole IPED initialization, metadata handling and image re-encryption are resolved in encrypted_xip_platform_iped.c, bootutil_hooks.c and flash backend porting layer.

Additional information for IPED in RW61x can be found in its reference manual.

1.1 Metadata structure#

The structure follows ROM code but the IPED configuration is handled manually from mcuboot context.

Metadata Flash Sector (IPED)
━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━

 0                    ┌─────────────────────────────────────────────────────┐
                      │  tag           [4 bytes]                            │
                      │  params        [252 bytes]                          │
                      │    configId    [4 bytes]                            │
                      │    princeRnds  [4 bytes]                            │
                      │    regionOff   [4 bytes]                            │
                      │    ipedConfig  [60 bytes]  × 4 = 240 bytes          │
                      │      start     [4 bytes]                            │
                      │      end       [4 bytes]                            │
                      │      flags     [1 byte]                             │
                      │      padding   [3 bytes]                            │
                      │      encIv     [48 bytes]                           │
                      │        iv      [16 bytes]                           │
                      │        cipher  [16 bytes]                           │
                      │        tag     [16 bytes]                           │
 +256                 ├╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌┤
                      │                                                     │
                      │              (erased 0xFF)                          │
                      │                                                     │
 SECTOR_SIZE/2        ╠═════════════════════════════════════════════════════╣
                      │                                                     │
                      │              (erased 0xFF)                          │
                      │                                                     │
 SECTOR_SIZE-32       ├─────────────────────────────────────────────────────┤
                      │  enc_confirm_t [32 bytes]                           │
 SECTOR_SIZE          └─────────────────────────────────────────────────────┘
━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━
flexspi_nor_mem_image_iped_config_t (256 bytes, 16-byte aligned):
  [  0..  3]  tag                        (4 bytes)   "IPCB" (0x42435049) validity marker
  [  4..  7]    configId                 (4 bytes)   engine selector: kNBOOT_MemCryptIped (0x95959595)
  [  8.. 11]    ipedPrinceRounds         (4 bytes)   number of PRINCE rounds: 12 or 22
  [ 12.. 15]    regionOffset             (4 bytes)   lowest IPED context register index
  [ 16..255]    ipedConfig[4]          (240 bytes)   4 × nboot_iped_region_config_t (60 bytes each):
  [ +0.. +3]      startAddress           (4 bytes)   IPEDx_START register value
  [ +4.. +7]      endAddress             (4 bytes)   IPEDx_END register value
  [ +8.. +8]      regionFlags            (1 byte)    bit0=enabled, bit1=locked
  [ +9..+11]      padding                (3 bytes)   explicit alignment padding
  [+12..+59]      encryptedIv           (48 bytes)   AES-GCM protected IV blob:
  [+12..+27]        iv                  (16 bytes)   AES-GCM nonce used to encrypt the IV
  [+28..+43]        ciphertext          (16 bytes)   encrypted IPED region IV
  [+44..+59]        tag                 (16 bytes)   AES-GCM authentication tag

enc_confirm_t (32 bytes):
  [  0.. 31]  magic                  (32 bytes)   written last in a separate flash page — confirms config block
                                                  was fully persisted; absence signals incomplete OTA update

2. Encryption of MCUboot (OVERWRITE_ONLY only)#

Encrypting the mcuboot partition is required only for case when a private key used for offline encryption is embedded in bootloader code as C array, otherwise, it’s optional.

To simplify the workflow, the MCUXpresso Secure Provisioning Tool (SEC tool) is used.

To provision the device and encrypt the bootloader perform the following steps:

  1. Erase the device

  2. Build mcuboot_opensource

  3. Get the device into ISP mode

    • Typically on development boards hold the ISP button and press the reset button

  4. Open the SEC tool and create new workspace for RW61x target device

    • Test the ISP connection in SEC tool

  5. Switch to PKI management tab

    • Click Generate keys (leave default settings)

  6. Build Image

    • Boot: Encrypted (IPED) Plain

    • Select or mcuboot_opensource output binary or ELF image as Source executable image

    • Lifecycle: Develop, OTP

    • Select an authentication key and generate CUST_MK_SK and OEM SB seed

    • Click Build image

  7. Configure IPED regions

    • Click IPED regions

    • Configure Region 0 for MCUBoot partition as shown in following image (Region 1 is reserved for execution slot)

  8. Write image

    • Click Write image

Note: This operation provisions the device with RKTH and CUST_MK_SK permanently, but the board will still be usable for development purposes as OTP BOOT_CFG0 (fuseword 15) remains intact. An user is advised to save SEC tool workspace (or atleast the keys somewhere) for future use.

Image

3. Initial SB3 image, OTA SB3 image (FLASH_REMAP only)#

Note: Encrypted XIP with FLASH_REMAP support is currently in an experimental state. The mode can be evaluated only with ota_mcuboot_basic example

Due of customized placement of configuration structures out of FCB, an initial SB3 is required for safe deployment during end-product manufacturing. SB3 container can be also used as secure capsule for signed image providing an encryption during the OTA image transport. Additional information can be found ib SB3 documentation

Note: The device must be provisioned with RKTH and CUST_MK_SK. For provisioning, you can follow the previous chapter.

To simplify the workflow, the MCUXpresso Secure Provisioning Tool (SEC tool) is used.

  1. Build ota_mcuboot_basic and sign image by imgtool as usual.

  2. Look into ota_examples/\_common/sb3_templates and ota_examples/\_common/binaries directories and copy the template and additional binaries to your $sec_tool_workspace

    • rw61x_IPED_initial_image.yaml for the initial image

    • rw61x_IPED_ota_slot0_image.yaml or rw61x_IPED_ota_slot1_image.yaml for OTA image

    • iped_conf_magic_page.bin magic (confirmation) for configuration structure

    • slot_trailer_page.bin MCUboot slot trailer with confirmation flag (required for DIRECT-XIP mode)

  3. Extract the FCB from mcuboot_opensource binary and place it in source_images folder

    • nxpimage utils binary-image extract -b mcuboot_opensource.bin -a 0x400 -s 512 -o parsed_fcb.bin

  4. In SEC tool open Tools/SB Editor and click Import to import the template

    • Check and eventually fix paths to keys and image binary

    • click Generate

    • alternatively use SPSDK directly: nxpimage sb31 export -c template.yaml

For initial image:

  1. Get the device into ISP mode

    • Typically on development boards hold the ISP button and press the reset button

    • Test the ISP connection in SEC tool

  2. The initial image can be loaded using blhost

    • blhost -t 100000 -p COM3,115200 receive-sb-file initial_image_slot_0.sb

For OTA update using SB3 follow instructions MCUBoot and encrypted XIP in OTA examples.