MCUXpresso SDK Documentation

Run a Demo Using MDK#

The Repository-Layout SDK Package does not ship pre-generated IDE projects. Instead, you generate a Keil MDK (μVision) project on demand from the CMake build, the same way you would from a GitHub Repository SDK checkout.

Prerequisites#

Ruby#

IDE project generation is implemented in Ruby and is only needed if you want to use MDK instead of the command line or VS Code. See Ruby - IDE Project Generation (Optional) for setup instructions before continuing.

CMSIS device pack#

Cortex Microcontroller Software Interface Standard (CMSIS) device packs must be installed in MDK to fully support the device from a debug perspective, including memory map information, register definitions, and flash programming algorithms. In μVision, select the Pack Installer icon and install the pack for your device before opening the generated project.

1. Generate the MDK project#

If this is a pristine build, specify board, example, toolchain and core on the command line:

west build -b evkbmimxrt1170 examples/demo_apps/hello_world --toolchain mdk -Dcore_id=cm7 --config flexspi_nor_debug -p always -t guiproject

If you already built the example with west build, you can regenerate the project with the shorter form:

west build -t guiproject

The project files are generated into mcuxsdk/build/mdk, using relative paths to refer to source files and include paths in the repository. For the full set of guiproject options, see IDE Project Generation.

Generate into a custom folder#

By default the project is generated into mcuxsdk/build/<toolchain>. To generate into a different location instead — for example to keep projects for several examples or boards side by side — pass -d with the pristine build command:

west build -b evkbmimxrt1170 examples/demo_apps/hello_world --toolchain mdk -Dcore_id=cm7 --config flexspi_nor_debug -p always -t guiproject -d build_hello_world_mdk

2. Open the project in μVision#

Open the generated .uvmpw workspace file from:

mcuxsdk/build/mdk

3. Build the demo application#

  1. Select Rebuild to build the demo project.

  2. The build completes without errors.

4. Run the demo application#

  1. Open a terminal application on the PC, such as PuTTY or TeraTerm, and connect to the debug COM port (see How to determine COM port).

  2. Click the Download button to download the application to the target.

  3. Click the Start/Stop Debug Session button to enter the debug session.

  4. Click the Run button to start the application.

  5. The terminal displays the demo application output.

Next steps#