Vector-dased draw operations#
This part of the API performs the hardware accelerated draw operations.
Draw and gradient enumerations#
This section provides an overview of draw and gradient enumerations.
vg_lite_blend_t enumeration#
This enumeration is defined under the “Blit enumerations” section (see vg_lite_blend_t enumeration).
Parent topic:Draw and gradient enumerations
vg_lite_color_t parameter#
The common parameter vg_lite_color_t is described in Common parameter types.
Parent topic:Draw and gradient enumerations
vg_lite_fill_t enumeration#
This enumeration is used to specify the fill rule to use. For drawing any path, the hardware supports both non-zero and odd-even fill rules.
To determine whether any point is contained inside an object, imagine drawing a line from that point out to infinity in any direction such that the line does not cross any vertex of the path. For each edge that is crossed by the line, add 1 to the counter if the edge is crossed from left to right, as seen by an observer walking across the line towards infinity, and subtract 1 if the edge crossed from right to left. In this way, each region of the plane will receive an integer value.
The non-zero fill rule says that a point is inside the shape if the resulting sum is not equal to zero. The even/odd rule says that a point is inside the shape if the resulting sum is odd, regardless of sign.
Used in function: vg_lite_render_masklayer.
Used in draw functions: vg_lite_draw, vg_lite_draw_grad, vg_lite_draw_radial_grad, vg_lite_draw_pattern.
vg_lite_fill_t string values |
Description |
|---|---|
VG_LITE_FILL_NON_ZERO |
Non-zero fill rule. A pixel is drawn if it crosses at least one path pixel. |
VG_LITE_FILL_EVEN_ODD |
Even-odd fill rule. A pixel is drawn if it crosses an odd number of path pixels. |
Parent topic:Draw and gradient enumerations
vg_lite_filter_t enumeration#
This enum is defined under the “Blit enumerations” section (see vg_lite_filter_t enumeration).
Parent topic:Draw and gradient enumerations
vg_lite_gradient_spreadmode_t enumeration#
vg_lite_gradient_spreadmode_t enum is defined to match OpenVG enum VGColorRampSpreadMode (from March 2023, replacesvg_lite_radial_gradient_spreadmode*, requires GC355/GC555 hardware)*
The application may only define stops with offsets between 0 and 1. Spread modes define how the given set of stops are repeated or extended in order to define interpolated color values for arbitrary input values outside the [0,1] range.
Used in structure: vg_lite_radial_gradient_t.
vg_lite_gradient_spreadmode_t String Values |
Description |
|---|---|
|
The current fill color is used for all stop values less than 0 or greater than 1 respectively. |
|
Colors defined at 0 and 1 are used for all stop values less than 0 or greater than 1 respectively. |
|
Color values defined between 0 and 1 are repeated indefinitely in both directions. |
|
Color values defined between 0 and 1 are repeated indefinitely in both directions but with alternate copies of the range reversed. |
Parent topic:Draw and gradient enumerations
vg_lite_pattern_mode_t enumeration#
Defines how the region outside the image pattern is filled for the path.
Used in function: vg_lite_draw_gradient, vg_lite_draw_pattern.
vg_lite_pattern_mode_t string values |
Description |
|---|---|
|
Pixels outside the bounds of the source image should be taken as the color. |
|
Pixels outside the bounds of the source image should be taken as having the same color as the closest edge pixel. The color of the pattern border is expanded to fill the region outside the pattern. |
|
Pixels outside the bounds of the source image should be repeated indefinitely in all directions. (from March 2023) |
|
Pixels outside the bounds of the source image should be reflected indefinitely in all directions. (from March 2023) |
Parent topic:Draw and gradient enumerations
vg_lite_radial_gradient_spreadmode_t enumeration#
(Deprecated March 2023) use vg_lite_gradient_spreadmode_t. Defines the radial gradient padding mode. (from Nov 2020, requires GC355 hardware)
Used in structure: vg_lite_radial_gradient_t.
vg_lite_radial_gradient_spreadmode_t String Values |
Description |
|---|---|
|
The current fill color is used for all stop values less than 0 or greater than 1 respectively. |
|
Colors defined at 0 and 1 are used for all stop values less than 0 or greater than 1 respectively. |
|
Color values defined between 0 and 1 are repeated indefinitely in both directions. |
|
Color values defined between 0 and 1 are repeated indefinitely in both directions but with alternate copies of the range reversed. |
Parent topic:Draw and gradient enumerations
Parent topic:Vector-dased draw operations
Draw and gradient structures#
This section provides an overview of the draw and gradient structures.
vg_lite_buffer_t structure#
This structure is defined under the “Pixel buffer structures” section (see vg_lite_buffer_t structure).
Parent topic:Draw and gradient structures
vg_lite_color_ramp_t structure#
This structure defines the stops for the radial gradient. The five parameters provide the offset and color for the stop. Each stop is defined by a set of floating point values which specify the offset and the sRGBA color and alpha values. Color channel values are in the form of a non-premultiplied (R, G, B, alpha) quad. All parameters are in the range of [0,1]. The red, green, blue, alpha value of [0, 1] is mapped to an 8-bit pixel value [0, 255].(from November 2020, requires GC355 hardware)
The define for the max number of radial gradient stops is #define MAX_COLOR_RAMP_STOPS256.
Used in radial gradient structure: vg_lite_radial_gradient_t.
vg_lite_color_ramp_t members |
Type |
Description |
|---|---|---|
|
|
Offset value for the color stop |
|
|
Red color channel value for the color stop |
|
|
Green color channel value for the color stop |
|
|
Blue color channel value for the color stop |
|
|
Alpha color channel value for the color stop |
Parent topic:Draw and gradient structures
vg_lite_linear_gradient_t structure#
This structure defines the organization of a linear gradient in VGLite data. The linear gradient is applied to filling a path. It generates a 256x1 image according to the specified settings.
Used in init and draw functions: vg_lite_init_grad, vg_lite_set_grad, vg_lite_update_grad, vg_lite_get_grad_matrix, vg_lite_clear_grad, vg_lite_draw_grad.
vg_lite_linear_gradient_t constants |
Type |
Description |
|---|---|---|
|
|
Constant. Maximum number of gradient colors = 16. |
vg_lite_linear_gradient_t members |
||
|
|
Color array for the gradient |
|
|
Number of colors |
|
|
Number of color stops, from 0 to 255 |
|
|
Struct for the matrix to transform the gradient color ramp |
|
|
Image object struct to represent the color ramp |
Parent topic:Draw and gradient structures
vg_lite_ext_linear_gradient structure#
This structure defines the organization of the extended parameters possible for a linear gradient (from April 2022).
Used in functions: vg_lite_draw_linear_grad.
vg_lite_ext_linear_gradient_t members |
Type |
Description |
|---|---|---|
|
|
Count of colors, up to 256. |
|
|
The matrix to transform the gradient. |
|
|
The image for rendering as gradient pattern. |
|
|
Linear gradient parameters. Includes center point, focal point and radius. |
|
|
Color ramp length for gradient paints provided to the driver. |
|
|
Color ramp parameter for gradient paints provided to the driver. |
|
|
Converted internal color ramp length. |
|
|
Converted internal color ramp. |
|
|
If this value is set to 1, the color value of |
|
|
The spread mode that is applied to the pixels out of the image after transformed. |
|
Parent topic:Draw and gradient structures
vg_lite_linear_gradient_parameter structure#
This structure defines a radial direction for a linear gradient. (from April 2022)
Line0 connects point (X0, Y0) to point (X1, Y1) and represents the radial direction of the linear gradient.
Line1 is a line perpendicular to line0 which passes through point (X0, Y0).
Line2 is a line perpendicular to line0 which passes through point (X1, Y1)
The linear gradient paint is applied at the intersection of the path fill area and the plane starting from line 1 and ending at line 2.
Used in structure: vg_lite_ext_linear_gradient.
Used in functions: vg_lite_set_linear_grad.
vg_lite_linear_gradient_parameter_t members |
Type |
Description |
|---|---|---|
X0 |
|
X origin of linear gradient radial direction. |
Y0 |
|
Y origin of linear gradient radial direction. |
X1 |
|
X end point of linear gradient radial direction. |
Y1 |
|
Y end point of linear gradient radial direction. |
Parent topic:Draw and gradient structures
vg_lite_matrix_t structure#
This structure is defined under the “Matrix control structures” section (see vg_lite_matrix_t structure).
Parent topic:Draw and gradient structures
vg_lite_path_t structure#
This structure is defined under the “Vector path structures” section (see vg_lite_path_t structure).
Parent topic:Draw and gradient structures
vg_lite_radial_gradient_parameter_t structure#
This structure defines the gradient radius and the X and Y coordinates for the center and focal points of the gradient (from November 2020, requires GC355 or GC555 hardware).
Used in radial gradient structure: vg_lite_radial_gradient_t.
vg_lite_radial_gradient_parameter_t member |
Type |
Description |
|---|---|---|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
Parent topic:Draw and gradient structures
vg_lite_radial_gradient_t structure#
This structure defines the application of the radial gradient to fill a path. (from November 2020, requires GC355 or GC555 hardware).
Used in radial gradient functions: vg_lite_draw_grad, vg_lite_set_radial_grad, vg_lite_update_radial_grad, vg_lite_get_radial_grad, vg_lite_clear_radial_grad.
vg_lite_radial_gradient_t member |
Type |
Description |
|---|---|---|
|
vg_lite_uint32_t |
Count of colors, up to 256 |
|
Structure that specifies the transform matrix for the gradient |
|
|
Structure that specifies the image for rendering as a gradient pattern |
|
|
Structure that specifies the location of the gradient’s center point (cx, cy), focal point(fx, fy) and radius(r) |
|
|
vg_lite_uint32_t |
Color ramp parameters for gradient paints provided to the driver |
|
Structure that specifies the color ramp |
|
|
vg_lite_uint32_t |
Converted internal color ramp. |
|
Structure that specifies the internal color ramp |
|
|
vg_lite_uint32_t |
If this value is set to 1, the color value of |
|
Enum that specifies the tiling mode, which is applied to the pixels out of the image after transformation |
Parent topic:Draw and gradient structures
Parent topic:Vector-dased draw operations
Draw functions#
This section provides an overview of the draw functions.
vg_lite_draw function#
Description:
This function performs a hardware accelerated 2D vector draw operation.
The size of the tessellation buffer can be specified at initialization and it is aligned with the minimum hardware alignment requirements of the kernel. Specifying a smaller size for tessellation buffer allocates less memory but reduces performance. Because the hardware walks the target with the provided tessellation window size, a path may be sent to the hardware multiple times. It is a good practice to set the tessellation buffer size to the most common path size. For example, if all you do is render up to 24-point fonts, you can set the tessellation buffer to 24x24.
Note:
All the color formats available in the vg_lite_buffer_format_t enum are supported as the destination buffer for the draw function
The hardware does not support strokes; they must be converted to paths before you use them in the draw API
Syntax:
vg_lite_error_t vg_lite_draw (
vg_lite_buffer_t *target,
vg_lite_path_t *path,
vg_lite_fill_t fill_rule,
vg_lite_matrix_t *matrix,
vg_lite_blend_t blend,
vg_lite_color_t color
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the |
|
Pointer to the |
|
Specifies the |
|
Pointer to a |
|
Select one of the hardware-supported blend modes in the |
|
The color applied to each pixel drawn by the path. |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Draw functions
vg_lite_draw_grad function#
Description:
This function is used to fill a path with a linear gradient according to the specified fill rules. The specified path is transformed according to the selected matrix and is filled with the specified color gradient.
Syntax:
vg_lite_error_t vg_lite_draw_grad (
vg_lite_buffer_t *target,
vg_lite_path_t *path,
vg_lite_fill_t fill_rule,
vg_lite_matrix_t *matrix,
vg_lite_linear_gradient_t *grad,
vg_lite_blend_t blend
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the |
|
Pointer to the |
|
Specifies the |
|
Pointer to the |
|
Pointer to the |
|
Specifies the blend mode in the |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Draw functions
vg_lite_draw_radial_grad function#
Description:
This function is used to fill a path with a radial gradient according to the specified fill rules. The specified path is transformed according to the selected matrix and is filled with the radial color gradient. The application can use VGLite API vg_lite_query_feature (gcFEATURE_BIT_VG_RADIAL_GRADIENT) to determine HW support for radial gradient.
Syntax:
vg_lite_error_t vg_lite_draw_radial_grad (
vg_lite_buffer_t *target,
vg_lite_path_t *path,
vg_lite_fill_t fill_rule,
vg_lite_matrix_t *path_matrix,
vg_lite_radial_gradient_t *grad,
vg_lite_color_t paint_color,
vg_lite_blend_t blend,
vg_lite_filter_t filter
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the |
|
Pointer to the |
|
Specifies the |
|
Pointer to a |
|
Pointer to the |
|
Specifies the paint color |
|
Specifies the blend mode in the |
|
Specified the filter mode |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Draw functions
vg_lite_draw_pattern function#
Description:
This function fills a path with an image pattern. The path is transformed according to the specified matrix and is filled with the transformed image pattern.
Syntax:
vg_lite_error_t vg_lite_draw_pattern (
vg_lite_buffer_t *target,
vg_lite_path_t *path,
vg_lite_fill_t fill_rule,
vg_lite_matrix_t *path_matrix,
vg_lite_buffer_t *pattern_image,
vg_lite_matrix_t *pattern_matrix,
vg_lite_blend_t blend,
vg_lite_pattern_mode_t pattern_mode,
vg_lite_color_t pattern_color,
vg_lite_color_t color,
vg_lite_filter_t filter
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the |
|
Pointer to the |
|
Specifies the vg_lite_fill_t enum value for the fill rule for the path. |
|
Pointer to the |
|
Pointer to a |
|
Pointer to the |
Pointer to a |
|
|
Specifies one of the |
|
Specifies the |
|
Specifies a 32bpp ARGB color ( |
|
Specifies a 32bpp ARGB color ( |
|
Specifies the filter type. All formats available in the |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Draw functions
Parent topic:Vector-dased draw operations
Linear gradient initialization and control functions#
This part of the API performs linear gradient operations.
A color gradient (color progression, color ramp) is a smooth transition between a set of colors (color stops) that is done along a line (linear, or axial color gradient) or radially, along concentric circles (radial color gradient). The color transition is done by linear interpolation between two consecutive color stops.
Note: VGLite supports linear color gradients for GCNanoLiteV and GCNanoUltraV. Both linear and radial gradients are supported with GC355 and GC555.
vg_lite_init_grad function#
Description:
This function initializes the internal buffer for the linear gradient object with default settings for rendering.
Syntax:
vg_lite_error_t vg_lite_init_grad (
vg_lite_linear_gradient_t *grad
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the vg_lite_linear_gradient_t structure, which defines the gradient to be initialized. Default values are used. |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Linear gradient initialization and control functions
vg_lite_clear_grad function#
Description:
This function is used to clear the values of a linear gradient object and free up the memory of the image buffer.
Syntax:
vg_lite_error_t vg_lite_clear_grad (
vg_lite_linear_gradient_t *grad
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the vg_lite_linear_gradient_t structure that is to be cleared |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Linear gradient initialization and control functions
vg_lite_set_grad function#
Description:
This function is used to set values for the members of the vg_lite_linear_gradient_t structure.
Note: The vg_lite_set_grad API adopts the following rules to set the default gradient colors if the input parameters are incomplete or invalid:
If no valid stops have been specified (for example, due to an empty input array, out-of-range or out-of-order stops), a stop at 0 with (R, G, B, A) color (0.0, 0.0, 0.0, 1.0) (opaque black) and a stop at 1 with color (1.0, 1.0, 1.0, 1.0) (opaque white) are implicitly defined
If at least one valid stop has been specified, but none has been defined with an offset of 0, then an implicit stop is added with an offset of 0 and the same color as the first user-defined stop
If at least one valid stop has been specified, but none has been defined with an offset of 1, then an implicit stop is added with an offset of 1 and the same color as the last user-defined stop
Syntax:
vg_lite_error_t vg_lite_set_grad (
vg_lite_linear_gradient_t *grad,
uint32_t count,
uint32_t *colors,
uint32_t *stops
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the vg_lite_linear_gradient_t structure to be set |
|
The number of colors in the linear gradient. The maximum color stop count is defined by |
|
Specifies the color array for the gradient stops. The color is in ARGB8888 format with alpha in the upper byte. |
|
Pointer to the gradient stop offset |
Returns:
Always returns VG_LITE_SUCCESS.
Parent topic:Linear gradient initialization and control functions
vg_lite_get_grad_matrix function#
Description:
This function is used to get a pointer to the transformation matrix of the gradient object. It allows an application to manipulate the matrix to facilitate correct rendering of the gradient path.
Syntax:
vg_lite_error_t vg_lite_get_grad_matrix (
vg_lite_linear_gradient_t *grad
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the vg_lite_linear_gradient_t structure, which contains the matrix to be retrieved |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Linear gradient initialization and control functions
vg_lite_update_grad function#
Description:
This function is used to update or generate values for an image object that is going to be rendered. The vg_lite_linear_gradient_t object has an image buffer, which is used to render the gradient pattern. The image buffer is created or updated with the corresponding gradient parameters.
Syntax:
vg_lite_error_t vg_lite_update_grad (
vg_lite_linear_gradient_t *grad
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the vg_lite_linear_gradient_t structure, which contains the update values to be used for the object to be rendered |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Linear gradient initialization and control functions
Parent topic:Vector-dased draw operations
Linear gradient extended functions#
The following functions are available only with IP that includes hardware support for extended linear gradient capabilities, such as GC355 and GC555. These functions are not available with GCNanoLiteV, GCNanoUltraV, or GCNanoV. Applications can use VGLite API vg_lite_query_feature (gcFEATURE_BIT_VG_LINEAR_GRADIENT_EXT) to determine HW support for linear gradient.
vg_lite_set_linear_grad function#
Description:
This function is used to set the values that define the linear gradient. (from April 2022)
Syntax:
vg_lite_error_t vg_lite_set_linear_grad (
vg_lite_ext_linear_gradient_t *grad,
vg_lite_uint32_t count,
vg_lite_color_ramp_t *color_ramp,
vg_lite_linear_gradient_parameter_t grad_param,
vg_lite_radial_gradient_spreadmode_t spread_mode,
vg_lite_uint8_t pre_mult
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the |
|
Count of the colors in the gradient. The maximum color stop count is defined by |
|
It is the array of stops for the linear gradient. The number of parameters for each stop is 5, and gives the offset and color of the stop. Each stop is defined by a floating-point offset value and four floating-point values containing the sRGBA color and alpha value associated with each stop, in the form of a non-premultiplied (R, G, B, alpha) quad. The range of all parameters is [0,1]. |
|
Gradient parameters as specified in the structure |
|
The fill mode is applied to the pixels out of the paint after transformation. Uses the same spread mode enumeration types as radial gradient. For details, see |
|
This parameter controls whether color and alpha values are interpolated in premultiplied or non-premultiplied form. |
Returns:
Returns VG_LITE_INVALID_ARGUMENTS to indicate the parameters are wrong.
Parent topic:Linear gradient extended functions
vg_lite_get_linear_grad_matrix function#
Description:
This function returns a pointer to an extended linear gradient object’s matrix.(from March 2023).
Syntax:
vg_lite_matrix_t* vg_lite_get_linear_grad_matrix (
vg_lite_ext_linear_gradient_t *grad,
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the |
Returns:
Returns a pointer to vg_lite_matrix_t for the specified extended linear gradient.
Parent topic:Linear gradient extended functions
vg_lite_draw_linear_grad function#
Description:
This function returns a pointer to an extended linear gradient object’s matrix.(from March 2023).
Syntax:
vg_lite_error_t vg_lite_draw_linear_grad (
vg_lite_buffer_t *target,
vg_lite_path_t *path,
vg_lite_fill_t fill_rule,
vg_lite_matrix_t *path_matrix,
vg_lite_ext_linear_gradient_t *grad,
vg_lite_color_t paint_color,
vg_lite_blend_t blend,
vg_lite_filter_t filter
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the |
|
Pointer to the |
|
Specifies the |
|
Pointer to a |
|
Pointer to the |
|
Specifies the paint color |
|
Specifies blend mode in the |
|
Specified the filter mode |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Linear gradient extended functions
vg_lite_update_linear_grad function#
Description:
This function is used to update or generate the corresponding image object to render (from April 2022).
The vg_lite_ext_linear_gradient_t object has an image buffer that is used to render the linear gradient paint. The image buffer is created/updated according to the specified grad parameters.
Syntax:
vg_lite_error_t vg_lite_update_linear_grad (
vg_lite_ext_linear_gradient_t *grad,
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Linear gradient extended functions
vg_lite_clear_linear_grad function#
Description:
This function is used to clear the linear gradient object. This resets the grad members and free the image buffer’s memory (from April 2022).
Syntax:
vg_lite_error_t vg_lite_clear_linear_grad (
vg_lite_ext_linear_gradient_t *grad,
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Linear gradient extended functions
Parent topic:Vector-dased draw operations
Radial gradient functions initialization and control functions#
The following functions are available only with IP that supports radial gradients, such as GC355 and GC555. These functions are not available with GCNanoLiteV, or GCNanoUltraV or GCNanoV.
Note: There is no init function required for radial gradients. Buffer initialization is done through the vg_lite_update_radial_grad function. (from Nov 2020, requires GC355 or GC555 hardware)
vg_lite_set_radial_grad function#
Description:
This function is used to set the values for the radial linear gradient definition. (from November 2020, requires GC355 or GC555 hardware)
Syntax:
vg_lite_error_t vg_lite_set_radial_grad (
vg_lite_radial_gradient_t *grad,
vg_lite_uint32_t count,
vg_lite_color_ramp_t *color_ramp,
vg_lite_radial_gradient_parameter_t grad_param,
vg_lite_radial_gradient_spreadmode_t spread_mode,
vg_lite_uint8_t pre_mult
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the vg_lite_radial_gradient_t structure for the radial gradient that has to be set |
|
The number of color stops in the gradient. The maximum color stop count is defined by |
|
Pointer to the vg_lite_color_ramp_t structure that defines the stops for the radial gradient. The five parameters provide the offset and color for each stop. Each stop is defined by a set of floating point values that specify the offset and the sRGBA color and alpha values. Color channel values are in the form of a non-premultiplied (R, G, B, alpha) quad. All parameters are in the range of [0,1]. The red, green, blue, alpha value of [0, 1] is mapped to an 8-bit pixel value [0, 255]. |
|
The radial gradient parameters are supplied as a vector of 5 floats. Parameters (cx, cy) specify the center point, parameters (fx, fy) specify the focal point, and r specifies the radius. See structure vg_lite_radial_gradient_parameter_t. |
|
The tiling mode that is applied to pixels out of the paint after transformation. See enum vg_lite_radial_gradient_spreadmode_t. |
|
Controls whether color and alpha values are interpolated in premultiplied or non-premultiplied form. If this value is set to 1, the color value of |
Returns:
Returns VG_LITE_INVALID_ARGUMENTS to indicate that the parameters are wrong.
Parent topic:Radial gradient functions initialization and control functions
vg_lite_update_radial_grad function#
Description:
This function is used to update or generate values for an image object that is going to be rendered. The vg_lite_radial_gradient_t object has an image buffer that is used to render the gradient pattern. The image buffer will be created or updated with the corresponding gradient parameters. (from November 2020, requires GC355 or GC555 hardware)
Syntax:
vg_lite_error_t vg_lite_update_radial_grad (
vg_lite_radial_gradient_t *grad,
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the vg_lite_radial_gradient_t structure, which contains the updated values to be used for the object to be rendered |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Radial gradient functions initialization and control functions
vg_lite_get_radial_grad_matrix function#
Description:
This function is used to get a pointer to the radial gradient object’s transformation matrix. This allows an application to manipulate the matrix to facilitate correct rendering of the gradient path*. (from Nov 2020, requires GC355 or GC555 hardware).*
Syntax:
vg_lite_error_t vg_lite_get_radial_grad_matrix (
vg_lite_radial_gradient_t *grad,
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the vg_lite_radial_gradient_t structure, which contains the matrix to be retrieved |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Radial gradient functions initialization and control functions
vg_lite_clear_rad_grad function#
Description:
This function is used to clear the values of a radial gradient object and free the image buffer’s memory*. (from Nov 2020, requires GC355 or GC555 hardware)*
Syntax:
vg_lite_error_t vg_lite_clear_radial_grad (
vg_lite_radial_gradient_t *grad,
);
Parameters:
Parameter |
Description |
|---|---|
|
Pointer to the vg_lite_radial_gradient_t structure which is to be cleared |
Returns:
Returns VG_LITE_SUCCESS if successful. See vg_lite_error_t enum for other return codes.
Parent topic:Radial gradient functions initialization and control functions
Parent topic:Vector-dased draw operations