MCUXpresso SDK Documentation

vg_lite_buffer_format_t enumeration

vg_lite_buffer_format_t enumeration#

This enumeration specifies the color format to use for a buffer. This applies to both image and Render Target. Formats include supported swizzles for RGB. For YUV swizzles, use the related values and parameters in vg_lite_swizzle_t.

The application shall use the vg_lite_query_feature API to determine support for some hardware-specific formats. For example, related vg_lite_feature_t enum values include gcFEATURE_BIT_VG_RGBA2_FORMAT and gcFEATURE_BIT_VG_IM_INDEX_FORMAT.

(Alignment columns refined March and Sept 2023)

Used in structure: vg_lite_buffer_t.

See also vg_lite_blit, vg_lite_clear, vg_lite_draw.

Attention: OpenVG VGImageFormat Note: The bits for each color channel are stored within a machine word from MSB to LSB in the order indicated by the pixel format name. This is the opposite of the original VG_LITE_* formats that are ordered from LSB to MSB. The formats with the same organization are listed in the same row as their VG_Lite counterparts.

Attention: Original VGLite API Image Format Note: The bits for each color channel are stored within a machine word from LSB to MSB in the order indicated by the pixel format name. This is the opposite of the OPENVG VG_* formats that are ordered from MSB to LSB.

The following codes, as also used in OpenVG 1.1 Specification Table 11, are used for format description:

  • A - Alpha channel

  • B - Blue color channel

  • G - Green color channel

  • R - Red color channel

  • X - Uninterpreted padding byte or bit

  • L - Grayscale

  • BW - 1-bit black and white

  • l - Linear color space

  • s - Non-linear (sRGB) color space

  • PRE - Alpha values are premultiplied

vg_lite_buffer_format_t String Value

Description

Supported as source

Supported as destination

Start address/ Stride alignment: bytes

VG_LITE_ABGR8888 VG_sRGBA_8888 VG_sRGBA_8888_PRE VG_lRGBA_8888 VG_lRGBA_8888_PRE

Yes

Yes

Start 4B / Stride 64B

VG_LITE_ARGB8888 VG_sBGRA_8888 VG_sBGRA_8888_PRE VG_lBGRA_8888 VG_lBGRA_8888_PRE

Yes

Yes

Start 4B / Stride 64B

VG_LITE_BGRA8888 VG_sARGB_8888 VG_sARGB_8888_PRE VG_lARGB_8888 VG_lARGB_8888_PRE

Yes

Yes

Start 4B / Stride 64B

VG_LITE_RGBA8888 VG_sABGR_8888 VG_sABGR_8888_PRE VG_lABGR_8888 VG_lABGR_8888_PRE

Yes

Yes

Start 4B / Stride 64B

VG_LITE_BGRX8888 VG_sXRGB_8888 VG_lXRGB_8888

Yes

Yes

Start 4B / Stride 64B

VG_LITE_RGBX8888 VG_sXBGR_8888 VG_lXBGR_8888

Yes

Yes

Start 4B / Stride 64B

VG_LITE_XBGR8888 RGBX VG_sRGBX_8888 VG_lRGBX_8888

Yes

Yes

Start 4B / Stride 64B

VG_LITE_XRGB8888 VG_sBGRX_8888 VG_lBGRX_8888

Yes

Yes

Start 4B / Stride 64B

VG_LITE_ABGR1555 VG_sRGBA_5551

Yes

Yes

Start 4B / Stride 32B

VG_LITE_ARGB1555 VG_sBGRA_5551

Yes

Yes

Start 4B / Stride 32B

VG_LITE_BGRA5551 VG_sARGB_1555

Yes

Yes

Start 4B / Stride 32B

VG_LITE_RGBA5551 VG_sABGR_1555

Yes

Yes

Start 4B / Stride 32B

VG_LITE_BGR565 VG_sRGB_565

Yes

Yes

Start 4B / Stride 32B

VG_LITE_RGB565 VG_sBGR_565

Yes

Yes

Start 4B / Stride 32B

VG_LITE_ABGR4444 VG_sRGBA_4444

Yes

Yes

Start 4B / Stride 32B

VG_LITE_ARGB4444 VG_sBGRA_4444

Yes

Yes

Start 4B / Stride 32B

VG_LITE_BGRA4444 VG_sARGB_4444

Yes

Yes

Start 4B / Stride 32B

VG_LITE_RGBA4444 VG_sABGR_4444

Yes

Yes

Start 4B / Stride 32B

VG_LITE_YUY2 VG_LITE_YUYV

Yes

No

Start 4B / Stride 32B

VG_LITE_A4 VG_A_4

Yes

No

Start 4B / Stride 8B

VG_LITE_A8 VG_A_8

Yes

Yes

Start 4B / Stride 16B

VG_LITE_L8 VG_sL_8 VG_lL_8

Yes

Yes

Start 4B / Stride 16B

Hardware-dependent formats for vg_lite_buffer_format_t

Description

Supported as source

Supported as destination

Alignment (bytes)

VG_LITE_ABGR2222

Yes

Yes

Start 4B / Stride 16B

VG_LITE_ARGB2222

Yes

Yes

Start 4B / Stride 16B

VG_LITE_BGRA2222

Yes

Yes

Start 4B / Stride 16B

VG_LITE_RGBA2222

Yes

No

8B

VG_LITE_INDEX_1

1-bit index format

Yes

No

8B

VG_LITE_INDEX_2

2-bit index format

Yes

No

both 8B

VG_LITE_INDEX_4

4-bit index format

Yes

No

both 8B

VG_LITE_INDEX_8

8-bit index format

Yes

No

both 16B

VG_LITE_NV12_TILED

Yes

No

Y: both 16 Bytes UV: both 8 Bytes

VG_LITE_ANV12_TILED

Yes

No

A, Y: both 16 Bytes UV: both 8 Bytes

VG_LITE_AYUY2_TILED

Yes

No

both 32B

VG_LITE_RGB888

Yes

Yes

Start 4B / Stride 32B

VG_LITE_BGR888

Yes

Yes

VG_LITE_ARGB8565

Yes

Yes

VG_LITE_BGRA5658

Yes

Yes

Start 4B / Stride 32B

VG_LITE_ABGR8565

Yes

Yes

Start 4B / Stride 32B

VG_LITE_RGBA5658

Yes

Yes

Start 4B / Stride 32B

Parent topic:Pixel buffer enumerations