MCUXpresso SDK Documentation

vg_lite_radial_gradient_spreadmode_t enumeration

vg_lite_radial_gradient_spreadmode_t enumeration#

(Deprecated March 2023) use vg_lite_gradient_spreadmode_t. Defines the radial gradient padding mode. (from Nov 2020, requires GC355 hardware)

Used in structure: vg_lite_radial_gradient_t.

vg_lite_radial_gradient_spreadmode_t String Values

Description

VG_LITE_RADIAL_GRADIENT_SPREAD_FILL = 0

The current fill color is used for all stop values less than 0 or greater than 1 respectively.

VG_LITE_RADIAL_GRADIENT_SPREAD_PAD

Colors defined at 0 and 1 are used for all stop values less than 0 or greater than 1 respectively.

VG_LITE_RADIAL_GRADIENT_SPREAD_REPEAT

Color values defined between 0 and 1 are repeated indefinitely in both directions.

VG_LITE_RADIAL_GRADIENT_SPREAD_REFLECT

Color values defined between 0 and 1 are repeated indefinitely in both directions but with alternate copies of the range reversed.

Parent topic:Draw and gradient enumerations