Maestro USB microphone example#
Table of content#
Overview#
The Maestro USB microphone example demonstrates audio processing on the ARM cortex core utilizing the Maestro Audio Framework library.
The application is controlled by commands from a shell interface using serial console.
The development board will be enumerated as a USB audio class 2.0 device on the USB host. The application takes audio samples from the microphone inputs and sends them to the USB host via the USB bus. User will see the volume levels obtained from the USB host but this is only an example application. To leverage the volume values, the demo has to be modified.
After the program starts and the USB audio cable is connected, the board will be visible in the operating system’s sound settings as a USB audio input device (microphone / Line-In). You can then select it as the active recording device in any application on your PC.
As shown in the table below, the application is supported on several development boards, and each development board may have certain limitations, some development boards may also require hardware modifications or allow to use of an audio expansion board. Therefore, please check the supported features and Hardware modifications or Example configuration sections before running the demo.
| Mode | Standard | ||
|---|---|---|---|
| Feature | Audio input [num of channels] | ||
| On board codec | DMICs | aud-exp-42448 | |
| EVKC-MIMXRT1060 | 1 | X | X |
| EVKB-MIMXRT1170 | 1 | X | X |
| LPCXpresso55s69 | 1 | X | X |
| EVK-MCXN5XX | 1 | X | X |
| RW612BGA | X | X | X |
| FRDM-IMXRT1152 | 1 | X | X |
Limitations:
Note:
When connected to MacBook, change the PCM format from (0x02,0x00,) to (0x01,0x00, ) in the g_config_descriptor[CONFIG_DESC_SIZE] in the
usb_descriptor.cfile. Otherwise, it can’t be enumerated and noise is present when recording with the QuickTime player because the sampling frequency and bit resolution do not match.When device functionality is changed, please uninstall the previous PC driver to make sure the device with changed functionality can run normally.
If you’re having audio problems on Windows 10 for recorder, please disable signal enhancement as the following if it is enabled and have a try again.
Known issues:
No known issues.
More information about supported features can be found on the Supported features page.
Hardware requirements#
Desired development board
2x Micro USB cable (USB-C for FRDM-IMXRT1152)
Personal Computer
LPCXpresso55s69:
Source of sound with 3.5 mm stereo jack connector
Hardware modifications#
Some development boards need some hardware modifications to run the application. If the development board is not listed here, its default setting is required.
FRDM-IMXRT1152:
Please remove below resistors to enable the microphone:
R183, R131, R151, R177, R124
Development board connectors#
Board |
Debug Port |
USB Port (Emulation) |
Line-In |
|---|---|---|---|
EVKC-MIMXRT1060 |
J53 |
J48 |
J101 |
EVKB-MIMXRT1170 |
J86 |
J20 |
J101 |
LPCXpresso55s69 |
P6 |
P10 (FULL SPD) |
J1 |
EVK-MCXN5XX |
J5 |
J27 |
J6 |
RW612BGA |
— |
— |
— |
FRDM-IMXRT1152 |
J13 |
J51 |
J30 |
Preparation#
Connect the first micro USB cable between the PC host and the debug USB port on the development board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
LPCXpresso55s69:
Insert source of sound to Audio Line-In connector (headphone jack) on the development board.
Connect the second micro USB cable between the PC host and the USB port on the development board.
Either press the reset button on your development board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, you should see similar output on the serial terminal as below:
*************************************************
Maestro audio USB microphone solutions demo start
*************************************************
Copyright 2022 NXP
[APP_Shell_Task] start
>> usb_mic -1
Starting maestro usb microphone application
The application will run until the board restarts
[STREAMER] Message Task started
Starting recording
[STREAMER] start usb microphone
Set Cur Volume : 1f00
Type help to see the command list. Similar description will be displayed on serial console:
>> help
"help": List all the registered commands
"exit": Exit program
"version": Display component versions
"usb_mic": Record MIC audio and playback to the USB port as an audio 2.0
microphone device.
USAGE: usb_mic <seconds>
<seconds> Time in seconds how long the application should run.
When you enter a negative number the application will
run until the board restarts.
EXAMPLE: The application will run for 20 seconds: usb_mic 20
Details of commands can be found here.
Example configuration#
The example only supports one mode and do not support any additional libraries, so the example can’t be configured by user.
Functionality#
The usb_mic command calls the STREAMER_mic_Create function from the app_streamer.cfile that creates pipeline with the following elements:
- ELEMENT_MICROPHONE_INDEX
- ELEMENT_USB_SINK_INDEX
Recording itself can be started with the STREAMER_Start function.
Each of the elements has several properties that can be accessed using the streamer_get_property or streamer_set_property function. These properties allow a user to change the values of the appropriate elements. The list of properties can be found in streamer_element_properties.h. See the example of setting property value in the following piece of code from the app_streamer.c file:
ELEMENT_PROPERTY_T prop;
prop.prop = PROP_MICROPHONE_SET_SAMPLE_RATE;
prop.val = AUDIO_SAMPLING_RATE;
streamer_set_property(handle->streamer, 0, prop, true);
prop.prop = PROP_MICROPHONE_SET_NUM_CHANNELS;
prop.val = 1;
streamer_set_property(handle->streamer, 0, prop, true);
prop.prop = PROP_MICROPHONE_SET_FRAME_MS;
prop.val = 1;
streamer_set_property(handle->streamer, 0, prop, true);
Some of the predefined values can be found in the streamer_api.h.
States#
The application can be in 2 different states:
Idle
Running
Commands in detail#
Legend for diagrams: