MCUXpresso SDK Documentation

Hardware#

For dual-chip implementation, the Bluetooth demo runs on a (reference board) along with the ported EdgeFast Open Bluetooth API host stack. The Linker Layer (LL) runs on a wireless module. A standard UART HCI and PCM is used to communicate between the two boards, the IMU is used to communicate in between. The Bluetooth host and controller stack run on different boards. The demo hardware requires two different boards; a development board for host stack and application and a wireless module adapter board for controller running. For example, the evkbmimxrt1170 any of the supported Murata modules with the Murata uSD-M.2 adapter. For details on the board hardware requirement and board setting, see the following documents. For one-chip implementation, the Bluetooth demo, EdgeFast Open Bluetooth API host stack, and LL run on one chip and they communicate with IMU.

  • Hardware rework guide document of the relative board, Hardware Rework Guide for MIMXRT1170-EVKB and Hardware Interconnection Guide for i.MX RT EVKs and Murata M.2 modules.

  • Readme file of the examples.

Reference boards list#

  • MIMXRT1170: For details, see the quick start guide of this reference board (MIMXRT1170).

Parent topic:Hardware

Dual-chip wireless module list#

Module

HCI

uSD-15x15 Adapter Board for AW-AM457-uSD

UART

uSD-15x15 Adapter Board for AW-CM358-uSD

UART

uSD-15x15 Adapter Board for AW-AM510-uSD

UART

AW-CM358MA

UART

AW-CM510MA

UART

K32W061

UART

Murata uSD-M.2 Adapter (LBEE0ZZ1WE-uSD-M2) and Embedded Artists 1ZM M.2 Module (EAR00364)

UART

Murata uSD-M.2 Adapter (LBEE0ZZ1WE-uSD-M2) and Embedded Artists 1XK M.2 Module (EAR00385)

UART

Murata uSD-M.2 Adapter (LBEE0ZZ1WE-uSD-M2) and Embedded Artists 2EL M.2 Module (Rev-A1)

UART

For details on AzureWave module, see the quick start guide of this reference board AW-AM457-uSD, AW-CM358-uSD, AW-CM358MA, AW-AM510-uSD, AW-CM510MA, and K32W061.

For Murata documentation, refer to the Quick Start Guide and User Guide here.

Note: The boards and wireless module lists are not random combination. For the wireless module support list of specific board, see the readme.txt of each example.

Parent topic:Hardware

Edgefast Open Board Module Support#

Board and Module Support Matrix#

Board

Default Module

Default Interface: M.2

Default Interface: Arduino

Default Interface: uSD Slot

MURATA_1XK (IW416)

MURATA_1ZM (88W8987)

MURATA_2EL (IW612)

MURATA_2LL (IW610)

AW300 (IW612)

K32W

evkbimxrt1050

MURATA_2EL

-

-

x

BLE/Classic

BLE/Classic

BLE/Classic

-

-

BLE

evkbmimxrt1170

MURATA_2EL

x

-

AW300 only

BLE/Classic

BLE/Classic

BLE/Classic/LE Audio

BLE

BLE/Classic

-

evkcmimxrt1060

MURATA_2EL

x

-

IW610 only

BLE/Classic

BLE/Classic

BLE/Classic/LE Audio

BLE

-

-

evkmimxrt595

MURATA_2EL

x

-

-

BLE/Classic

BLE/Classic

BLE/Classic

BLE

-

BLE

evkmimxrt685

MURATA_2EL

-

-

x

BLE/Classic

BLE/Classic

BLE/Classic

BLE

-

-

evkmimxrt1040

MURATA_1ZM

x

-

-

BLE

BLE

-

-

-

-

evkmimxrt1180

MURATA_2EL

x

-

-

BLE/Classic

BLE/Classic

BLE/Classic

BLE

-

-

frdmmcxn947

MURATA_2LL + adapter

-

x

-

BLE/Classic

-

-

BLE

-

-

frdmmcxn947t

MURATA_2LL + adapter

-

x

-

BLE/Classic

-

-

BLE

-

-

mcxn5xxevk

MURATA_1XK

x

-

-

BLE/Classic

-

-

BLE

-

-

mcxn9xxevk

MURATA_1XK

x

-

-

BLE/Classic

-

-

BLE

-

-

mimxrt685audevk

MURATA_2EL

x

-

-

BLE/Classic

BLE/Classic

BLE/Classic

BLE

-

-

mimxrt700evk

MURATA_2EL

x

-

-

BLE/Classic

BLE/Classic

BLE/Classic/LE Audio

BLE

-

-

Board

Default Module

support feature

frdmimxrt700

IW612

BLE/Classic/LE Audio

frdmimxrt1152

IW612

BLE/Classic

frdmrw612

-

BLE

rdrw612bga

-

BLE

Notes#

  • x in a Default Interface column indicates the physical interface used on that board to connect the default module.

  • BLE means only Bluetooth Low Energy is supported.

  • BLE/Classic means both BLE and Bluetooth Classic are supported.

  • BLE/Classic/LE Audio means BLE, Bluetooth Classic, and LE Audio are all supported.

Parent topic:Hardware