eIQ MPP Hardware Abstraction Layer API#
MPP-HAL VERSION 4.4
Chapter 1#
This is the documentation for the Hardware Abstraction Layer (HAL) API.
1.1 HAL overview#
The hardware abstraction layer abstracts hardware and software components so that the vision pipeline can leverage hardware-accelerated components whenever they are available.
1.1.1 MPP HAL description#
The HAL is organized around the following conventions:
A common header file hal.h includes all hardware top-level functions.
All hardware top-level functions use the prefix hal_ .
For each platform, all hal_ functions defined in hal.h must be implemented (at least as empty stubs).
Here is an overview:

Figure 1.1 HAL overview
1.1.2 MPP HAL components#
Source elements HAL
Camera (MIPI CSI, FlexIO, USB/UVC)
Static image (from memory buffer)
File source (from SD card storage)
Multicore source (receive frames from another core over RPMsg)
Processing elements HAL
Graphics driver (image conversion, scaling, cropping, rotation, flip)
Image decoder (JPEG SW/HW, H.264 SW)
Vision algorithms (ML inference: TFLite, ExecuTorch)
Labeled rectangle and landmarks drawing
Sink elements HAL
Display panel
File sink (write to SD card)
RTSP/RTP network streaming sink
Null sink
Multicore sink (send frames to another core over RPMsg)
Multicore HAL The
hal_mccomponent provides inter-core communication for multicore pipelines on SoCs such as i.MX RT1170 (CM7 + CM4). It implements themc_dev_operator_tinterface and handles:
RPMsg endpoint creation and teardown
Shared-memory buffer negotiation between cores
Synchronization locks for exclusive buffer access
Enqueue/dequeue of frame buffers to/from the remote core
MCMGR event signalling (when HAL_ENABLE_MULTICORE=1 ) The multicore HAL is enabled by setting
HAL_ENABLE_MULTICORE=1inmpp_config.h.
1.1.3 Supported devices#
At present, the MPP HAL supports the following devices:
Cameras:
OV5640 (MIPI CSI)
MT9M114 (parallel, deprecated)
OV7670 (FlexIO)
USB UVC cameras (e.g. Logitech C920 PRO HD WEBCAM)
Displays:
LVGL (software framebuffer)
RK055AHD091 (MIPI DSI 720x1280)
RK055MHD091 (MIPI DSI 720x1280)
RK043FN02H-CT (parallel, deprecated)
Mikroe TFT Proto 5” (SSD1963 controller, FlexIO/LCD DBI)
NXP LCD-PAR-S035 (ST7796S controller, 8080 parallel)
FBdev (Linux framebuffer)
Zephyr display (via Zephyr display driver API)
Graphics:
PXP (Pixel Pipeline, hardware accelerated)
VGLite (GPU, hardware accelerated)
CPU (software)
Image decoders:
JPEG SW decoder
JPEG HW decoder
H.264 SW decoder
Storage:
SD card (FatFS)
RTSP/RTP streaming:
H.264 RTP streaming over UDP
Multicore communication:
RPMsg + MCMGR (i.MX RT1170 CM7/CM4)
1.1.4 Supported boards#
Currently, the MPP HAL supports the following boards:
evkbmimxrt1170 is supported with the following devices:
Cameras: OV5640.
Displays: LVGL, RK055AHD091 and RK055MHD091.
Graphics: PXP, CPU.
Decoders: JPEG SW, JPEG HW.
frdmmcxn947 is supported with the following devices:
Cameras: OV7670.
Displays: Mikroe TFT Proto 5” and NXP LCD-PAR-S035.
Graphics: CPU.
Decoders: JPEG SW.
mimxrt700evk is supported with the following devices:
Cameras: OV7670, USB UVC (Logitech C920 PRO HD WEBCAM).
Displays: RK055AHD091 and RK055MHD091.
Graphics: PXP, VGLite, CPU.
Decoders: JPEG SW, JPEG HW.
Storage: SD card.
Streaming: RTSP/RTP H.264 (multicore: core0 + core1).
Multicore: RPMsg + MCMGR (CM33 + CM33).
frdmimxrt700 is supported with the following devices:
Cameras: OV7670, USB UVC.
Displays: Raspberry Pi 7”.
Graphics: VGLite, CPU.
Decoders: JPEG SW, JPEG HW.
Storage: SD card.
frdmimxrt1152 is supported with the following devices:
Cameras: OV5640.
Displays: RK055AHD091 and RK055MHD091.
Graphics: PXP, CPU.
Decoders: JPEG SW, JPEG HW.
How to port new boards/devices: The MPP HAL provides the flexibility for users to port new boards and devices (cameras, displays, etc.).
Supporting new boards:
To support a new board, add a new file hal_{board_name}.c under the hal/ directory. The file must implement all hardware-specific setup functions declared in hal.h.
Supporting new devices: The HAL components that can support new devices are:
Cameras
Displays
Graphics processing
A new device can be supported by:
Providing the appropriate hal_{device_module} implementation.
Adding its name and setup entry point to the appropriate device list in the associated board file hal_{board_name}.c .
Enabling/Disabling HAL components and devices:
HAL components can be enabled or disabled from mpp_config.h using compilation flags of the form HAL_ENABLE_{COMPONENT_NAME} .
Individual HAL devices can also be enabled or disabled from mpp_config.h using flags of the form HAL_ENABLE_{DEVICE_NAME} .
Chapter 2#
Data Structures
struct camera_dev_static_config_t
struct _camera_dev
struct virtual_usb_cam_config_msg_t
struct virtual_usb_cam_req_msg_t
struct virtual_usb_cam_rsp_msg_t
struct virtual_usb_cam_msg_t
struct static_image_static_config_t
struct _static_image
struct filesrc_config_t
struct _filesrc
struct filesink_config_t
struct _filesink
struct rtspsink_config_t
struct _rtspsink
struct rtspsrc_config_t
struct _rtspsrc
struct gfx_surface_t
struct gfx_rotate_config_t
struct _gfx_dev
struct hal_rect_t
struct vdec_h264_frame_info_t
struct _vdec_dev
struct _vdec_h264_dev
struct model_param_t
struct vision_frame_t
struct _vision_algo_dev
struct _display_dev
struct hw_buf_desc_t
struct hal_img_decoder_setup_t
struct hal_graphics_setup_t
struct hal_display_setup_t
struct hal_camera_setup_t
struct checksum_data_t
struct mc_dev_operator_t
struct mc_dev_static_buf_config
struct mc_dev_static_config_t
struct _multicore_dev
struct venc_h264_frame_info_t
struct _venc_h264_dev
Macros
#define MAX_STREAM_REQUESTERS
#define TARGET_CAMERA0_WIDTH
#define TARGET_CAMERA0_HEIGHT
#define TARGET_CAMERA1_WIDTH
#define TARGET_CAMERA1_HEIGHT
#define TARGET_CAMERA0_RESOLUTION
#define TARGET_CAMERA1_RESOLUTION
#define TARGET_CAMERA_MAX_RESOLUTION
#define TARGET_CAMERA_FPS
#define CAMERA_DEV_BUFFER_ALIGN
#define CORE1_EPT_ADDRESS
#define MPP_EPT_ADDRESS
#define RTSP_EPT_ADDRESS
#define APP_EP_READY_EVENT_DATA
#define FILE_SOURCE_FILEPATH_MAX_LEN
#define FILE_SINK_FILEPATH_MAX_LEN
#define HAL_GFX_DEV_CPU_NAME
#define GUI_PRINTF_BUF_SIZE
#define HAL_VDEC_DEV_NAME
#define MAX_INPUT_PORTS
#define MAX_OUTPUT_PORTS
#define HAL_DEVICE_NAME_MAX_LENGTH
#define HAL_VENC_DEV_NAME
Typedefs
typedef int(* camera_dev_callback_t)(const camera_dev_t *dev, camera_event_t event, void *param, uint8_t fromISR)
typedef void * vision_algo_private_data_t
typedef int(* mpp_callback_t)(mpp_t mpp, mpp_evt_t evt, void *evt_data, void *user_data)
typedef int(* img_decoder_setup_func_t)(vdec_dev_t *)
typedef int(* graphic_setup_func_t)(gfx_dev_t *)
typedef int(* display_setup_func_t)(display_dev_t *)
typedef int(* camera_setup_func_t)(const char *, camera_dev_t *)
Enumerations
enum hal_camera_status_t {
enum camera_event_t {
enum virtual_usb_cam_msg_type_e {
enum virtual_usb_cam_user_id_e {
enum virtual_usb_cam_col_format_e {
enum hal_image_status_t {
enum hal_filesrc_status_t {
enum hal_filesink_status_t {
enum gfx_rotate_target_t {
enum hal_vdec_status_t {
enum hal_valgo_status_t {
enum display_event_t {
enum hal_display_status_t {
enum mpp_memory_policy_t {
enum checksum_type_t {
enum hal_mc_status_t {
enum hal_mc_dev_type_t {
enum hal_venc_status_t {
Functions
int search_h264_nalu (const uint8_t * data, int32_t len)
int HAL_GfxDev_CPU_Register (gfx_dev_t * dev)
int HAL_GfxDev_GPU_Register (gfx_dev_t * dev)
void HAL_JPEG_PrintValidationStats (void)
int HAL_JPEG_CPU_Register (vdec_dev_t * dev)
int HAL_JPEG_HW_Register (vdec_dev_t * dev)
hal_vdec_status_t HAL_VdecDev_H264_CPU_Register (vdec_h264_dev_t * dev)
int setup_static_image_elt (static_image_t * elt)
int setup_filesrc_elt (filesrc_t * elt)
int setup_rtspsrc_elt (rtspsrc_t * elt)
uint32_t calc_checksum (int size_b, void * pbuf)
hal_venc_status_t HAL_VencDev_H264_CPU_Register (venc_h264_dev_t * dev)
2.1 HAL Types#
This section provides the detailed documentation for the MPP HAL types.
2.1.1 Function Documentation#
search_h264_nalu#
int search_h264_nalu ( const uint8_t * data, int32_t len )
Search function for H.264 NALU boundaries.
This function searches for H.264 Network Abstraction Layer Unit (NALU) start codes in the provided data buffer. It looks for:
4-byte start code: 0x00 0x00 0x00 0x01
3-byte start code: 0x00 0x00 0x01
Parameters
in/out |
name |
description |
|---|---|---|
in |
data |
Pointer to buffer containing H.264 bitstream data |
in |
len |
Length of data in buffer (bytes) |
Returns
Offset to next NALU start code, or -1 if not found
HAL_GfxDev_CPU_Register#
int HAL_GfxDev_CPU_Register ( gfx_dev_t * dev )
Register the graphic device with the CPU operations.
Parameters
in/out |
name |
description |
|---|---|---|
in |
dev |
graphic device to register |
Returns
error code (0: success, otherwise: failure)
HAL_GfxDev_GPU_Register#
int HAL_GfxDev_GPU_Register ( gfx_dev_t * dev )
Register the graphic device with the GPU operations.
Parameters
in/out |
name |
description |
|---|---|---|
in |
dev |
graphic device to register |
Returns
error code (0: success, otherwise: failure)
HAL_JPEG_PrintValidationStats#
void HAL_JPEG_PrintValidationStats ( void )
Print JPEG decoding validation statistics to the debug console.
HAL_JPEG_CPU_Register#
int HAL_JPEG_CPU_Register ( vdec_dev_t * dev )
Register the jpeg SW decoder device.
Parameters
in/out |
name |
description |
|---|---|---|
in |
dev |
decoder device to register |
Returns
error code (0: success, otherwise: failure)
HAL_JPEG_HW_Register#
int HAL_JPEG_HW_Register ( vdec_dev_t * dev )
Register the jpeg HW decoder device.
Parameters
in/out |
name |
description |
|---|---|---|
in |
dev |
decoder device to register |
Returns
error code (0: success, otherwise: failure)
HAL_VdecDev_H264_CPU_Register#
hal_vdec_status_t HAL_VdecDev_H264_CPU_Register ( vdec_h264_dev_t * dev )
Register the H.264 SW decoder device.
Parameters
in/out |
name |
description |
|---|---|---|
in |
dev |
decoder device to register |
Returns
error code (0: success, otherwise: failure)
setup_static_image_elt#
int setup_static_image_elt ( static_image_t * elt )
Register the static image source element.
Parameters
in/out |
name |
description |
|---|---|---|
in |
elt |
static image element to register |
Returns
error code (0: success, otherwise: failure)
setup_filesrc_elt#
int setup_filesrc_elt ( filesrc_t * elt )
Register the file source element.
Parameters
in/out |
name |
description |
|---|---|---|
in |
elt |
file source element to register |
Returns
error code (0: success, otherwise: failure)
setup_rtspsrc_elt#
int setup_rtspsrc_elt ( rtspsrc_t * elt )
Register the RTSP source element.
Parameters
in/out |
name |
description |
|---|---|---|
in |
elt |
RTSP source element to register |
Returns
error code (0: success, otherwise: failure)
calc_checksum#
uint32_t calc_checksum ( int size_b, void * pbuf )
Compute a 32-bit checksum over a memory buffer.
Parameters
in/out |
name |
description |
|---|---|---|
in |
size_b |
buffer size in bytes |
in |
pbuf |
pointer to the buffer |
Returns
32-bit checksum value
HAL_VencDev_H264_CPU_Register#
hal_venc_status_t HAL_VencDev_H264_CPU_Register ( venc_h264_dev_t * dev )
Register the H.264 SW encoder device.
Parameters
in/out |
name |
description |
|---|---|---|
in |
dev |
encoder device to register |
Returns
error code (0: success, otherwise: failure)
2.1.2 Data Structure Documentation#
camera_dev_static_config_t#
struct camera_dev_static_config_t
Structure that characterizes the camera device.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
buffer height |
int |
width |
buffer width |
int |
pitch |
buffer pitch |
int |
left |
left position |
int |
top |
top position |
int |
right |
right position |
int |
bottom |
bottom position |
mpp_rotate_degree_t |
rotate |
rotate degree |
mpp_flip_mode_t |
flip |
flip |
int |
swapByte |
swap byte per two bytes |
mpp_pixel_format_t |
format |
pixel format |
int |
framerate |
frame rate |
int |
stripe_size |
stripe size in bytes |
bool |
stripe |
stripe mode |
uint32_t |
n_streams |
number of total output video streams |
uint32_t |
min_stream_req_cnt |
minimum number of enqueue calls to wait for |
uint32_t |
crt_stream_req_cnt |
number of streams requested for enqueue |
mpp_exec_flag_t |
req_cnt_type |
flag to control stream request counting |
mpp_camera_stream_cfg |
stream[NUM_STREAMS] |
stream configuration |
bool |
stream_requested[NUM_STREAMS] |
flag to track if a stream is required for enqueue |
void * |
stream_requester[NUM_STREAMS][MAX_STREAM_REQUESTERS] |
array of requesters for each stream |
bool |
in_advance_enqueue |
flag to indicate advance enqueue mode |
camera_dev_private_capability_t#
struct camera_dev_private_capability_t
camera device private capability.
Data Fields
type |
name |
description |
|---|---|---|
callback |
callback |
|
void * |
param |
parameter for the callback |
_camera_dev#
struct _camera_dev
Attributes of a camera device.
Data Fields
type |
name |
description |
|---|---|---|
int |
id |
unique id which is assigned by camera manager during registration |
char |
name[HAL_DEVICE_NAME_MAX_LENGTH] |
name of the device |
const camera_dev_operator_t * |
ops |
operations |
config |
static configurations |
|
cap |
private capability |
|
void * |
data |
device private data |
virtual_usb_cam_config_msg_t#
struct virtual_usb_cam_config_msg_t
Structure that characterizes the payload of the camera config message sent from core 0 to core 1.
Data Fields
type |
name |
description |
|---|---|---|
uint32_t |
camera_width |
Width of the camera output in pixels. |
uint32_t |
camera_height |
Height of the camera output in pixels. |
color_format |
Color format for the camera output (e.g., JPEG) |
|
uint32_t |
fps |
Frames per second for camera capture rate. |
virtual_usb_cam_req_msg_t#
struct virtual_usb_cam_req_msg_t
Structure that characterizes the payload of the camera request message containing frame buffer addresses for RGB and IR data.
Data Fields
type |
name |
description |
|---|---|---|
uint32_t |
rgb_frame_addr |
Physical address of the RGB frame buffer. |
uint32_t |
rgb_max_frame_size |
Maximum size allocated for RGB frame buffer. |
uint32_t |
ir_frame_addr |
Physical address of the IR frame buffer. |
uint32_t |
ir_max_frame_size |
Maximum size allocated for IR frame buffer. |
virtual_usb_cam_rsp_msg_t#
struct virtual_usb_cam_rsp_msg_t
Structure that characterizes the payload of the camera request message containing frame addresses and sizes for RGB and IR data.
Data Fields
type |
name |
description |
|---|---|---|
uint32_t |
rgb_frame_addr |
Physical address of the RGB frame buffer (looped back by the core 1 camera app) |
uint32_t |
rgb_frame_size |
Size in bytes of the RGB frame data. |
uint32_t |
ir_frame_addr |
Physical address of the IR frame buffer (looped back by the core 1 camera app) |
uint32_t |
ir_frame_size |
Size in bytes of the IR frame data. |
virtual_usb_cam_msg_t#
struct virtual_usb_cam_msg_t
Structure that characterizes the messages sent between cores.
Data Fields
type |
name |
description |
|---|---|---|
msg_type |
Type of message being sent (config, request, response, etc.) |
|
user_id |
Identifier for the user/component sending the message (RTSP or MPP) |
|
msg_payload |
Union containing the actual message data based on msg_type. |
static_image_static_config_t#
struct static_image_static_config_t
Structure that characterize the image element.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
buffer height |
int |
width |
buffer width |
int |
left |
left position |
int |
top |
top position |
int |
right |
right position |
int |
bottom |
bottom position |
mpp_pixel_format_t |
format |
pixel format |
bool |
stripe |
stripe mode |
int |
compressed_size |
compressed size in bytes |
_static_image#
struct _static_image
Attributes of an image element.
Data Fields
type |
name |
description |
|---|---|---|
int |
id |
unique id which is assigned by image manager |
const static_image_operator_t * |
ops |
operations |
config |
static configs |
|
int |
stripe_idx |
the current stripe index |
uint8_t * |
buffer |
static image buffer |
filesrc_config_t#
struct filesrc_config_t
Structure that characterize the file source element.
Data Fields
type |
name |
description |
|---|---|---|
char |
filepath[FILE_SOURCE_FILEPATH_MAX_LEN] |
File name to read. |
bool |
loop_enabled |
Flag to enable looping the file. |
int |
file_buffer_size |
File buffer size in bytes. |
slice_search_func_t |
slice_search_func |
Optional slice search function. |
_filesrc#
struct _filesrc
Attributes of a file source element.
Data Fields
type |
name |
description |
|---|---|---|
const filesrc_operator_t * |
ops |
operations |
config |
file source configs |
|
uint8_t * |
buffer |
Pointer to file read buffer. |
uint32_t |
buffer_size |
File read buffer size. |
filesink_config_t#
struct filesink_config_t
Structure that characterize the file sink element.
Data Fields
type |
name |
description |
|---|---|---|
char |
filepath[FILE_SINK_FILEPATH_MAX_LEN] |
File name to write. |
bool |
append_mode |
Flag to enable append mode. |
_filesink#
struct _filesink
Attributes of a file sink element.
Data Fields
type |
name |
description |
|---|---|---|
const filesink_operator_t * |
ops |
operations |
config |
file sink configs |
rtspsink_config_t#
struct rtspsink_config_t
Structure that characterize the RTSP sink element.
Data Fields
type |
name |
description |
|---|---|---|
uint16_t |
port |
RTSP server port number. |
char |
ip_addr[IPV4_STR_LEN] |
destination IP address string |
uint32_t |
frame_width |
video frame width in pixels |
uint32_t |
frame_height |
video frame height in pixels |
rtp_payload_type_t |
payload_type |
RTP payload type. |
rtp_frame_type_t |
frame_type |
RTP frame type. |
_rtspsink#
struct _rtspsink
Attributes of an RTSP sink element.
Data Fields
type |
name |
description |
|---|---|---|
const rtspsink_operator_t * |
ops |
operations |
config |
RTSP sink configuration. |
rtspsrc_config_t#
struct rtspsrc_config_t
Configuration parameters kept inside the RTSP source device.
Data Fields
char rtsp_url[RTSP_URL_MAX_LEN]
_rtspsrc#
struct _rtspsrc
Attributes of an RTSP source element.
Data Fields
type |
name |
description |
|---|---|---|
const rtspsrc_operator_t * |
ops |
Operations. |
config |
RTSP source config. |
|
uint8_t * |
buffer |
Frame reassembly buffer (HAL-allocated) |
uint32_t |
buffer_size |
Size of buffer in bytes. |
gfx_surface_t#
struct gfx_surface_t
Gfx surface parameters.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
buffer height |
int |
width |
buffer width |
int |
pitch |
buffer pitch |
int |
pitch_uv |
buffer pitch for chroma planes |
int |
left |
left position |
int |
top |
top position |
int |
right |
right position |
int |
bottom |
bottom position |
int |
swapByte |
swap byte per two bytes |
mpp_pixel_format_t |
format |
pixel format |
void * |
buf |
buffer |
void * |
buf_u |
buffer for chroma plane U |
void * |
buf_v |
buffer for chroma plane V |
void * |
lock |
the structure is determined by hal and set to null if not use in hal |
gfx_rotate_config_t#
struct gfx_rotate_config_t
gfx rotate configuration
Data Fields
gfx_rotate_target_t target
mpp_rotate_degree_t degree
float custom_angle
_gfx_dev#
struct _gfx_dev
Attributes of a graphics device.
Data Fields
type |
name |
description |
|---|---|---|
int |
id |
unique id |
const gfx_dev_operator_t * |
ops |
operations |
src |
graphic source surface |
|
dst |
graphic destination surface |
|
callback |
callback |
|
void * |
cb_user_data |
param for the callback |
void * |
user_data |
stores the vglite context pointer |
mpp_t |
mpp |
mpp handle to be passed to the callback |
hal_rect_t#
struct hal_rect_t
rectangle positions.
Data Fields
int top
int left
int bottom
int right
vdec_h264_frame_info_t#
struct vdec_h264_frame_info_t
H.264 decode frame information structure.
Data Fields
type |
name |
description |
|---|---|---|
uint8_t * |
src_data |
pointer to input compressed H.264 bitstream |
int32_t |
src_size |
size of input bitstream in bytes |
uint8_t * |
dst_y |
pointer to output luma (Y) plane |
uint8_t * |
dst_u |
pointer to output chroma U plane |
uint8_t * |
dst_v |
pointer to output chroma V plane |
int32_t |
width |
decoded frame width in pixels |
int32_t |
height |
decoded frame height in pixels |
int32_t |
y_stride |
luma plane stride in bytes |
int32_t |
uv_stride |
chroma plane stride in bytes |
_vdec_dev#
struct _vdec_dev
Attributes of a JPEG/image decoder device.
Data Fields
type |
name |
description |
|---|---|---|
int |
id |
unique id |
const vdec_dev_operator_t * |
ops |
operations |
callback |
callback |
|
void * |
user_data |
param for the callback |
_vdec_h264_dev#
struct _vdec_h264_dev
Attributes of an H.264 decoder device.
Data Fields
type |
name |
description |
|---|---|---|
int |
id |
unique id |
const vdec_h264_dev_operator_t * |
ops |
operations |
callback |
callback |
|
void * |
user_data |
param for the callback |
model_param_t#
struct model_param_t
Structure passed to HAL as description of the binary model provided by user.
Data Fields
type |
name |
description |
|---|---|---|
const void * |
model_data |
pointer to model binary |
int |
model_size |
model binary size |
float |
model_input_mean |
model ‘mean’ of input values, used for normalization |
float |
model_input_std |
model ‘standard deviation’ of input values, used for normalization |
uint32_t |
model_id |
unique model identifier |
mpp_inference_params_t |
inference_params |
inference parameters |
int |
height |
frame height |
int |
width |
frame width |
mpp_pixel_format_t |
format |
pixel format |
mpp_tensor_type_t |
inputType |
input type |
mpp_tensor_order_t |
tensor_order |
tensor order |
mpp_t |
mpp |
mpp handle |
int |
(*evt_callback_f)(mpp_t mpp, mpp_evt_t evt, void *evt_data, void *user_data) |
the callback to be called when model output is ready |
void * |
cb_userdata |
pointer to user data, should be passed by callback |
valgo_dev_private_capability_t#
struct valgo_dev_private_capability_t
Valgo devices private capability.
Data Fields
type |
name |
description |
|---|---|---|
void * |
param |
param for the callback |
vision_frame_t#
struct vision_frame_t
Characteristics that need to be defined by a vision algo.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
frame height |
int |
width |
frame width |
int |
pitch |
frame pitch |
mpp_pixel_format_t |
format |
pixel format |
void * |
input_buf |
pixel input buffer |
_vision_algo_dev#
struct _vision_algo_dev
Attributes of a vision algo device.
Data Fields
type |
name |
description |
|---|---|---|
int |
id |
unique id which is assigned by algorithm manager during the registration |
char |
name[HAL_DEVICE_NAME_MAX_LENGTH] |
name to identify |
cap |
private capability |
|
const vision_algo_dev_operator_t * |
ops |
operations |
priv_data |
private data |
_display_dev_private_capability#
struct _display_dev_private_capability
Structure that characterizes the display device.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
buffer height |
int |
width |
buffer width |
int |
pitch |
buffer pitch |
int |
left |
left position |
int |
top |
top position |
int |
right |
right position |
int |
bottom |
bottom position |
int |
stripe_height |
stripe height (0 if stripe mode is off) |
bool |
stripe |
stripe mode |
mpp_rotate_degree_t |
rotate |
rotate degree |
mpp_pixel_format_t |
format |
pixel format |
int |
nbFrameBuffer |
number of input buffers |
void ** |
frameBuffers |
array of pointers to frame buffer |
callback |
callback |
|
void * |
user_data |
parameter for the callback |
void * |
handle |
Handle to the LVGL widget ‘image’. |
void ** |
p_in_buf_addr |
Pointer to current input buffer address. |
_display_dev#
struct _display_dev
Attributes of a display device.
hal display device declaration. Display devices can be used to display images, GUI overlays, etc. Examples of display devices include display panels like the RK024hh298 display, and external displays like UVC (video over USB).
Data Fields
type |
name |
description |
|---|---|---|
int |
id |
unique id which is assigned by the display manager during the registration |
char |
name[HAL_DEVICE_NAME_MAX_LENGTH] |
name of the device |
const display_dev_operator_t * |
ops |
operations |
display_dev_private_capability_t |
cap |
private capability |
void * |
data |
device private data |
hw_buf_desc_t#
struct hw_buf_desc_t
the hardware specific buffer requirements
Data Fields
type |
name |
description |
|---|---|---|
int |
stride |
the number of bytes between 2 lines of image |
int |
stride_uv |
the number of bytes between 2 lines of UV planes (for planar YUV formats) |
int |
nb_lines |
the number of lines required (set to 0 if the element doesn’t require a specific number of lines) |
int |
alignment |
alignment requirement in bytes |
int |
max_image_size |
the number of bytes allocated |
bool |
cacheable |
if true, HW will require cache maintenance |
unsigned char * |
addr |
the aligned buffer address |
unsigned char * |
addr_u |
the aligned buffer address for chroma plane U (for planar YUV formats) |
unsigned char * |
addr_v |
the aligned buffer address for chroma plane V (for planar YUV formats) |
unsigned char * |
heap_p |
pointer to the heap that should be freed |
hal_img_decoder_setup_t#
struct hal_img_decoder_setup_t
Video decoder setup descriptor.
Data Fields
type |
name |
description |
|---|---|---|
const char * |
vdec_dev_name |
name of the video decoder device |
decoder_setup_func |
pointer to the decoder setup function |
hal_graphics_setup_t#
struct hal_graphics_setup_t
Graphics device setup descriptor.
Data Fields
type |
name |
description |
|---|---|---|
const char * |
gfx_dev_name |
name of the graphics device |
gfx_setup_func |
pointer to the graphics setup function |
hal_display_setup_t#
struct hal_display_setup_t
Display device setup descriptor.
Data Fields
type |
name |
description |
|---|---|---|
const char * |
display_name |
name of the display device |
display_setup_func |
pointer to the display setup function |
hal_camera_setup_t#
struct hal_camera_setup_t
Camera device setup descriptor.
Data Fields
type |
name |
description |
|---|---|---|
const char * |
camera_name |
name of the camera device |
camera_setup_func |
pointer to the camera setup function |
checksum_data_t#
struct checksum_data_t
computed checksum
Data Fields
type |
name |
description |
|---|---|---|
type |
checksum calculation method |
|
uint32_t |
value |
checksum value |
mc_dev_operator_t#
struct mc_dev_operator_t
Operation that needs to be implemented by a mc device.
Data Fields
type |
name |
description |
|---|---|---|
(*init)(multicore_dev_t *dev, mpp_mc_params_t *config, hal_mc_dev_type_t type) |
initialize the dev |
|
(*deinit)(multicore_dev_t *dev) |
deinitialize the dev |
|
(*start)(multicore_dev_t *dev) |
start the dev |
|
(*stop)(multicore_dev_t *dev) |
stop the dev |
|
(*enqueue)(const multicore_dev_t *dev, void **data, int *compressed_size, int *stripe, unsigned short *frame_id) |
enqueue a buffer to the dev |
|
(*dequeue)(const multicore_dev_t *dev, void **data, int *compressed_size, int *stripe, unsigned short *frame_id) |
dequeue a buffer from the dev (blocking) |
|
(*get_buf_desc)(const multicore_dev_t *dev, void *io_desc, mpp_memory_policy_t prev_mem_policy) |
get buffer descriptors and policy |
|
(*lock)(const multicore_dev_t *dev) |
lock the device for exclusive access and operations |
|
(*unlock)(const multicore_dev_t *dev) |
unlock the device after exclusive operations |
mc_dev_static_buf_config#
struct mc_dev_static_buf_config
Static buffer configuration for mc device.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
buffer height |
int |
width |
buffer width |
int |
pitch |
buffer pitch |
mpp_pixel_format_t |
format |
pixel format |
int |
stripe_size |
stripe size in bytes |
bool |
stripe |
stripe mode |
uint32_t |
compressed_size |
compressed buffer size in bytes |
mc_dev_static_config_t#
struct mc_dev_static_config_t
Structure that characterizes the mc device.
Data Fields
type |
name |
description |
|---|---|---|
dev_type |
device type (sink or source) |
|
buf_config[MAX_OUTPUT_PORTS] |
buffer configuration |
|
bool |
initial_enqueue_done |
flag to indicate if initial enqueue is done |
uint32_t |
min_req_cnt |
minimum number of buffers required |
uint32_t |
crt_req_cnt |
current number of buffers requested |
mpp_exec_flag_t |
req_exec_type |
execution type for buffer requests |
bool |
requested[MAX_OUTPUT_PORTS] |
buffer request status |
bool |
enqueued[MAX_OUTPUT_PORTS] |
buffer enqueued status |
void * |
buff_desc[MAX_OUTPUT_PORTS] |
hw address to receive data |
int |
(*callback)(mpp_t mpp, mpp_evt_t evt, void *evt_data, void *user_data) |
optional pipeline event callback - set before calling init to receive MPP_EVENT_MC_REMOTE_DEINIT |
void * |
cb_user_data |
opaque pointer forwarded to callback |
_multicore_dev#
struct _multicore_dev
Attributes of a multicore device.
hal mc device declaration. This multicore hardware abstraction layer provides interfaces for multicore communication between elements of pipeline running on different core (multicore sink and multicore source elements).
Data Fields
type |
name |
description |
|---|---|---|
int |
id |
unique id which is assigned by mc manager during registration |
char |
name[HAL_DEVICE_NAME_MAX_LENGTH] |
name of the device |
const mc_dev_operator_t * |
ops |
operations |
config |
static configurations |
|
void * |
data |
device private data |
venc_h264_frame_info_t#
struct venc_h264_frame_info_t
H.264 encode frame information structure.
Data Fields
mpp_pixel_format_t format
uint8_t * src_y
uint8_t * src_u
uint8_t * src_v
int32_t y_stride
int32_t uv_stride
int32_t width
int32_t height
uint8_t * dst
int32_t dst_size
bool intraframe
_venc_h264_dev#
struct _venc_h264_dev
Attributes of an H.264 encoder device.
Data Fields
type |
name |
description |
|---|---|---|
int |
id |
unique id |
const venc_h264_dev_operator_t * |
ops |
operations |
callback |
callback function |
|
void * |
user_data |
parameter for the callback |
2.1.3 Macro Definition Documentation#
MAX_STREAM_REQUESTERS#
#define MAX_STREAM_REQUESTERS
hal camera device declaration.
Camera devices can enqueue and dequeue frames as well as react to events from input devices via the “inputNotify” function. Camera devices can use any number of interfaces, including MIPI and CSI as long as the HAL driver implements the necessary functions found in camera_dev_operator_t . Examples of camera devices include the Orbbec U1S 3D SLM camera module and the OnSemi MT9M114 camera module.
TARGET_CAMERA0_WIDTH#
#define TARGET_CAMERA0_WIDTH
Default width in pixels of camera output for camera 0.
TARGET_CAMERA0_HEIGHT#
#define TARGET_CAMERA0_HEIGHT
Default height in pixels of camera output for camera 0.
TARGET_CAMERA1_WIDTH#
#define TARGET_CAMERA1_WIDTH
Default width in pixels of camera output for camera 1.
TARGET_CAMERA1_HEIGHT#
#define TARGET_CAMERA1_HEIGHT
Default height in pixels of camera output for camera 1.
TARGET_CAMERA0_RESOLUTION#
#define TARGET_CAMERA0_RESOLUTION
Total pixel count for camera 0 resolution.
TARGET_CAMERA1_RESOLUTION#
#define TARGET_CAMERA1_RESOLUTION
Total pixel count for camera 1 resolution.
TARGET_CAMERA_MAX_RESOLUTION#
#define TARGET_CAMERA_MAX_RESOLUTION
Maximum pixel count across all camera resolutions.
TARGET_CAMERA_FPS#
#define TARGET_CAMERA_FPS
Default camera capture rate in frames per second.
CAMERA_DEV_BUFFER_ALIGN#
#define CAMERA_DEV_BUFFER_ALIGN
Buffer alignment requirement for camera device buffers in bytes.
CORE1_EPT_ADDRESS#
#define CORE1_EPT_ADDRESS
Endpoint address for Core 1 inter-core communication channel.
MPP_EPT_ADDRESS#
#define MPP_EPT_ADDRESS
Endpoint address for MPP (Media Processing Pipeline) inter-core communication channel.
MPP might use a range of endpoints starting with 40 and up to 49 included
RTSP_EPT_ADDRESS#
#define RTSP_EPT_ADDRESS
Endpoint address for RTSP (Real Time Streaming Protocol) inter-core communication channel.
APP_EP_READY_EVENT_DATA#
#define APP_EP_READY_EVENT_DATA
Event data value indicating that the application endpoint is ready for communication.
FILE_SOURCE_FILEPATH_MAX_LEN#
#define FILE_SOURCE_FILEPATH_MAX_LEN
Maximum file path length for file source elements.
FILE_SINK_FILEPATH_MAX_LEN#
#define FILE_SINK_FILEPATH_MAX_LEN
Maximum file path length for file sink elements.
HAL_GFX_DEV_CPU_NAME#
#define HAL_GFX_DEV_CPU_NAME
hal graphics (gfx) device declaration.
Graphics processing devices can be used to perform conversion from one image format to another, resize images and compose images on top of one another. Examples of graphics devices include the PXP (pixel pipeline) found on many i.MXRT series MCUs. Name of the graphic device using CPU operations
GUI_PRINTF_BUF_SIZE#
#define GUI_PRINTF_BUF_SIZE
Local text buffer size.
HAL_VDEC_DEV_NAME#
#define HAL_VDEC_DEV_NAME
hal video decoder (vdec) device declaration.
Video decoder devices can be used to perform decompression of image. Examples of decoder devices include the PNG/JPEG HW or SW found on many i.MXRT series MCUs. Name of the jpeg decoder device using CPU operations
MAX_INPUT_PORTS#
#define MAX_INPUT_PORTS
HAL public types header.
maximum number of element inputs
MAX_OUTPUT_PORTS#
#define MAX_OUTPUT_PORTS
Maximum number of element outputs.
HAL_DEVICE_NAME_MAX_LENGTH#
#define HAL_DEVICE_NAME_MAX_LENGTH
maximum length of device name
HAL_VENC_DEV_NAME#
#define HAL_VENC_DEV_NAME
hal video encoder (venc) device declaration.
Video encoder devices can be used to perform compressing of image / video data. Examples of decoder devices include the H.264 SW encoder present in SDK. Name of the H.264 encoder device using CPU operations
2.1.4 Typedef Documentation#
camera_dev_callback_t#
typedef int(* camera_dev_callback_t)(const camera_dev_t *dev, camera_event_t event, void *param, uint8_t fromISR)
Callback function to notify camera manager that one frame is dequeued.
vision_algo_private_data_t#
typedef void * vision_algo_private_data_t
Opaque private data pointer for vision algorithm devices.
mpp_callback_t#
typedef int(* mpp_callback_t)(mpp_t mpp, mpp_evt_t evt, void *evt_data, void *user_data)
The mpp callback function prototype.
img_decoder_setup_func_t#
typedef int(* img_decoder_setup_func_t)(vdec_dev_t *)
Video decoder setup function pointer type.
graphic_setup_func_t#
typedef int(* graphic_setup_func_t)(gfx_dev_t *)
Graphics setup function pointer type.
display_setup_func_t#
typedef int(* display_setup_func_t)(display_dev_t *)
Display setup function pointer type.
camera_setup_func_t#
typedef int(* camera_setup_func_t)(const char *, camera_dev_t *)
Camera setup function pointer type.
2.1.5 Enumeration Type Documentation#
hal_camera_status_t#
enum hal_camera_status_t
{ kStatus_HAL_CameraSuccess,
kStatus_HAL_CameraBusy,
kStatus_HAL_CameraNoData,
kStatus_HAL_CameraNonBlocking,
kStatus_HAL_CameraError }
Camera return status.
camera_event_t#
enum camera_event_t
{ kCameraEvent_SendFrame,
kCameraEvent_CameraDeviceInit }
Type of events that are supported by calling the callback function.
virtual_usb_cam_msg_type_e#
enum virtual_usb_cam_msg_type_e
{ VIRT_USB_CAM_NOMSG,
VIRT_USB_CAM_CONFIG,
VIRT_USB_CAM_CONFIG_ACK,
VIRT_USB_CAM_CONFIG_ERR,
VIRT_USB_CAM_REQRGB,
VIRT_USB_CAM_REQIR,
VIRT_USB_CAM_REQRGBIR,
VIRT_USB_CAM_RSPRGB,
VIRT_USB_CAM_RSPIR,
VIRT_USB_CAM_RSPRGBIR,
VIRT_USB_CAM_ERROR }
Structure that characterizes the exchanged message types between core 0 and core 1.
virtual_usb_cam_user_id_e#
enum virtual_usb_cam_user_id_e
{ RTSP_USER_ID,
MPP_USER_ID }
User identifier for multicore virtual camera messages.
virtual_usb_cam_col_format_e#
enum virtual_usb_cam_col_format_e
{ VIRT_USB_CAM_JPEG }
Structure that characterizes the color format for the camera output.
hal_image_status_t#
enum hal_image_status_t
{ MPP_kStatus_HAL_ImageSuccess,
MPP_kStatus_HAL_ImageError }
static image return status
hal_filesrc_status_t#
enum hal_filesrc_status_t
{ MPP_kStatus_HAL_FileSrcSuccess,
MPP_kStatus_HAL_FileSrcError,
MPP_kStatus_HAL_FileSrcEOF }
File source return status.
hal_filesink_status_t#
enum hal_filesink_status_t
{ MPP_kStatus_HAL_FileSinkSuccess,
MPP_kStatus_HAL_FileSinkError }
File sink return status.
gfx_rotate_target_t#
enum gfx_rotate_target_t
{ kGFXRotateTarget_None,
kGFXRotate_SRCSurface,
kGFXRotate_DSTSurface }
gfx rotate target
hal_vdec_status_t#
enum hal_vdec_status_t
{ MPP_kStatus_HAL_VDecSuccess,
MPP_kStatus_HAL_VDecSkipped,
MPP_kStatus_HAL_VDecError }
video decoder return status
hal_valgo_status_t#
enum hal_valgo_status_t
{ kStatus_HAL_ValgoSuccess,
kStatus_HAL_ValgoMallocError,
kStatus_HAL_ValgoInitError,
kStatus_HAL_ValgoError,
kStatus_HAL_ValgoStop }
Valgo Error codes for hal operations.
display_event_t#
enum display_event_t
{ kDisplayEvent_RequestFrame }
Type of events that are supported by calling the callback function.
hal_display_status_t#
enum hal_display_status_t
{ kStatus_HAL_DisplaySuccess,
kStatus_HAL_DisplayTxBusy,
kStatus_HAL_DisplayNonBlocking,
kStatus_HAL_DisplayError }
Error codes for display hal devices.
mpp_memory_policy_t#
enum mpp_memory_policy_t
{ HAL_MEM_ALLOC_NONE,
HAL_MEM_ALLOC_INPUT,
HAL_MEM_ALLOC_OUTPUT,
HAL_MEM_ALLOC_BOTH }
The memory allocation policy of an element’s hal.
During the pipeline construction, the HAL uses this enum to tell the pipeline if it already owns input/ouput buffers. Before the pipeline starts, the memory manager will map the existing buffers to elements and allocate missing buffers from the heap.
checksum_type_t#
enum checksum_type_t
{ CHECKSUM_TYPE_PISANO,
CHECKSUM_TYPE_CRC_ELCDIF }
checksum calculation method
hal_mc_status_t#
enum hal_mc_status_t
{ kStatus_HAL_MultiCoreSuccess,
kStatus_HAL_MultiCoreError,
kStatus_HAL_MultiCoreNoDataReq }
multicore return status
hal_mc_dev_type_t#
enum hal_mc_dev_type_t
{ kHAL_MultiCoreDevTypeSink,
kHAL_MultiCoreDevTypeSource }
Multicore device type.
hal_venc_status_t#
enum hal_venc_status_t
{ MPP_kStatus_HAL_VEncSuccess,
MPP_kStatus_HAL_VEncError }
video encoder return status
Chapter 3#
Data Structures
struct camera_dev_operator_t
struct static_image_operator_t
struct filesrc_operator_t
struct filesink_operator_t
struct rtspsink_operator_t
struct rtspsrc_operator_t
struct gfx_dev_operator_t
struct vdec_dev_operator_t
struct vdec_h264_dev_operator_t
struct vision_algo_dev_operator_t
struct display_dev_operator_t
struct venc_h264_dev_operator_t
Typedefs
typedef int(* mpp_callback_t)(mpp_t mpp, mpp_evt_t evt, void *evt_data, void *user_data)
Functions
void GUI_DrawText (uint16_t * lcd_buf, uint16_t fcolor, uint16_t bcolor, uint32_t width, int x, int y, const char * label)
void hal_draw_pixel565 (uint16_t * pDst, uint32_t x, uint32_t y, uint16_t color, uint32_t lcd_w)
void hal_draw_text565 (uint16_t * lcd_buf, uint16_t fcolor, uint16_t bcolor, uint32_t width, int x, int y, const char * label, int stripe_top, int stripe_bottom)
void hal_draw_rect565 (uint16_t * lcd_buf, hal_rect_t rect, mpp_color_t rgb, uint32_t width, int stripe_top, int stripe_bottom)
int get_bitpp (mpp_pixel_format_t type)
void swap_2_bytes (uint8_t * data, int size)
3.1 HAL OPERATIONS#
This section provides the detailed documentation for the MPP HAL operations that needs to be implemented for each component.
3.1.1 Function Documentation#
GUI_DrawText#
void GUI_DrawText ( uint16_t * lcd_buf, uint16_t fcolor, uint16_t bcolor, uint32_t width, int x, int y, const char * label )
Draws text stored in label pointer to LCD buffer.
This function copy content of data from label text buffer to the LCD.
Parameters
in/out |
name |
description |
|---|---|---|
lcd_buf |
LCD buffer address destination for drawing text |
|
fcolor |
foreground color in rgb565 format |
|
bcolor |
background color in rgb565 format |
|
width |
LCD width |
|
x |
drawing position on X axe |
|
y |
drawing position on Y axe |
|
label |
C string pointed by label |
hal_draw_pixel565#
void hal_draw_pixel565 ( uint16_t * pDst, uint32_t x, uint32_t y, uint16_t color, uint32_t lcd_w )
Draws pixel with RGB565 color to defined point.
Parameters
in/out |
name |
description |
|---|---|---|
pDst |
image data address of destination buffer |
|
x |
drawing position on X axe |
|
y |
drawing position on Y axe |
|
color |
RGB565 encoded value |
|
lcd_w |
lcd width |
hal_draw_text565#
void hal_draw_text565 ( uint16_t * lcd_buf, uint16_t fcolor, uint16_t bcolor, uint32_t width, int x, int y, const char * label, int stripe_top, int stripe_bottom )
Draws text stored in label pointer to LCD buffer.
This function copy content of data from label text buffer to the LCD.
Parameters
in/out |
name |
description |
|---|---|---|
lcd_buf |
LCD buffer address destination for drawing text |
|
fcolor |
foreground color in rgb565 format |
|
bcolor |
background color in rgb565 format |
|
width |
LCD width in pixels |
|
x |
drawing position on X axis |
|
y |
drawing position on Y axis |
|
label |
C string to draw |
|
stripe_top |
top boundary of the stripe in which to draw (pixels from top) |
|
stripe_bottom |
bottom boundary of the stripe in which to draw (pixels from top) |
hal_draw_rect565#
void hal_draw_rect565 ( uint16_t * lcd_buf, hal_rect_t rect, mpp_color_t rgb, uint32_t width, int stripe_top, int stripe_bottom )
Draws rectangle.
Parameters
in/out |
name |
description |
|---|---|---|
in |
lcd_buf |
LCD buffer address destination for drawing rectangle |
in |
rect |
rectangle position and size (top, left, bottom, right) |
in |
rgb |
color encoded as mpp_color_t (r, g, b fields) |
in |
width |
LCD width in pixels |
in |
stripe_top |
top boundary of the stripe in which to draw (pixels from top) |
in |
stripe_bottom |
bottom boundary of the stripe in which to draw (pixels from top) |
get_bitpp#
int get_bitpp ( mpp_pixel_format_t type )
Returns the number of bits per pixel for a given format.
Parameters
in/out |
name |
description |
|---|---|---|
in |
type |
pixel format |
Returns
bits per pixel, or 0 for unknown format
swap_2_bytes#
void swap_2_bytes ( uint8_t * data, int size )
Swaps a buffer’s MSB and LSB bytes.
Parameters
in/out |
name |
description |
|---|---|---|
data |
pointer to the buffer to be converted(from little endian to big endian and vice-versa). |
|
size |
buffer size. |
3.1.2 Data Structure Documentation#
camera_dev_operator_t#
struct camera_dev_operator_t
Operation that needs to be implemented by a camera device.
Data Fields
type |
name |
description |
|---|---|---|
(*init)(camera_dev_t *dev, mpp_camera_params_t *config, camera_dev_callback_t callback, void *param) |
initialize the dev |
|
(*deinit)(camera_dev_t *dev) |
deinitialize the dev |
|
(*start)(const camera_dev_t *dev) |
start the dev |
|
(*stop)(const camera_dev_t *dev) |
stop the dev |
|
(*enqueue)(const camera_dev_t *dev, void *data) |
enqueue a buffer to the dev |
|
(*dequeue)(const camera_dev_t *dev, void **data, int *stripe, int *compressed_size) |
dequeue a buffer from the dev (blocking) |
|
(*get_buf_desc)(const camera_dev_t *dev, hw_buf_desc_t *out_buf, mpp_memory_policy_t *policy) |
get buffer descriptors and policy |
|
(*lock)(const camera_dev_t *dev) |
lock the device for exclusive access and operations |
|
(*unlock)(const camera_dev_t *dev) |
unlock the device after exclusive operations |
static_image_operator_t#
struct static_image_operator_t
Operation that needs to be implemented by an image element.
Data Fields
type |
name |
description |
|---|---|---|
(*init)(static_image_t *elt, mpp_img_params_t *config, void *param) |
initialize the elt |
|
(*dequeue)(static_image_t *elt, hw_buf_desc_t *out_buf, int *stripe_num) |
dequeue a buffer from the elt |
filesrc_operator_t#
struct filesrc_operator_t
Operation that needs to be implemented by a file source element.
Data Fields
type |
name |
description |
|---|---|---|
(*init)(filesrc_t *dev, mpp_filesrc_params_t *config, void *param) |
initialize the dev |
|
(*deinit)(filesrc_t *dev) |
deinitialize the dev |
|
(*start)(const filesrc_t *dev) |
start the dev |
|
(*stop)(const filesrc_t *dev) |
stop the dev |
|
(*dequeue)(const filesrc_t *dev, void **data, uint32_t *size) |
dequeue a buffer |
|
(*get_buf_desc)(const filesrc_t *dev, hw_buf_desc_t *out_buf, mpp_memory_policy_t *policy) |
get buffer descriptors and policy |
filesink_operator_t#
struct filesink_operator_t
Operation that needs to be implemented by a file sink element.
Data Fields
type |
name |
description |
|---|---|---|
(*init)(filesink_t *dev, mpp_filesink_params_t *config, void *param) |
initialize the dev |
|
(*deinit)(filesink_t *dev) |
deinitialize the dev |
|
(*start)(const filesink_t *dev) |
start the dev |
|
(*stop)(const filesink_t *dev) |
stop the dev |
|
(*enqueue)(const filesink_t *dev, void *data, uint32_t size) |
enqueue a buffer |
|
(*get_buf_desc)(const filesink_t *dev, hw_buf_desc_t *in_buf, mpp_memory_policy_t *policy) |
get buffer descriptors and policy |
rtspsink_operator_t#
struct rtspsink_operator_t
Operation that needs to be implemented by an RTSP sink element.
Data Fields
type |
name |
description |
|---|---|---|
hal_rtspsink_status_t |
(*init)(rtspsink_t *dev, mpp_rtspsink_params_t *config, void *param) |
initialize the dev |
hal_rtspsink_status_t |
(*deinit)(rtspsink_t *dev) |
deinitialize the dev |
hal_rtspsink_status_t |
(*start)(const rtspsink_t *dev) |
start the dev |
hal_rtspsink_status_t |
(*stop)(const rtspsink_t *dev) |
stop the dev |
hal_rtspsink_status_t |
(*enqueue)(const rtspsink_t *dev, void *data, uint32_t size) |
enqueue a buffer |
hal_rtspsink_status_t |
(*get_buf_desc)(const rtspsink_t *dev, hw_buf_desc_t *in_buf, mpp_memory_policy_t *policy) |
get buffer descriptors and policy |
rtspsrc_operator_t#
struct rtspsrc_operator_t
Operations that need to be implemented by an RTSP source element.
Data Fields
type |
name |
description |
|---|---|---|
hal_rtspsrc_status_t |
(*init)(rtspsrc_t *dev, mpp_rtspsrc_params_t *config) |
initialize the RTSP source device |
hal_rtspsrc_status_t |
(*deinit)(rtspsrc_t *dev) |
de-initialize the RTSP source device |
hal_rtspsrc_status_t |
(*start)(const rtspsrc_t *dev) |
start streaming |
hal_rtspsrc_status_t |
(*stop)(const rtspsrc_t *dev) |
stop streaming |
hal_rtspsrc_status_t |
(*dequeue)(const rtspsrc_t *dev, void **data, uint32_t *size) |
dequeue a received buffer |
hal_rtspsrc_status_t |
(*get_buf_desc)(const rtspsrc_t *dev, hw_buf_desc_t *out_buf, mpp_memory_policy_t *policy) |
get buffer descriptor and memory policy |
gfx_dev_operator_t#
struct gfx_dev_operator_t
Operation that needs to be implemented by gfx device.
Data Fields
type |
name |
description |
|---|---|---|
int |
(*init)(gfx_dev_t *dev, void *param) |
initialize the dev |
int |
(*deinit)(gfx_dev_t *dev) |
deinitialize the dev |
int |
(*get_buf_desc)(const gfx_dev_t *dev, hw_buf_desc_t *in_buf, hw_buf_desc_t *out_buf, mpp_memory_policy_t *policy) |
get buffer descriptors and policy |
int |
(*blit)(const gfx_dev_t *dev, const gfx_surface_t *pSrc, const gfx_surface_t *pDst, const gfx_rotate_config_t *pRotate, mpp_flip_mode_t flip) |
blit source to destination surface |
int |
(*drawRect)(const gfx_dev_t *dev, gfx_surface_t *pOverlay, int x, int y, int w, int h, int color) |
draw rectangle in overlay surface |
int |
(*drawPicture)(const gfx_dev_t *dev, gfx_surface_t *pOverlay, int x, int y, int w, int h, int alpha, const char *pIcon) |
draw picture in overlay surface |
int |
(*drawText)(const gfx_dev_t *dev, gfx_surface_t *pOverlay, int x, int y, int textColor, int bgColor, int type, const char *pText) |
draw text in overlay surface |
int |
(*compose)(const gfx_dev_t *dev, gfx_surface_t *pSrc, gfx_surface_t *pOverlay, gfx_surface_t *pDst, gfx_rotate_config_t *pRotate, mpp_flip_mode_t flip) |
blit source with overlay to destination surface |
int |
(*finish)(gfx_dev_t *dev) |
finalize rendering into destination surface |
vdec_dev_operator_t#
struct vdec_dev_operator_t
Operation that needs to be implemented by vdec device.
Operation that needs to be implemented by a JPEG/image decoder device
Data Fields
type |
name |
description |
|---|---|---|
int |
(*init)(vdec_dev_t *dev, void *param) |
initialize the dev |
int |
(*deinit)(const vdec_dev_t *dev) |
deinitialize the dev |
int |
(*get_buf_desc)(const vdec_dev_t *dev, hw_buf_desc_t *in_buf, hw_buf_desc_t *out_buf, mpp_memory_policy_t *policy) |
get buffer descriptors and policy |
int |
(*decode)(const vdec_dev_t *dev, uint8_t *pSrc, uint8_t *pDst, int32_t jpg_size, uint32_t row_stride) |
decode image data |
vdec_h264_dev_operator_t#
struct vdec_h264_dev_operator_t
Operation that needs to be implemented by an H.264 decoder device.
Data Fields
type |
name |
description |
|---|---|---|
(*init)(vdec_h264_dev_t *dev, void *param) |
initialize the dev |
|
(*deinit)(const vdec_h264_dev_t *dev) |
deinitialize the dev |
|
(*get_buf_desc)(const vdec_h264_dev_t *dev, hw_buf_desc_t *in_buf, hw_buf_desc_t *out_buf, mpp_memory_policy_t *policy) |
get buffer descriptors and policy |
|
(*decode)(const vdec_h264_dev_t *dev, vdec_h264_frame_info_t *frame_info) |
decode H.264 frame |
vision_algo_dev_operator_t#
struct vision_algo_dev_operator_t
Operation that needs to be implemented by a vision algorithm device.
Data Fields
type |
name |
description |
|---|---|---|
(*init)(vision_algo_dev_t *dev, model_param_t *param) |
initialize the dev |
|
(*deinit)(vision_algo_dev_t *dev) |
deinitialize the dev |
|
(*run)(const vision_algo_dev_t *dev, void *data) |
start the dev |
|
(*get_buf_desc)(const vision_algo_dev_t *dev, hw_buf_desc_t *in_buf, mpp_memory_policy_t *policy) |
read input parameters |
display_dev_operator_t#
struct display_dev_operator_t
Operation that needs to be implemented by a display device.
Data Fields
type |
name |
description |
|---|---|---|
(*init)(display_dev_t *dev, mpp_display_params_t *config, mpp_callback_t callback, void *user_data) |
initialize the dev |
|
(*deinit)(const display_dev_t *dev) |
deinitialize the dev |
|
(*start)(display_dev_t *dev) |
start the dev |
|
(*stop)(display_dev_t *dev) |
stop the dev |
|
(*blit)(const display_dev_t *dev, void *frame, int stripe) |
blit a buffer to the dev |
|
(*get_buf_desc)(const display_dev_t *dev, hw_buf_desc_t *in_buf, mpp_memory_policy_t *policy) |
get buffer descriptors and policy |
venc_h264_dev_operator_t#
struct venc_h264_dev_operator_t
Operations that need to be implemented by an H.264 encoder device.
Data Fields
type |
name |
description |
|---|---|---|
(*init)(venc_h264_dev_t *dev, void *param) |
initialize the device |
|
(*deinit)(const venc_h264_dev_t *dev) |
deinitialize the device |
|
(*get_buf_desc)(const venc_h264_dev_t *dev, hw_buf_desc_t *in_buf, hw_buf_desc_t *out_buf, mpp_memory_policy_t *policy) |
get buffer descriptors and policy |
|
(*encode)(const venc_h264_dev_t *dev, venc_h264_frame_info_t *frame_info) |
encode the incoming data |
3.1.3 Typedef Documentation#
mpp_callback_t#
typedef int(* mpp_callback_t)(mpp_t mpp, mpp_evt_t evt, void *evt_data, void *user_data)
The mpp callback function prototype.
Chapter 4#
Functions
int hal_label_rectangle (uint8_t * frame, int width, int height, mpp_pixel_format_t format, mpp_labeled_rect_t * lr, int stripe, int stripe_max)
int hal_landmark (uint8_t * frame, int width, int height, mpp_pixel_format_t format, mpp_landmark_t * lk, int stripe, int stripe_max)
int hal_inference_tflite_setup (vision_algo_dev_t * dev)
int hal_inference_executorch_setup (vision_algo_dev_t * dev)
int hal_display_setup (const char * name, display_dev_t * dev)
int hal_camera_setup (const char * name, camera_dev_t * dev)
int hal_gfx_setup (const char * name, gfx_dev_t * dev)
int hal_img_decoder_setup (const char * name, vdec_dev_t * dev)
int hal_mc_dev_setup (const char * name, multicore_dev_t * dev)
4.1 HAL Setup Functions#
This section provides the detailed documentation for the HAL setup functions that should be defined by each device.
4.1.1 Function Documentation#
hal_label_rectangle#
int hal_label_rectangle ( uint8_t * frame, int width, int height, mpp_pixel_format_t format, mpp_labeled_rect_t * lr, int stripe, int stripe_max )
Implementation of hal labeled rectangle component that draws a rectangle and a text on an input image.
Parameters
in/out |
name |
description |
|---|---|---|
in |
frame |
The buffer address |
in |
width |
Image width |
in |
height |
Image height |
in |
format |
Image format |
in |
lr |
Labeled rectangle parameters |
in |
stripe |
stripe number (0=no stripe) |
in |
stripe_max |
max nb of stripes |
Returns
0
hal_landmark#
int hal_landmark ( uint8_t * frame, int width, int height, mpp_pixel_format_t format, mpp_landmark_t * lk, int stripe, int stripe_max )
Implementation of hal landmark component that draws a landmark on an input image.
Parameters
in/out |
name |
description |
|---|---|---|
in |
frame |
The buffer address |
in |
width |
Image width |
in |
height |
Image height |
in |
format |
Image format |
in |
lk |
landmark parameters |
in |
stripe |
stripe number (0=no stripe) |
in |
stripe_max |
max nb of stripes |
Returns
0
hal_inference_tflite_setup#
int hal_inference_tflite_setup ( vision_algo_dev_t * dev )
Hal setup function for inference engine Tensorflow-Lite Micro.
Parameters
in/out |
name |
description |
|---|---|---|
in |
dev |
vision algo device to register |
Returns
error code (0: success, otherwise: failure)
hal_inference_executorch_setup#
int hal_inference_executorch_setup ( vision_algo_dev_t * dev )
Hal setup function for inference engine ExecuTorch.
Parameters
in/out |
name |
description |
|---|---|---|
in |
dev |
vision algo device to register |
Returns
error code (0: success, otherwise: failure)
hal_display_setup#
int hal_display_setup ( const char * name, display_dev_t * dev )
Register with a display device specified by name.
If name is NULL, return error.
Parameters
in/out |
name |
description |
|---|---|---|
in |
name |
display name |
in |
dev |
display device to register |
Returns
error code (0: success, otherwise: failure)
hal_camera_setup#
int hal_camera_setup ( const char * name, camera_dev_t * dev )
Register with a camera device specified by name.
If name is NULL, return error.
Parameters
in/out |
name |
description |
|---|---|---|
in |
name |
camera name |
in |
dev |
camera device to register |
Returns
error code (0: success, otherwise: failure)
hal_gfx_setup#
int hal_gfx_setup ( const char * name, gfx_dev_t * dev )
Register with a graphic processing device specified by name.
If name is NULL, the first available graphic processing supported by Hw will be selected. The graphic device using CPU operations will be selected if name is not specified and if no graphic processing is available for the Hw.
Parameters
in/out |
name |
description |
|---|---|---|
in |
name |
graphic processing device performing the image conversion |
in |
dev |
graphic device to register |
Returns
error code (0: success, otherwise: failure)
hal_img_decoder_setup#
int hal_img_decoder_setup ( const char * name, vdec_dev_t * dev )
Register with an image decoder device specified by name.
If name is NULL, the first available decoder supported by Hw will be selected. The decoder device using CPU operations will be selected if name is not specified and if no decoder is available for the Hw.
Parameters
in/out |
name |
description |
|---|---|---|
in |
name |
image decoding device name |
in |
dev |
decoder device to register |
Returns
error code (0: success, otherwise: failure)
hal_mc_dev_setup#
int hal_mc_dev_setup ( const char * name, multicore_dev_t * dev )
Register multicore device.
Parameters
in/out |
name |
description |
|---|---|---|
in |
name |
multicore device name |
in |
dev |
multicore device to register |
Returns
error code (0: success, otherwise: failure)