MCUXpresso SDK Documentation

Register only used operators

Register only used operators#

Use the tflite::MicroMutableOpResolver object template, which is later passed to the tflite::MicroInterpreter object. Depending on the list of used operators, the result should be similar to Register only used operators in TensorFlow Lite Micro. Make sure to update the MicroMutableOpResolver template parameter to reflect the number of operators that need to be registered.

Register only used operators in TensorFlow Lite Micro#

#include "tensorflow/lite/micro/kernels/micro_ops.h"
#include "tensorflow/lite/micro/micro_mutable_op_resolver.h"
tflite::MicroMutableOpResolver<6> microOpResolver;
microOpResolver.AddAveragePool2D();
microOpResolver.AddConv2D();
microOpResolver.AddDepthwiseConv2D();
microOpResolver.AddDequantize();
microOpResolver.AddReshape();
microOpResolver.AddSoftmax();
static tflite::MicroInterpreter interpreter(
    model, microOpResolver, tensorArena, kTensorArenaSize, microErrorReporter);