MCMGR Porting guide to version v5.0.0#
This porting guide will describe steps to port Multicore Manager (MCMGR) to version v5.0.0.
Overview#
The implementation of MCMGR before version v5.0.0. assumed that only two cores were
present on device.
That caused some functions were missing parameter specifying on what core to call
that function and it was always assumed that it is other core then itself internally.
With introduction of device with more than two core this limitation needed to be
addressed and change in API was introduced in this release.
Changes in Directory Structure#
All include files were moved from src/ directory to inc/ directory.
New platform specific include directory added inc/platform/<platform_name>/mcmgr_platform.h.
This contains platform specific macros like MCMGR_CORECOUNT (2).
Please update your project include paths accordingly.
Changes in the API#
Main change in public API is adding the core number parameter to functions described bellow.
Before, for example just calling MCMGR_GetStartupData() function assumed that it
requires data from other core.
But with more than two cores Application using this function needs to decide from what
core number it wants to receive startup data.
And same way for MCMGR_TriggerEvent function.
Event Callback function change#
Change in Event Callback function will now receive core number from core which event
was sent.
This information then can be used by application to capture events from specific cores.
- typedef void (*mcmgr_event_callback_t)(uint16_t data, void *context);
+ typedef void (*mcmgr_event_callback_t)(mcmgr_core_t coreNum, uint16_t data, void *context);
MCMGR_GetStartupData() change#
- mcmgr_status_t MCMGR_GetStartupData(uint32_t *startupData);
+ mcmgr_status_t MCMGR_GetStartupData(mcmgr_core_t coreNum, uint32_t *startupData);
MCMGR_TriggerEvent() change#
- mcmgr_status_t MCMGR_TriggerEvent(mcmgr_event_type_t type, uint16_t eventData);
+ mcmgr_status_t MCMGR_TriggerEvent(mcmgr_core_t coreNum, mcmgr_event_type_t type, uint16_t eventData);
MCMGR_TriggerEventForce() change#
- mcmgr_status_t MCMGR_TriggerEventForce(mcmgr_event_type_t type, uint16_t eventData);
+ mcmgr_status_t MCMGR_TriggerEventForce(mcmgr_core_t coreNum, mcmgr_event_type_t type, uint16_t eventData);
How to port your Application#
This chapter will describe necessary steps to port your application using MCMGR.
Event Handler change#
Before this change event handler only received event data from one core.
void RPMsgRemoteReadyEventHandler(uint16_t eventData, void *context)
{
uint16_t *data = (uint16_t *)context;
*data = eventData;
}
void main()
{
uint16_t RPMsgRemoteReadyEventData = {0};
MCMGR_RegisterEvent(kMCMGR_RemoteApplicationEvent, RPMsgRemoteReadyEventHandler,
RPMsgRemoteReadyEventData);
}
After this change event handler can receive event data from multiple cores and application
is responsible to register callback data RPMsgRemoteReadyEventData array with length of
cores in the system.
For this MCMGR_CORECOUNT platform specific macro can be used.
The type of context data is Applications specific and make sure to do correct casting
in application event handler.
NOTE: In case the Application is running on system with only two cores
then application can still useMCMGR_RegisterEventand Event handler as before. This is because the event handler really cannot be trigger by any other core if there
are only two.
static void RPMsgRemoteReadyEventHandler(mcmgr_core_t coreNum, uint16_t eventData, void *context)
{
uint16_t *data = &((uint16_t *)context)[coreNum];
*data = eventData;
}
int main(void)
{
volatile uint16_t RPMsgRemoteReadyEventData[MCMGR_CORECOUNT] = {0};
MCMGR_RegisterEvent(kMCMGR_RemoteApplicationEvent, RPMsgRemoteReadyEventHandler,
(void *)RPMsgRemoteReadyEventData);
}
GetStartupData and TriggerEvent functions#
For these functions application needs to provide new parameter of core number.
- MCMGR_TriggerEvent(kMCMGR_RemoteApplicationEvent, APP_RPMSG_READY_EVENT_DATA);
+ MCMGR_TriggerEvent(kMCMGR_Core0, kMCMGR_RemoteApplicationEvent, APP_RPMSG_READY_EVENT_DATA);
Example of getting startup data from secondary core kMCMGR_Core1 will specify it
wants to request data from kMCMGR_Core0.
uint32_t startupData;
do
{
- mcmgrStatus = MCMGR_GetStartupData(&startupData);
+ mcmgrStatus = MCMGR_GetStartupData(kMCMGR_Core0, &startupData);
} while (mcmgrStatus != kStatus_MCMGR_Success);