MCUXpresso SDK Documentation

Run TF-M tests and applications on Arm platforms#

Instructions for how to run TF-M tests and applications on Arm platforms.

Follow build instruction to build the binaries. Follow secure boot to build the binaries with or without BL2 bootloader.

Execute TF-M regression tests on MPS2 boards and FVP#

The BL2 bootloader and TF-M example application and tests have been verified using the reference model for MPS2 (AN521), in Keil MDK , Fixed Virtual Platforms and Arm Development Studio .

Note

The name of the reference model’s executable can vary depending on toolchain.

For more information please refer to the appropriate toolchain’s documentation: Keil MDK Documentation , Fixed Virtual Platforms Documentation , Arm Development Studio Documentation

To run the example code on an SSE-200 Fast-Model#

Using FVP_MPS2_AEMv8M provided by Arm Development Studio 2019.1.

Example application and regression tests without BL2 bootloader#

Add tfm_s.axf and tfm_ns.axf to symbol files in Debug Configuration menu.

<DS_PATH>/sw/models/bin/FVP_MPS2_AEMv8M \
--parameter fvp_mps2.platform_type=2 \
--parameter cpu0.baseline=0 \
--parameter cpu0.INITVTOR_S=0x10000000 \
--parameter cpu0.semihosting-enable=0 \
--parameter fvp_mps2.DISABLE_GATING=0 \
--parameter fvp_mps2.telnetterminal0.start_telnet=1 \
--parameter fvp_mps2.telnetterminal1.start_telnet=0 \
--parameter fvp_mps2.telnetterminal2.start_telnet=0 \
--parameter fvp_mps2.telnetterminal0.quiet=0 \
--parameter fvp_mps2.telnetterminal1.quiet=1 \
--parameter fvp_mps2.telnetterminal2.quiet=1 \
--application cpu0=<build_dir>/bin/tfm_s.axf \
--data cpu0=<build_dir>/bin/tfm_ns.bin@0x00100000

Example application and regression tests with BL2 bootloader#

To test TF-M with bootloader, one must apply the following changes:

  • Add bl2.axf to symbol files in DS-5 in Debug Configuration menu.

  • Replace the last two lines of the previous command with this:

--application cpu0=<build_dir>/bin/bl2.axf \
--data cpu0=<build_dir>/tfm_s_ns_signed.bin@0x10080000
Test software upgrade with BL2 bootloader#

BL2 bootloader is mandatory to test software update. Furthermore, two TF-M blobs must be built. Outputs of example application and regression test can be used to test it. Load output of example application to the primary slot (0x10080000) and output of regression test to the secondary slot (0x10180000). Add the following line to the end of the previous chapter:

--data cpu0=<build_dir>/tfm_s_ns_signed.bin@0x10180000

To run the example code on SSE 200 FPGA on MPS2 board#

FPGA image is available to download here

To run BL2 bootloader and TF-M example application and tests in the MPS2 board, it is required to have SMM-SSE-200 for MPS2 (AN521) image in the MPS2 board SD card. The image should be located in <MPS2 device name>/MB/HBI0263<board revision letter>/AN521

The MPS2 board tested is HBI0263C referred also as MPS2+.

Warning

If you change the exe names, MPS2 expects file names in 8.3 format.

Example application#

  1. Copy bl2.bin and tfm_s_ns_signed.bin files from <build_dir>/bin to <MPS2 device name>/SOFTWARE/

  2. Open <MPS2 device name>/MB/HBI0263C/AN521/images.txt

  3. Update the AN521/images.txt file as follows:

    TITLE: Versatile Express Images Configuration File
    [IMAGES]
    TOTALIMAGES: 2                     ;Number of Images (Max: 32)
    IMAGE0ADDRESS: 0x10000000
    IMAGE0FILE: \Software\bl2.bin  ; BL2 bootloader
    IMAGE1ADDRESS: 0x10080000
    IMAGE1FILE: \Software\tfm_s_ns_signed.bin ; TF-M example application binary blob
    
  4. Close <MPS2 device name>/MB/HBI0263C/AN521/images.txt

  5. Unmount/eject the <MPS2 device name> unit

  6. Reset the board to execute the TF-M example application

  7. After completing the procedure you should be able to visualize on the serial port (baud 115200 8n1) the following messages:

    [INF] Starting bootloader
    [INF] Image 0: magic=good, copy_done=0xff, image_ok=0xff
    [INF] Scratch: magic=bad, copy_done=0x5, image_ok=0xcf
    [INF] Boot source: primary slot
    [INF] Swap type: none
    [INF] Bootloader chainload address offset: 0x80000
    [INF] Jumping to the first image slot
    [Sec Thread] Secure image initializing!
    

Regression tests#

After completing the procedure you should be able to visualize on the serial port (baud 115200 8n1) the following messages:

[INF] Starting bootloader
[INF] Image 0: magic=good, copy_done=0xff, image_ok=0xff
[INF] Scratch: magic=bad, copy_done=0x5, image_ok=0xcf
[INF] Boot source: primary slot
[INF] Swap type: none
[INF] Bootloader chainload address offset: 0x80000
[INF] Jumping to the first image slot
[Sec Thread] Secure image initializing!

#### Execute test suites for the protected storage service ####
Running Test Suite PS secure interface tests (TFM_PS_TEST_2XXX)...

> Executing 'TFM_PS_TEST_2001'
  Description: 'Create interface'
  TEST PASSED!
> Executing 'TFM_PS_TEST_2002'
  Description: 'Get handle interface (DEPRECATED)'
This test is DEPRECATED and the test execution was SKIPPED
  TEST PASSED!
> Executing 'TFM_PS_TEST_2003'
  Description: 'Get handle with null handle pointer (DEPRECATED)'
This test is DEPRECATED and the test execution was SKIPPED
  TEST PASSED!
> Executing 'TFM_PS_TEST_2004'
  Description: 'Write interface'
  TEST PASSED!
> Executing 'TFM_PS_TEST_2005'
  Description: 'Read interface'
....

Note

PS reliability tests take a few minutes to run on the MPS2.

Example application without BL2 bootloader#

  1. Copy tfm_s.bin and tfm_ns.bin files from <build_dir>/bin to <MPS2 device name>/SOFTWARE/

  2. Open <MPS2 device name>/MB/HBI0263C/AN521/images.txt

  3. Update the AN521/images.txt file as follows:

    TITLE: Versatile Express Images Configuration File
    [IMAGES]
    TOTALIMAGES: 2                   ;Number of Images (Max: 32)
    IMAGE0ADDRESS: 0x10000000
    IMAGE0FILE: \Software\tfm_s.bin  ; Secure code
    IMAGE1ADDRESS: 0x00100000
    IMAGE1FILE: \Software\tfm_ns.bin ; Non-secure code
    
  4. Close <MPS2 device name>/MB/HBI0263C/AN521/images.txt

  5. Unmount/eject the <MPS2 device name> unit

  6. Reset the board to execute the TF-M example application

  7. After completing the procedure you should be able to visualize on the serial port (baud 115200 8n1) the following messages:

    [Sec Thread] Secure image initializing!
    

Regression tests without BL2 bootloader#

After completing the procedure you should be able to visualize on the serial port (baud 115200 8n1) the following messages:

[Sec Thread] Secure image initializing!

#### Execute test suites for the protected storage service ####
Running Test Suite PS secure interface tests (TFM_PS_TEST_2XXX)...

> Executing 'TFM_PS_TEST_2001'
  Description: 'Create interface'
  TEST PASSED!
> Executing 'TFM_PS_TEST_2002'
  Description: 'Get handle interface (DEPRECATED)'
This test is DEPRECATED and the test execution was SKIPPED
  TEST PASSED!
> Executing 'TFM_PS_TEST_2003'
  Description: 'Get handle with null handle pointer (DEPRECATED)'
This test is DEPRECATED and the test execution was SKIPPED
  TEST PASSED!
> Executing 'TFM_PS_TEST_2004'
  Description: 'Write interface'
  TEST PASSED!
> Executing 'TFM_PS_TEST_2005'
  Description: 'Read interface'
....

Execute TF-M regression tests on Musca test chip boards#

Note

Before executing any images on Musca-B1 board, please check the target platform readme to have the correct setup.

Install SRecord for Musca test chip boards:

Example application with BL2 bootloader#

  1. Create a unified hex file comprising of both bl2.bin and tfm_s_ns_signed.bin for Musca-B1 or Musca-S1 platforms:

    srec_cat bin/bl2.bin -Binary -offset 0xA000000 bin/tfm_s_ns_signed.bin -Binary -offset 0xA020000 -o tfm.hex -Intel
    
  2. Power up the Musca board by connecting it to a computer with a USB lead. Press the PBON button if the green ON LED does not immediately turn on. The board should appear as a USB drive.

  3. Copy tfm.hex to the USB drive. The orange PWR LED should start blinking.

  4. Once the PWR LED stops blinking, power cycle or reset the board to boot from the new image.

  5. After completing the procedure you should see the following messages on the DAPLink UART (baud 115200 8n1):

    [INF] Starting bootloader
    [INF] Image 0: magic=good, copy_done=0xff, image_ok=0xff
    [INF] Scratch: magic=bad, copy_done=0x5, image_ok=0xd9
    [INF] Boot source: primary slot
    [INF] Swap type: none
    [INF] Bootloader chainload address offset: 0x20000
    [INF] Jumping to the first image slot
    [Sec Thread] Secure image initializing!
    

Regression tests with BL2 bootloader#

Note

As the Internal Trusted Storage and Protected Storage tests use persistent storage, it is recommended to erase the storage area before running the tests. Existing data may prevent the tests from running to completion if, for example, there is not enough free space for the test data or the UIDs used by the tests have already been created with the write-once flag set. Repeated test runs can be done without erasing between runs.

To erase the storage when flashing an image, -fill 0xFF <start_addr> <end_addr> can be added to the srec_cat command used to create the combined hex file. The <start_addr> and <end_addr> are the start and end addresses of the storage area, found in the board’s flash_layout.h file. The board’s flash can also be erased via a debugger; see your IDE’s documentation for instructions.

After completing the procedure you should see the following messages on the DAPLink UART (baud 115200 8n1):

[INF] Starting bootloader
[INF] Image 0: magic=good, copy_done=0xff, image_ok=0xff
[INF] Scratch: magic=bad, copy_done=0x5, image_ok=0x9
[INF] Boot source: primary slot
[INF] Swap type: none
[INF] Bootloader chainload address offset: 0x20000
[INF] Jumping to the first image slot
[Sec Thread] Secure image initializing!

#### Execute test suites for the protected storage service ####
Running Test Suite PS secure interface tests (TFM_PS_TEST_2XXX)...
> Executing 'TFM_PS_TEST_2001'
  Description: 'Create interface'
  TEST PASSED!
> Executing 'TFM_PS_TEST_2002'
  Description: 'Get handle interface (DEPRECATED)'
This test is DEPRECATED and the test execution was SKIPPED
  TEST PASSED!
> Executing 'TFM_PS_TEST_2003'
  Description: 'Get handle with null handle pointer (DEPRECATED)'
This test is DEPRECATED and the test execution was SKIPPED
  TEST PASSED!
> Executing 'TFM_PS_TEST_2004'
  Description: 'Get attributes interface'
  TEST PASSED!
> Executing 'TFM_PS_TEST_2005'
  Description: 'Get attributes with null attributes struct pointer'
....

PSA API tests#

Follow the build instructions for the PSA API tests and then follow the above procedures for flashing the image to the board. The PSA API tests are linked into the TF-M binaries and will automatically run. A log similar to the following should be visible on the UART; it is normal for some tests to be skipped but there should be no failed tests:

[Sec Thread] Secure image initializing!
Booting TFM v1.1
Non-Secure system starting...

***** PSA Architecture Test Suite - Version 1.0 *****

Running.. Storage Suite
******************************************

TEST: 401 | DESCRIPTION: UID not found check
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Call get API for UID 6 which is not set
[Check 2] Call get_info API for UID 6 which is not set
[Check 3] Call remove API for UID 6 which is not set
[Check 4] Call get API for UID 6 which is removed
[Check 5] Call get_info API for UID 6 which is removed
[Check 6] Call remove API for UID 6 which is removed
[Check 7] Call get API for different UID 5
[Check 8] Call get_info API for different UID 5
[Check 9] Call remove API for different UID 5

[Info] Executing PS tests
[Check 1] Call get API for UID 6 which is not set
[Check 2] Call get_info API for UID 6 which is not set
[Check 3] Call remove API for UID 6 which is not set
[Check 4] Call get API for UID 6 which is removed
[Check 5] Call get_info API for UID 6 which is removed
[Check 6] Call remove API for UID 6 which is removed
[Check 7] Call get API for different UID 5
[Check 8] Call get_info API for different UID 5
[Check 9] Call remove API for different UID 5

TEST RESULT: PASSED

******************************************

<further tests removed from log for brevity>

************ Storage Suite Report **********
TOTAL TESTS     : 17
TOTAL PASSED    : 11
TOTAL SIM ERROR : 0
TOTAL FAILED    : 0
TOTAL SKIPPED   : 6
******************************************

Note

The Internal Trusted Storage and Protected Storage flash areas must be wiped before running the Storage test suites.

Many IDEs for embedded development (such as Keil µVision) offer a function to erase a device’s flash. Refer to your IDE’s documentation for instructions.

Another way this can be achieved is by using srec_cat with the -fill parameter to fill the corresponding area in the binary with the erase value of the flash (0xFF).

Refer to the platform flash layout for appropriate addresses to erase on other platforms.

This step is not required on targets that emulate flash storage in RAM, as it will be erased each time the device is reset. Note, however, that a warm reset may not clear SRAM contents, so it may be necessary to power the device off and on again between test runs.

Example application or regression tests on Musca-B1 without BL2 bootloader#

Follow the above procedures, but create a unified hex file out of tfm_s.bin and tfm_ns.bin:

  • Windows:

    srec_cat.exe bin\tfm_s.bin -Binary -offset 0xA000000 bin\tfm_ns.bin -Binary -offset 0xA080000 -o tfm.hex -Intel
    
  • Linux:

    srec_cat bin/tfm_s.bin -Binary -offset 0xA000000 bin/tfm_ns.bin -Binary -offset 0xA080000 -o tfm.hex -Intel
    

Execute TF-M example and regression tests on MPS3 boards#

Firmware upgrade and image validation with BL2 bootloader#

High level operation of BL2 bootloader and instructions for testing firmware upgrade is described in secure boot.


Copyright (c) 2017-2024, Arm Limited. All rights reserved.