Details for the platform/ext folder#
This folder has code that has been imported from other projects. This means the files in this folder and subfolders have Apache 2.0 license which is different to BSD 3.0 license applied to the parent TF-M project.
Note
This folder is strictly Apache 2.0 with the exception of cmake files. Maintainers should be consulted if this needs to be revisited.
Sub-folders#
accelerator#
This folder contains cmake and code files to interact cryptographic accelerators.
In order to use a cryptographic accelerator, a platform must set
CRYPTO_HW_ACCELERATOR_TYPE in preload.cmake. This option maps directly to
the subdirectories of the accelerator directory. Currently available
accelerators are : the CryptoCell cc312, the STMicroelectronics accelerator
stm .
A minimal API is exposed to interact with accelerators, the details of this api
are in accelerator/interface/crypto_hw.h. Implementation of the API is
inside the subdirectory of the individual accelerator.
To configure a cryptographic accelerator at build time, two cmake options can be specified.
CRYPTO_HW_ACCELERATORONAll possible mbedtls cryptographic operations will be offloaded to the accelerator.OFFThe cryptographic accelerator will be ignored and software cryptography will be used.
cmsis#
This folder contains core and compiler specific header files imported from the
CMSIS_5 project.
common#
armclang and gcc#
These contain the linker scripts used to configure the memory regions in TF-M regions.
template#
This directory contains platform-independent dummy implementations of the
interfaces in platform/include. These implementations can be built directly
for initial testing of a platform port, or used as a basic template for a real
implementation for a particular target. They must not be used in production
systems.
driver#
This folder contains the headers with CMSIS compliant driver definitions that that TF-M project expects a target to provide.
target_cfg.h#
This file is expected to define the following macros respectively.
TFM_DRIVER_STDIO- This macro should expand to a structure of typeARM_DRIVER_USART. TFM redirects its standard input and output to this instance of USART.NS_DRIVER_STDIO- This macro should expand to a structure of typeARM_DRIVER_USART. Non-Secure application redirects its standard input and output to this instance of USART.
target#
This folder contains the files for individual target. For a buildable target,
the directory path from the target directory to its CMakeLists.txt file
is the argument that would be given to -DTFM_PLATFORM=.
The standard directory structure is as follows:
- target
- <Vendor name>
common
<buildable target 1>
<buildable target 2>
<buildable target 3>
Each buildable target must contain the cmake files mandated in the section below.
The common directory is not required, but can be used to contain code that
is used by multiple targets.
There must not be any directories inside the vendor directory that is not either
the common directory or a buildable platform, to avoid confusion about what
directories are a valid TFM_PLATFORM.
Buildable target required cmake files#
A buildable target must provide 3 mandatory cmake files. These files must all be placed in the root of the buildable target directory.
preload.cmake#
This file contains variable definitions that relate to the underlying hardware of the target.
TFM_SYSTEM_PROCESSOR: The processor used by the target. The format is that same as the format used in the-mcpu=argument of GNUARM or ARMCLANG. The special+modifiersyntax must not be used.TFM_SYSTEM_ARCHITECTURE: The architecture used by the target. The format is that same as the format used in the-march=argument of GNUARM or ARMCLANG. The special+modifiersyntax must not be used.TFM_SYSTEM_DSP: Whether the target has the DSP feature of the givenTFM_SYSTEM_PROCESSORCRYPTO_HW_ACCELERATOR_TYPE: The type of cryptographic accelerator the target has, if it has one. This maps exactly to the subdirectories ofplatform/ext/acceleratorCONFIG_TFM_FP_ARCH: The “FPU architecture” (Armclang) or “FP hardware” (GNU) used by the target for compiling C source files. The value will be transferred to-mfpuargument of GNUARM or ARMCLANGCONFIG_TFM_FP_ARCH_ASM: The “FPU architecture” (Armclang) used by the target for assembling ASM source files. This value will be transferred to the--fpuargument of ARMCLANG. This value is not used by GNUARM.
For more details on CONFIG_TFM_FP_ARCH and CONFIG_TFM_FP_ARCH_ASM,
please refer to
Floating-Point Support.
Other than these particular cmake variables, it is permissible for the
preload.cmake file to contain add_definitions statements, in order for
set compile definitions that are global for the hardware. This is commonly used
to select a particular set of code from a vendor SDK.
It is not permissible to contains code other than the above in a
preload.cmake file, any general cmake code should be placed in
CMakeLists.txt and any configuration options should be contained in
config.cmake
config.cmake#
This file collects platform-specific overrides to the configuration options.
This should only contain cmake options that are included in
config_base.cmake. These options should be set as CACHE variables, as
they are in config_base.cmake.
CMakeLists.txt#
This file should contain all other required cmake code for the platform. This primarily consists of the following:
Adding an include directory to the target
platform_region_defs, which contains the headersflash_layout.handregion_defs.hAdding startup and scatter files to the
tfm_s,tfm_nsandbl2targets.linking
CMSIS_5_tfm_nsto the correct version of the CMSIS RTX libraries, as defined inlib/ext/CMSIS_5/CMakeLists.txtAdding required source files, include directories and compile definitions to the
platform_s,platform_nsandplatform_bl2targets.
preload_ns.cmake#
This optional cmake file is required only if the target runs the NSPE on a
core that requires different compiler options than the SPE core. This file has
the same format as preload.cmake, but instead details the hardware of the
NS core that is not running the main TF-M secure code.
install.cmake#
This optional cmake file is required only if additional files need to be installed for the platform.
Flash layout header file#
Target must provide a header file, called flash_layout.h, which defines the
information explained in the follow subsections. The defines must be named
as they are in the subsections.
BL2 bootloader#
The BL2 bootloader requires the following definitions:
FLASH_BASE_ADDRESS- Defines the first valid address in the flash.FLASH_AREA_BL2_OFFSET- Defines the offset from the flash base address where the BL2 - MCUBOOT area starts.FLASH_AREA_BL2_SIZE- Defines the size of the BL2 area.FLASH_AREA_SCRATCH_OFFSET- Defines the offset from the flash base address where the scratch area starts, which is used during image swapping.FLASH_AREA_SCRATCH_SIZE- Defines the size of the scratch area. The minimal size must be as the biggest sector size in the flash.FLASH_DEV_NAME- Specifies the flash device used by BL2.
The BL2 requires further definitions depending on the number of images, the meaning of these macros are also slightly different:
Required definitions in case of 1 image (S and NS images are concatenated and handled together as one binary blob):
FLASH_AREA_0_OFFSET- Defines the offset from the flash base address where the primary image area starts, which hosts the active firmware image.FLASH_AREA_0_SIZE- Defines the size of the primary image area.FLASH_AREA_2_OFFSET- Defines the offset from the flash base address where the secondary image area starts, which is a placeholder for new firmware images.FLASH_AREA_2_SIZE- Defines the size of the secondary image area.
Required definitions in case of 2 images (S and NS images are handled and updated separately):
FLASH_AREA_0_OFFSET- Defines the offset from the flash base address where the primary image areas start, which host the active firmware images. It is also the offset of the primary (active) secure image area.FLASH_AREA_0_SIZE- Defines the size of the primary secure image area.FLASH_AREA_1_OFFSET- Defines the offset from the flash base address where the primary (active) non-secure image area starts.FLASH_AREA_1_SIZE- Defines the size of the primary non-secure image area.FLASH_AREA_2_OFFSET- Defines the offset from the flash base address where the secondary image areas start, which are placeholders for new firmware images. It is also the offset of the secondary secure image area.FLASH_AREA_2_SIZE- Defines the size of the secondary secure image area.FLASH_AREA_3_OFFSET- Defines the offset from the flash base address where the secondary non-secure image area starts.FLASH_AREA_3_SIZE- Defines the size of the secondary non-secure image area.
The table below shows a fraction of the flash layout in case of 2 and 1 updatable images with the related flash areas that hold the firmware images:
Image number: 2 |
Image number: 1 |
||
|---|---|---|---|
Flash area |
Content |
Flash area |
Content |
FLASH_AREA_0 |
Secure image
primary slot
|
FLASH_AREA_0 |
Secure + Non-secure image
primary slot
|
FLASH_AREA_1 |
Non-secure image
primary slot
|
||
FLASH_AREA_2 |
Secure image
secondary slot
|
FLASH_AREA_2 |
Secure + Non-secure image
secondary slot
|
FLASH_AREA_3 |
Non-secure image
secondary slot
|
||
FLASH_AREA_SCRATCH |
Scratch area |
FLASH_AREA_SCRATCH |
Scratch area |
IMAGE_EXECUTABLE_RAM_START- Defines the start of the region to which images are allowed to be loaded. Only used ifMCUBOOT_UPGRADE_STRATEGYis configured to beRAM_LOAD.IMAGE_EXECUTABLE_RAM_SIZE- Defines the size of the region to which images are allowed to be loaded. Only used ifMCUBOOT_UPGRADE_STRATEGYis configured to beRAM_LOAD.
Assemble tool#
The assemble.py tool is used to concatenate secure and non-secure binary
to a single binary blob. It requires the following definitions:
SECURE_IMAGE_OFFSET- Defines the offset from the single binary blob base address, where the secure image starts.SECURE_IMAGE_MAX_SIZE- Defines the maximum size of the secure image area.NON_SECURE_IMAGE_OFFSET- Defines the offset from the single binary blob base address, where the non-secure image starts.NON_SECURE_IMAGE_MAX_SIZE- Defines the maximum size of the non-secure image area.
Image tool#
The imgtool.py tool is used to handle the tasks related to signing the
binary. It requires the following definition:
S_IMAGE_LOAD_ADDRESS- Defines the address to where the Secure (or combined Secure and Non-secure) image is loaded and is executed from. Only used ifMCUBOOT_UPGRADE_STRATEGYis configured to beRAM_LOAD.NS_IMAGE_LOAD_ADDRESS- Defines the address to where the Non-secure image is loaded and is executed from. Only used ifMCUBOOT_UPGRADE_STRATEGYis configured to beRAM_LOADandMCUBOOT_IMAGE_NUMBERis greater than 1.
Expose target support for HW components#
Services may require HW components to be supported by the target to enable some features (e.g. PS service with rollback protection, etc). The following definitions need to be set in the .cmake file if the target has the following HW components:
TARGET_NV_COUNTERS_ENABLE- Specifies that the target has non-volatile (NV) counters.
Copyright (c) 2017-2023, Arm Limited. All rights reserved. Copyright (c) 2020-2022 Cypress Semiconductor Corporation (an Infineon company) or an affiliate of Cypress Semiconductor Corporation. All rights reserved.