MCUXpresso SDK Documentation

Corstone-1000#

Introduction#

The ARM’s Corstone-1000 platform is a reference implementation of PSA FF-M architecture where NSPE and SPE environments are partitioned/isolated into Cortex-A35 and Cortex-M0+ respectively.

Cortex-M0+ acting as Secure Enclave is the Root-of-trust of SoC. Its software comprises of two boot loading stages, i.e. Bl1 and Bl2 (based on mcuboot) and TF-M as run time software. Cortex-A35, also referred as host, is treated as non-secure from the Secure Enclave perspective. The Cortex-A35 is brought out of rest by Secure Enclave in aarch64 bit mode, and boots the software ecosystem based on linux, u-boot, UEFI run time services, TF-A, Secure Partitions and Optee.

The communication between NSPE and SPE is based on PSA IPC protocol running on top of the RSE communication protocol. The Corstone-1000 supports only the Embed protocol, and the ATU support is removed.

The secure enclave subsystem has ARM’s CC-312 (Crypto Cell) hardware to accelerate cryptographic operations. Additionaly, platform supports Secure Debug using SDC-600 as the communication interface between host debugger and platform target. The platform has the build option to enable secure debug protocol to unlock debug ports during boot time. The protocol is based on ARM’s ADAC (Authenticated Debug Access Control) standard.

System boot#

  • The SoC reset brings Secure Enclave (SE), that is Cortex-M0+, out of rest.

  • SE executes the BL1 ROM code based on mcuboot.

  • BL1 load, verifies and transfer execution to BL2 which is again based on mcuboot.

  • BL2 loads and verifies TF-M and host’s initial boot loader image.

  • BL2 transfer the execution to the TF-M.

  • During TF-M initialization, the host is taken out of rest.

  • Hashes of the keys used for image verification are stored in the OTP memory.

Build#

Platform solution#

The platform binaries are build using Yocto. Below is the user guide:

Arm Corstone-1000 User Guide

Secure Test#

This section can be used to test the secure enclave software independently from the host. The below configuration builds the secure enclave binaries with CI test frame integrated. On boot, secure enclave softwares stack is brought up, and CI tests starts executing at the end of the initialization process. In the below configuration, host software support is disabled, and meant only to test/verify the secure enclave softwares.

FVP#

  • Download Corstone-1000 FVP from : Arm Ecosystem FVPs

  • Install FVP by running the shell script.

  • Running of the binary will boot secure enclave software stack and at the end all CI test from tf-m-test along with platform specific tests are executed.

cd <tf-m-root>/
cmake -B build/ -S . -DCMAKE_BUILD_TYPE=Debug -DTFM_TOOLCHAIN_FILE=<tf-m-root>/toolchain_GNUARM.cmake -DTFM_PLATFORM=arm/corstone1000 -DPLATFORM_IS_FVP=TRUE -DTEST_NS=OFF -DTEST_S=ON -DEXTRA_S_TEST_SUITE_PATH=platform/ext/target/arm/corstone1000/ci_regression_tests/
cmake --build build -- install
dd conv=notrunc bs=1 if=build/install/outputs/bl1_1.bin of=build/install/outputs/bl1.bin seek=0
dd conv=notrunc bs=1 if=build/install/outputs/bl1_provisioning_bundle.bin of=build/install/outputs/bl1.bin seek=40960
./platform/ext/target/arm/corstone1000/create-flash-image.sh build/install/outputs cs1000.bin

<path-to-FVP-installation>/models/Linux64_GCC-9.3/FVP_Corstone-1000 -C board.flashloader0.fname="none" -C se.trustedBootROMloader.fname="build/install/outputs/bl1.bin" -C board.xnvm_size=64 -C se.trustedSRAM_config=6 -C se.BootROM_config="3" -C board.smsc_91c111.enabled=0  -C board.hostbridge.userNetworking=true --data board.flash0=build/install/outputs/cs1000.bin@0x68000000 -C diagnostics=4 -C disable_visualisation=true -C board.se_flash_size=8192 -C diagnostics=4  -C disable_visualisation=true

FPGA#

  • Follow the above pointed platform user guide to setup the FPGA board.

  • Use the BL1 generated from the below commands to place it inside FPGA board SD Card.

  • Use the cs1000.bin created from the below commands to place it inside FPGA board SD Card.

cd <tf-m-root>/
cmake -B build/ -S . -DCMAKE_BUILD_TYPE=Debug -DTFM_TOOLCHAIN_FILE=<tf-m-root>/toolchain_GNUARM.cmake -DTFM_PLATFORM=arm/corstone1000 -DTEST_NS=OFF -DTEST_S=ON -DTEST_S_PS=OFF -DTEST_S_PLATFORM=OFF -DEXTRA_S_TEST_SUITE_PATH=platform/ext/target/arm/corstone1000/ci_regression_tests/
cmake --build build -- install
dd conv=notrunc bs=1 if=build/install/outputs/bl1_1.bin of=build/install/outputs/bl1.bin seek=0
dd conv=notrunc bs=1 if=build/install/outputs/bl1_provisioning_bundle.bin of=build/install/outputs/bl1.bin seek=40960
./platform/ext/target/arm/corstone1000/create-flash-image.sh build/install/outputs cs1000.bin
cp build/install/outputs/bl1.bin <path-to-FPGA-SD-CARD>/SOFTWARE/
cp build/install/outputs/cs1000.bin <path-to-FPGA-SD-CARD>/SOFTWARE/

FPGA build can not compile all the CI tests into a single build as it exceeds the available RAM size. So there is a need to select few tests but not all. The above configuration disable build of -DTEST_S_PS and -DTEST_S_PLATFORM. Other test configurations are:

  • -DTEST_S_ATTESTATION=ON/OFF

  • -DTEST_S_CRYPTO=ON/OFF

  • -DTEST_S_ITS=ON/OFF

  • -DTEST_S_PS=ON/OFF

  • -DTEST_S_PLATFORM=ON/OFF

Copyright (c) 2021-2024, Arm Limited. All rights reserved.