Host MSD command + CDC virtual com example#
This section provides a step-by-step example for how to implement a host that supports CDC virtual com and MSD command. This example is based on the existing host CDC virtual com example.
USB component files#
Add the usb_host_msd component files, the usb_host_msd_ufi source file, and the host_msd_command component files into the current project. Normally, the host_msd_command component should be in the source folder, shown in Figure 2. The usb_host_msd component and the usb_host_msd_ufi source file should be located in the class folder showing in the Figure 3.
|
|
|
|
Parent topic:Host MSD command + CDC virtual com example
USB_HostEvent function#
Add the USB_HostMsdEvent function into the USB_HostEvent function.
usb_status_t USB_HostEvent(usb_device_handle deviceHandle,
usb_host_configuration_handle configurationHandle,
uint32_t event_code)
{
usb_status_t status1;
usb_status_t status2;
usb_status_t status = kStatus_USB_Success;
switch (event_code)
{
case kUSB_HostEventAttach:
status1 = USB_HostCdcEvent(deviceHandle, configurationHandle, event_code);
status2 = USB_HostMsdEvent(deviceHandle, configurationHandle, event_code);
if ((status1 == kStatus_USB_NotSupported) && (status2 ==
kStatus_USB_NotSupported))
{
status = kStatus_USB_NotSupported;
}
break;
case kUSB_HostEventNotSupported:
usb_echo("device not supported.\r\n");
break;
case kUSB_HostEventEnumerationDone:
status1 = USB_HostCdcEvent(deviceHandle, configurationHandle, event_code);
status2 = USB_HostMsdEvent(deviceHandle, configurationHandle, event_code);
if ((status1 != kStatus_USB_Success) && (status2 != kStatus_USB_Success))
{
status = kStatus_USB_Error;
}
break;
case kUSB_HostEventDetach:
status1 = USB_HostCdcEvent(deviceHandle, configurationHandle, event_code);
status2 = USB_HostMsdEvent(deviceHandle, configurationHandle, event_code);
if ((status1 != kStatus_USB_Success) && (status2 != kStatus_USB_Success))
{
status = kStatus_USB_Error;
}
break;
default:
break;
}
return status;
}
Parent topic:Host MSD command + CDC virtual com example
Main function task#
Add the USB_HostMsdTask function into the main function. The modified code should look like this:
int main(void)
{
gpio_pin_config_t pinConfig;
BOARD_InitPins();
BOARD_BootClockRUN();
BOARD_InitDebugConsole();
/* enable usb host vbus */
pinConfig.pinDirection = kGPIO_DigitalOutput;
pinConfig.outputLogic = 1U;
GPIO_PinInit(PTD, 8U, &pinConfig);
APP_init();
while (1)
{
USB_HostTaskFn(g_HostHandle);
/* cdc class task */
USB_HosCdcTask(&g_cdc);
/* msd class task */
USB_HostMsdTask(&g_MsdCommandInstance);
}
}
Parent topic:Host MSD command + CDC virtual com example