MCUXpresso SDK Documentation

Connectivity Test application setup

Connectivity Test application setup#

The figure below describes the Connectivity Test Application possible configurations.

Test bed description#

  • Running the Connectivity Test Demo Application requires a PC and two devices.

  • Connectivity Test Application CLI is accessed using the serial port of the devices.

  • Some features of the Connectivity Test Application like Packet Error Rate or Range Tests require the usage of two devices.

  • For capturing over the air traffic, an RF sniffer can be used.

  • For tests where the output power or the modulated output power of the radio should be measured, a spectrum analyzer should be used.

Parent topic:Connectivity Test application setup