![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The diff_p_interrupt.c file implements the ISSDK DIFF_P sensor driver example demonstration with Interrupt mode. More...
#include "board.h"#include "pin_mux.h"#include "clock_config.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "diff_p_drv.h"#include "systick_utils.h"
Go to the source code of this file.
Macros | |
| #define | DIFF_P_DATA_SIZE (3) /* 2 byte Pressure and 1 byte Temperature. */ |
Functions | |
| void | diff_p_isr (void *pUserData) |
| This is the Sensor Data Ready ISR implementation. More... | |
| int | main (void) |
| Main function. More... | |
Variables | |
| volatile bool | diff_pInterrupt = false |
| const registerwritelist_t | cDiffPConfigNormal [] |
| Register settings for Normal Mode. More... | |
| const registerwritelist_t | cDiffPClearStatusBits [] |
| Register settings for Clearing Pressure and Temperature Data Ready Bits. More... | |
| const registerreadlist_t | cDiffPStatus [] = {{.readFrom = DIFF_P_INT_STATUS_0, .numBytes = 1}, __END_READ_DATA__} |
| Address of Status Register. More... | |
| const registerreadlist_t | cDiffPOutputNormal [] |
| Address and size of Raw Pressure+Temperature Data in Normal Mode. More... | |
The diff_p_interrupt.c file implements the ISSDK DIFF_P sensor driver example demonstration with Interrupt mode.
Definition in file diff_p_interrupt.c.
Definition at line 61 of file diff_p_interrupt.c.
Referenced by main().
| void diff_p_isr | ( | void * | pUserData | ) |
This is the Sensor Data Ready ISR implementation.
This function sets the flag which indicates if a new sample(s) is available for reading.
| [in] | pUserData | This is a void pointer to the instance of the user specific data structure for the ISR. |
Set flag to indicate Sensor has signalled data ready.
Definition at line 102 of file diff_p_interrupt.c.
References diff_pInterrupt.
Referenced by main().

| int main | ( | void | ) |
Main function.
Initialize INT1_DIFF_P pin used by FRDM board
Initialize RGB LED pin used by FRDM board
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize DIFF_P sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the DIFF_P sensor.
Clear the data ready flag, it will be set again by the ISR.
Check for both data ready bits from the DIFF_P.
Read new raw sensor data from the DIFF_P.
Explicitly clear the Status Bits.
Process the sample and convert the raw sensor data.
Definition at line 110 of file diff_p_interrupt.c.
References ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), BOARD_SystickEnable(), data, diff_p_i2c_sensorhandle_t::deviceInfo, DIFF_P_DATA_SIZE, DIFF_P_I2C_ADDR, DIFF_P_I2C_Configure(), DIFF_P_I2C_Initialize(), DIFF_P_I2C_ReadData(), DIFF_P_I2C_SetIdleTask(), DIFF_P_INT1, DIFF_P_INT_STATUS_0_PDR_DRDY, DIFF_P_INT_STATUS_0_PDR_MASK, DIFF_P_INT_STATUS_0_TDR_DRDY, DIFF_P_INT_STATUS_0_TDR_MASK, diff_p_isr(), DIFF_P_NPS3000VV_WHOAMI_VALUE, DIFF_P_NPS3001DV_WHOAMI_VALUE, DIFF_P_NPS3002VV_WHOAMI_VALUE, DIFF_P_NPS3005DV_WHOAMI_VALUE, diff_pInterrupt, Driver_GPIO_KSDK, GPIO_DIRECTION_IN, GPIO_DIRECTION_OUT, GREEN_LED, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, int32_t(), NPS3000VV_PRESSURE_DIV_FACTOR, NPS3001DV_PRESSURE_DIV_FACTOR, NPS3002VV_PRESSURE_DIV_FACTOR, NPS3005DV_PRESSURE_DIV_FACTOR, diff_p_i2c_sensorhandle_t::pCommDrv, GENERIC_DRIVER_GPIO::pin_init, diff_p_pressuredata_t::pressure, rawData, SENSOR_ERROR_NONE, Sensor_I2C_Write(), diff_p_i2c_sensorhandle_t::slaveAddress, SMC, SMC_SetPowerModeWait(), status, diff_p_pressuredata_t::temperature, and GENERIC_DRIVER_GPIO::toggle_pin.

| const registerwritelist_t cDiffPClearStatusBits[] |
Register settings for Clearing Pressure and Temperature Data Ready Bits.
Definition at line 81 of file diff_p_interrupt.c.
| const registerwritelist_t cDiffPConfigNormal[] |
Register settings for Normal Mode.
Definition at line 72 of file diff_p_interrupt.c.
| const registerreadlist_t cDiffPOutputNormal[] |
Address and size of Raw Pressure+Temperature Data in Normal Mode.
Definition at line 88 of file diff_p_interrupt.c.
| const registerreadlist_t cDiffPStatus[] = {{.readFrom = DIFF_P_INT_STATUS_0, .numBytes = 1}, __END_READ_DATA__} |
Address of Status Register.
Definition at line 85 of file diff_p_interrupt.c.
| volatile bool diff_pInterrupt = false |
Definition at line 66 of file diff_p_interrupt.c.
Referenced by diff_p_isr(), and main().