57 #define MMA845x_COUNTSPERG 8192.0 58 #define MMA8451_ACCEL_FIFO_SIZE 32 123 #if (ACCEL_ODR_HZ <= 1) 125 #elif (ACCEL_ODR_HZ <= 6) 127 #elif (ACCEL_ODR_HZ <= 12) 129 #elif (ACCEL_ODR_HZ <= 50) 131 #elif (ACCEL_ODR_HZ <= 100) 133 #elif (ACCEL_ODR_HZ <= 200) 135 #elif (ACCEL_ODR_HZ <= 400) 150 #if (ACCEL_ODR_HZ <= 1) 152 #elif (ACCEL_ODR_HZ <= 6) 154 #elif (ACCEL_ODR_HZ <= 12) 156 #elif (ACCEL_ODR_HZ <= 50) 158 #elif (ACCEL_ODR_HZ <= 100) 160 #elif (ACCEL_ODR_HZ <= 200) 162 #elif (ACCEL_ODR_HZ <= 400) 181 sfg->Accel.iWhoAmI = reg;
206 sfg->Accel.isEnabled =
true;
216 uint8_t sensor_fifo_count = 1;
228 sensor_fifo_count = I2C_Buffer[0] & 0x3F;
230 sensor_fifo_count = (I2C_Buffer[0] & 0x08)>>3;
240 MMA845x_DATA_READ[0].
numBytes = 6 * sensor_fifo_count;
244 for (j = 0; j < sensor_fifo_count; j++)
246 sample[
CHX] = (I2C_Buffer[6 * j ] << 8) | I2C_Buffer[6 * j + 1];
247 sample[
CHY] = (I2C_Buffer[6 * j + 2] << 8) | I2C_Buffer[6 * j + 3];
248 sample[
CHZ] = (I2C_Buffer[6 * j + 4] << 8) | I2C_Buffer[6 * j + 5];
273 sfg->Accel.isEnabled =
false;
279 #endif // F_USING_ACCEL The sensor_drv.h file contains sensor state and error definitions.
#define __END_WRITE_DATA__
void * bus_driver
should be of type (ARM_DRIVER_I2C* for I2C-based sensors, ARM_DRIVER_SPI* for SPI) ...
#define CHY
Used to access Y-channel entries in various data data structures.
int32_t Sensor_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerreadlist_t *pReadList, uint8_t *pOutBuffer)
Read register data from a sensor.
#define ACCEL_FIFO_SIZE
FXOS8700 (accel), MMA8652, FXLS8952 all have 32 element FIFO.
#define __END_READ_DATA__
The top level fusion structure.
#define MMA8452_WHO_AM_I_WHOAMI_VALUE
uint16_t addr
I2C address if applicable.
void addToFifo(union FifoSensor *sensor, uint16_t maxFifoSize, int16_t sample[3])
addToFifo is called from within sensor driver read functions
The sensor_fusion.h file implements the top level programming interface.
The FifoSensor union allows us to use common pointers for Accel, Mag & Gyro logical sensor structures...
#define CHZ
Used to access Z-channel entries in various data data structures.
uint16_t isInitialized
Bitfields to indicate sensor is active (use SensorBitFields from build.h)
registerDeviceInfo_t deviceInfo
I2C device context.
Provides function prototypes for driver level interfaces.
#define CHX
Used to access X-channel entries in various data data structures.
void conditionSample(int16_t sample[3])
conditionSample ensures that we never encounter the maximum negative two's complement value for a 16-...
The mma845x.h contains the MMA845x sensor register definitions and its bit mask.
#define MMA845x_COUNTSPERG
int32_t Register_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register.
#define MMA8453_WHO_AM_I_WHOAMI_VALUE
This structure defines the Write command List.
This structure defines the Read command List.
#define F_USING_ACCEL
nominally 0x0001 if an accelerometer is to be used, 0x0000 otherwise
#define MMA8451_ACCEL_FIFO_SIZE
An instance of PhysicalSensor structure type should be allocated for each physical sensors (combo dev...
The sensor_io_i2c.h file declares low-level interface functions for reading and writing sensor regist...
#define MMA8451_WHO_AM_I_WHOAMI_VALUE
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor.