![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The fxas21002_interrupt.c file implements the ISSDK FXAS21002 sensor driver example demonstration with interrupt mode. More...
#include "board.h"#include "pin_mux.h"#include "clock_config.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "gpio_driver.h"#include "fxas21002_drv.h"
Go to the source code of this file.
Functions | |
| void | fxas21002_isr (void *pUserData) |
| This is the Sensor Data Ready ISR implementation. More... | |
| int | main (void) |
| This is the The main function implementation. More... | |
Variables | |
| const registerwritelist_t | fxas21002_Config_Isr [] |
| const registerreadlist_t | fxas21002_DRDY [] = {{.readFrom = FXAS21002_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| const registerreadlist_t | fxas21002_Output_Values [] |
| volatile bool | fxas21002Interrupt = false |
The fxas21002_interrupt.c file implements the ISSDK FXAS21002 sensor driver example demonstration with interrupt mode.
Definition in file fxas21002_interrupt.c.
| void fxas21002_isr | ( | void * | pUserData | ) |
This is the Sensor Data Ready ISR implementation.
This function sets the flag which indicates if a new sample(s) is available for reading.
| [in] | pUserData | This is a void pointer to the instance of the user specific data structure for the ISR. |
Set flag to indicate Sensor has signalled data ready.
Definition at line 96 of file fxas21002_interrupt.c.
References fxas21002Interrupt.
Referenced by main().

| int main | ( | void | ) |
This is the The main function implementation.
This function invokes board initializes routines, then then brings up the sensor and finally enters an endless loop to continuously read available samples.
| [in] | void | This is no input parameter. |
Initialize the MCU hardware.
Initialize INT1_FXAS21002 pin used by FRDM board
Initialize RGB LED pin used by FRDM board
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the FXAS21002 sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the FXAS21002 sensor driver.
Clear the data ready flag, it will be set again by the ISR.
Read the raw sensor data from the FXAS21002.
Convert the raw sensor data to signed 16-bit container for display to the debug port.
Definition at line 110 of file fxas21002_interrupt.c.
References ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, Driver_GPIO_KSDK, FXAS21002_GYRO_DATA_SIZE, FXAS21002_I2C_ADDR, FXAS21002_I2C_Configure(), FXAS21002_I2C_Initialize(), FXAS21002_I2C_ReadData(), FXAS21002_I2C_SetIdleTask(), FXAS21002_INT1, fxas21002_isr(), FXAS21002_WHO_AM_I_WHOAMI_PROD_VALUE, fxas21002Interrupt, GPIO_DIRECTION_IN, GPIO_DIRECTION_OUT, GREEN_LED, fxas21002_gyrodata_t::gyro, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, int32_t(), GENERIC_DRIVER_GPIO::pin_init, rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeWait(), status, and GENERIC_DRIVER_GPIO::toggle_pin.

| const registerwritelist_t fxas21002_Config_Isr[] |
Prepare the register write list to configure FXAS21002 in non-FIFO mode.
Definition at line 65 of file fxas21002_interrupt.c.
| const registerreadlist_t fxas21002_DRDY[] = {{.readFrom = FXAS21002_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Prepare the register read list to read FXAS21002 DataReady status.
Definition at line 75 of file fxas21002_interrupt.c.
| const registerreadlist_t fxas21002_Output_Values[] |
Prepare the register read list to read the raw gyro data from the FXAS21002.
Definition at line 78 of file fxas21002_interrupt.c.
| volatile bool fxas21002Interrupt = false |
Definition at line 83 of file fxas21002_interrupt.c.
Referenced by fxas21002_isr(), and main().