44 #include "clock_config.h"    45 #include "fsl_debug_console.h"    48 #include "Driver_I2C.h"    51 #include "issdk_hal.h"    57 #define RAW_ACCELMAG_DATA_SIZE (12)   106     PRINTF(
"\r\n ISSDK FXOS8700 sensor driver example demonstration with poll mode\r\n");
   110     if (ARM_DRIVER_OK != status)
   112         PRINTF(
"\r\n I2C Initialization Failed\r\n");
   117     status = I2Cdrv->PowerControl(ARM_POWER_FULL);
   118     if (ARM_DRIVER_OK != status)
   120         PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
   125     status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   126     if (ARM_DRIVER_OK != status)
   128         PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
   137         PRINTF(
"\r\n Sensor Initialization Failed\r\n");
   140     PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
   149         PRINTF(
"\r\n FXOS8700 Sensor Configuration Failed, Err = %d\r\n", status);
   152     PRINTF(
"\r\n Successfully Applied FXOS8700 Sensor Configuration\r\n");
   165         if (ARM_DRIVER_OK != status)
   167             PRINTF(
"\r\n Read Failed. \r\n");
   172         rawData.
accel[0] = ((int16_t)data[0] << 8) | data[1];
   173         rawData.
accel[0] /= 4;
   174         rawData.
accel[1] = ((int16_t)data[2] << 8) | data[3];
   175         rawData.
accel[1] /= 4;
   176         rawData.
accel[2] = ((int16_t)data[4] << 8) | data[5];
   177         rawData.
accel[2] /= 4;
   178         rawData.
mag[0] = ((int16_t)data[6] << 8) | data[7];
   179         rawData.
mag[1] = ((int16_t)data[8] << 8) | data[9];
   180         rawData.
mag[2] = ((int16_t)data[10] << 8) | data[11];
   183         PRINTF(
"\r\n Accel X = %d  Y = %d  Z = %d\r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
   184         PRINTF(
"\r\n Mag   X = %d  Y = %d  Z = %d\r\n", rawData.
mag[0], rawData.
mag[1], rawData.
mag[2]);
 #define FXOS8700_M_CTRL_REG1_M_HMS_MASK
 
#define FXOS8700_M_CTRL_REG1_M_ACAL_EN
 
#define __END_WRITE_DATA__
 
The fxos8700_drv.h file describes the fxos8700 driver interface and structures. 
 
This structure defines the fxos8700 raw data buffer. 
 
void FXOS8700_I2C_SetIdleTask(fxos8700_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define BOARD_BootClockRUN
 
const registerreadlist_t FXOS8700_STATUS_READ[]
 
uint8_t data[FXLS8962_DATA_SIZE]
 
void BOARD_InitDebugConsole(void)
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
This defines the sensor specific information for I2C. 
 
const registerwritelist_t fxos8700_Config_Hybrid[]
 
#define FXOS8700_M_CTRL_REG2_M_RST_CNT_DISABLE
 
#define __END_READ_DATA__
 
const registerreadlist_t FXOS8700_ACCELMAG_READ[]
 
#define FXOS8700_CTRL_REG1_DR_HYBRID_25_HZ
 
const registerreadlist_t FXOS8700_ACCEL_MAG_READ[]
 
#define FXOS8700_WHO_AM_I_PROD_VALUE
 
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_MASK
 
#define FXOS8700_M_CTRL_REG1_M_ACAL_MASK
 
#define ASK_USER_TO_RESUME(x)
 
int main(void)
Main function. 
 
int32_t FXOS8700_I2C_Initialize(fxos8700_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
int32_t FXOS8700_I2C_ReadData(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_HYBRID_MODE
 
#define I2C_S_DEVICE_INDEX
 
#define FXOS8700_M_CTRL_REG2_M_RST_CNT_MASK
 
int32_t FXOS8700_I2C_Configure(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
#define FXOS8700_CTRL_REG1_DR_MASK
 
fxls8962_acceldataUser_t rawData
 
#define FXOS8700_DR_STATUS_ZYXDR_MASK
 
This structure defines the Write command List. 
 
This structure defines the Read command List. 
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
#define RAW_ACCELMAG_DATA_SIZE
 
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features. 
 
#define FXOS8700_I2C_ADDR
 
#define FXOS8700_M_CTRL_REG1_M_HMS_HYBRID_MODE
 
#define I2C_S_SIGNAL_EVENT