46 #include "clock_config.h"    47 #include "fsl_debug_console.h"    52 #include "Driver_I2C.h"    55 #include "issdk_hal.h"    62 #define FIFO_WATERMARK (16)             63 #define MMA865x_ACCEL_DATA_SIZE (6)    108     PRINTF(
"\r\n ISSDK MMA865x sensor driver example for FIFO Mode. \r\n");
   112     if (ARM_DRIVER_OK != status)
   114         PRINTF(
"\r\n I2C Initialization Failed\r\n");
   119     status = I2Cdrv->PowerControl(ARM_POWER_FULL);
   120     if (ARM_DRIVER_OK != status)
   122         PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
   127     status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   128     if (ARM_DRIVER_OK != status)
   130         PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
   139         PRINTF(
"\r\n Sensor Initialization Failed\r\n");
   142     PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
   151         PRINTF(
"\r\n MMA865x Sensor Configuration Failed, Err = %d \r\n", status);
   154     PRINTF(
"\r\n MMA865x now active and entering data read loop... \r\n");
   167         if (ARM_DRIVER_OK != status)
   169             PRINTF(
"\r\n Read Failed. \r\n");
   178             rawData.
accel[0] /= 16;
   181             rawData.
accel[1] /= 16;
   184             rawData.
accel[2] /= 16;
   188         PRINTF(
"\r\n Accel X = %d  Y = %d  Z = %d \r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
 #define MMA865x_XYZ_DATA_CFG_FS_MASK
 
#define __END_WRITE_DATA__
 
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
This structure defines the mma865x raw data buffer. 
 
#define MMA865x_F_SETUP_F_MODE_STOP_MODE
 
#define BOARD_BootClockRUN
 
#define MMA865x_F_STATUS_F_WMKF_MASK
 
uint8_t data[FXLS8962_DATA_SIZE]
 
int32_t MMA865x_I2C_ReadData(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
void BOARD_InitDebugConsole(void)
 
This defines the sensor specific information. 
 
const registerreadlist_t cMma865xFifoStatus[]
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
#define MMA865x_CTRL_REG1_DR_MASK
 
#define __END_READ_DATA__
 
#define MMA865x_F_SETUP_F_WMRK_MASK
 
const registerwritelist_t cMma865xConfigFifo[]
 
#define MMA865x_CTRL_REG1_DR_100HZ
 
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define MMA8652_WHOAMI_VALUE
 
const registerreadlist_t cMma865xOutputValues[]
 
#define ASK_USER_TO_RESUME(x)
 
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
#define MMA865x_XYZ_DATA_CFG_FS_2G
 
#define MMA865x_CTRL_REG2_MODS_MASK
 
#define MMA865x_ACCEL_DATA_SIZE
 
#define I2C_S_DEVICE_INDEX
 
#define MMA865x_F_SETUP_F_MODE_MASK
 
The mma865x_drv.h file describes the MMA865x driver interface and structures. 
 
fxls8962_acceldataUser_t rawData
 
#define MMA865x_CTRL_REG2_MODS_HR
 
This structure defines the Write command List. 
 
This structure defines the Read command List. 
 
int main(void)
Main function. 
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features. 
 
#define I2C_S_SIGNAL_EVENT