![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The fxls8471q_poll_spi.c file implements the ISSDK FXLS8471Q sensor driver example demonstration for SPI Mode with polling. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "issdk_hal.h"#include "gpio_driver.h"#include "fxls8471q_drv.h"#include "Driver_SPI.h"
Go to the source code of this file.
Functions | |
| int | main (void) |
| This is the The main function implementation. More... | |
Variables | |
| const registerwritelist_t | cFxls8471q_Config_Normal [] |
| const registerreadlist_t | cFxls8471q_DataReady [] = {{.readFrom = FXLS8471Q_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| const registerreadlist_t | cFxls8471q_Output_Values [] |
The fxls8471q_poll_spi.c file implements the ISSDK FXLS8471Q sensor driver example demonstration for SPI Mode with polling.
Definition in file fxls8471q_spi_poll.c.
| int main | ( | void | ) |
This is the The main function implementation.
This function invokes board initializes routines, then then brings up the sensor and finally enters an endless loop to continuously read available samples.
| [in] | void | This is no input parameter. |
Initialize the MCU hardware.
Initialize the SPI driver.
Set the SPI Power mode.
Set the SPI Slave speed.
Initialize the FXLS8471Q sensor driver.
Set the task to be executed while waiting for SPI transactions to complete.
Configure the FXLS8471Q sensor driver.
Wait for data ready from the FXLS8471Q.
Read the raw sensor data from the FXLS8471Q.
Convert the raw sensor data to signed 16-bit container for display to the debug port.
Definition at line 63 of file fxls8471q_spi_poll.c.
References fxls8471q_acceldata_t::accel, ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, FXLS8471_SPI_CS, FXLS8471Q_ACCEL_DATA_SIZE, FXLS8471Q_SPI_Configure(), FXLS8471Q_SPI_Initialize(), FXLS8471Q_SPI_ReadData(), FXLS8471Q_SPI_SetIdleTask(), FXLS8471Q_STATUS_ZYXDR_MASK, FXLS8471Q_WHO_AM_I_WHOAMI_VALUE, gFxls8471qDataReady, int32_t(), rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), SPI_S_BAUDRATE, SPI_S_DEVICE_INDEX, SPI_S_DRIVER, SPI_S_SIGNAL_EVENT, and status.

| const registerwritelist_t cFxls8471q_Config_Normal[] |
Prepare the register write list to configure FXLS8471Q in non-FIFO mode.
Definition at line 39 of file fxls8471q_spi_poll.c.
| const registerreadlist_t cFxls8471q_DataReady[] = {{.readFrom = FXLS8471Q_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Prepare the register read list to read FXLS8471Q DataReady status.
Definition at line 45 of file fxls8471q_spi_poll.c.
| const registerreadlist_t cFxls8471q_Output_Values[] |
Prepare the register read list to read the raw accel data from the FXLS8471Q.
Definition at line 48 of file fxls8471q_spi_poll.c.