![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The fxps7250a4_interrupt.c file implements the ISSDK FXPS7250A4 analog sensor driver example demonstration with interrupt mode. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_lptmr.h"#include "fsl_adc12.h"#include "fsl_debug_console.h"#include "issdk_hal.h"#include "gpio_driver.h"
Go to the source code of this file.
Macros | |
| #define | pa7250_odr_callback PWT_LPTMR0_IRQHandler |
| #define | adc12_irq_callback ADC0_IRQHandler |
| #define | FXPS7250A4_ODR_ms 1000U |
Functions | |
| void | KE15Z_LPTMR0_ADC0_Initialize (void) |
| float | analog_output_transfer_fn (float volt) |
| void | pa7250_odr_callback (void) |
| void | adc12_irq_callback (void) |
| int | main (void) |
| Main function. More... | |
Variables | |
| volatile uint32_t | gAdcConversionValue |
| volatile bool | bAdcCompletedFlag = false |
| adc12_channel_config_t | gAdcChannelConfigStruct |
The fxps7250a4_interrupt.c file implements the ISSDK FXPS7250A4 analog sensor driver example demonstration with interrupt mode.
Definition in file fxps7250a4_interrupt.c.
| #define adc12_irq_callback ADC0_IRQHandler |
Definition at line 36 of file fxps7250a4_interrupt.c.
| #define FXPS7250A4_ODR_ms 1000U |
Definition at line 39 of file fxps7250a4_interrupt.c.
Referenced by KE15Z_LPTMR0_ADC0_Initialize().
| #define pa7250_odr_callback PWT_LPTMR0_IRQHandler |
Definition at line 34 of file fxps7250a4_interrupt.c.
| void adc12_irq_callback | ( | void | ) |
Definition at line 67 of file fxps7250a4_interrupt.c.
References bAdcCompletedFlag, FXPS7250A4_ADC12_CHANNEL_GROUP, and gAdcConversionValue.
| float analog_output_transfer_fn | ( | float | volt | ) |
Definition at line 107 of file fxps7250a4_interrupt.c.
References FXPS7250A4_OFFSET.
Referenced by main().

| void KE15Z_LPTMR0_ADC0_Initialize | ( | void | ) |
Definition at line 74 of file fxps7250a4_interrupt.c.
References FXPS7250A4_ADC12_CHANNEL, FXPS7250A4_ODR_ms, and gAdcChannelConfigStruct.
Referenced by main().

| int main | ( | void | ) |
Main function.
Initialize GREEN LED pin used by FRDM board
Definition at line 118 of file fxps7250a4_interrupt.c.
References analog_output_transfer_fn(), ASK_USER_TO_RESUME, bAdcCompletedFlag, BIT12RES, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), Driver_GPIO_KSDK, gAdcConversionValue, GPIO_DIRECTION_OUT, GREEN_LED, KE15Z_LPTMR0_ADC0_Initialize(), GENERIC_DRIVER_GPIO::pin_init, SMC, SMC_SetPowerModeWait(), GENERIC_DRIVER_GPIO::toggle_pin, and VCC.

| void pa7250_odr_callback | ( | void | ) |
Definition at line 59 of file fxps7250a4_interrupt.c.
References FXPS7250A4_ADC12_CHANNEL_GROUP, and gAdcChannelConfigStruct.
| volatile bool bAdcCompletedFlag = false |
Definition at line 45 of file fxps7250a4_interrupt.c.
Referenced by adc12_irq_callback(), and main().
| adc12_channel_config_t gAdcChannelConfigStruct |
Definition at line 46 of file fxps7250a4_interrupt.c.
Referenced by KE15Z_LPTMR0_ADC0_Initialize(), and pa7250_odr_callback().
| volatile uint32_t gAdcConversionValue |
Definition at line 44 of file fxps7250a4_interrupt.c.
Referenced by adc12_irq_callback(), and main().