ISSDK  1.8
IoT Sensing Software Development Kit
driver_MMA8652.c
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015, Freescale Semiconductor, Inc.
3  * Copyright 2016-2017 NXP
4  * All rights reserved.
5  *
6  * SPDX-License-Identifier: BSD-3-Clause
7  */
8 
9 /*! \file driver_MMA8652.c
10  \brief Provides init() and read() functions for the MMA8652 3-axis accel family.
11 
12 1G*/
13 
14 #include "board.h" // generated by Kinetis Expert. Long term - merge sensor_board.h into this file
15 #include "sensor_fusion.h" // Sensor fusion structures and types
16 #include "sensor_drv.h"
17 #include "sensor_io_i2c.h" // Required for registerreadlist_t / registerwritelist_t declarations
18 #include "mma865x.h"
19 #include "drivers.h" // Device specific drivers supplied by NXP (can be replaced with user drivers)
20 #define MMA8652_COUNTSPERG 8192.0
21 #define MMA8652_ACCEL_FIFO_SIZE 32
22 
23 #if F_USING_ACCEL
24 
25 // Command definition to read the WHO_AM_I value.
26 const registerreadlist_t MMA8652_WHO_AM_I_READ[] =
27 {
28  { .readFrom = MMA865x_WHO_AM_I, .numBytes = 1 }, __END_READ_DATA__
29 };
30 
31 // Command definition to read the number of entries in the accel FIFO.
32 const registerreadlist_t MMA8652_F_STATUS_READ[] =
33 {
34  { .readFrom = MMA865x_STATUS, .numBytes = 1 }, __END_READ_DATA__
35 };
36 
37 // Command definition to read the number of entries in the accel FIFO.
38 registerreadlist_t MMA8652_DATA_READ[] =
39 {
40  { .readFrom = MMA865x_OUT_X_MSB, .numBytes = 6 }, __END_READ_DATA__
41 };
42 
43 // Each entry in a RegisterWriteList is composed of: register address, value to write, bit-mask to apply to write (0 enables)
44 const registerwritelist_t MMA8652_Initialization[] =
45 {
46  // write 0000 0000 = 0x00 to CTRL_REG1 to place MMA8652 into standby
47  // [7-1] = 0000 000
48  // [0]: active=0
49  { MMA865x_CTRL_REG1, 0x00, 0x00 },
50 
51  // write 0000 0000 = 0x00 to CTRL_REG1 to place MMA8652 into standby
52  // [7-1] = 0000 000
53  // [0]: active=0
54  { MMA865x_F_SETUP, 0x40, 0x00 },
55 
56  // OK: write 0000 0001 = 0x01 to XYZ_DATA_CFG register to set g range
57  // [7-5]: reserved=000
58  // [4]: HPF_OUT=0
59  // [3-2]: reserved=00
60  // [1-0]: FS=01 for +/-4g: 512 counts / g = 8192 counts / g after 4 bit left shift
61  { MMA865x_XYZ_DATA_CFG, 0x01, 0x00 },
62 
63  // OK: write 0000 0010 = 0x02 to CTRL_REG2 to set MODS bits
64  // [7]: ST=0: self test disabled
65  // [6]: RST=0: reset disabled
66  // [5]: unused
67  // [4-3]: SMODS=00
68  // [2]: SLPE=0: auto sleep disabled
69  // [1-0]: mods=10 for high resolution (maximum over sampling)
70  { MMA865x_CTRL_REG2, 0x02, 0x00 },
71 
72  // write 00XX X001 to CTRL_REG1 to set data rate and exit standby
73  // [7-6]: aslp_rate=00
74  // [5-3]: dr=111 for 1.56Hz data rate giving 0x39
75  // [5-3]: dr=110 for 6.25Hz data rate giving 0x31
76  // [5-3]: dr=101 for 12.5Hz data rate giving 0x29
77  // [5-3]: dr=100 for 50Hz data rate giving 0x21
78  // [5-3]: dr=011 for 100Hz data rate giving 0x19
79  // [5-3]: dr=010 for 200Hz data rate giving 0x11
80  // [5-3]: dr=001 for 400Hz data rate giving 0x09
81  // [5-3]: dr=000 for 800Hz data rate giving 0x01
82  // [2]: unused=0
83  // [1]: f_read=0 for normal 16 bit reads
84  // [0]: active=1 to take the part out of standby and enable sampling
85 #if (ACCEL_ODR_HZ <= 1)
86  { MMA865x_CTRL_REG1, 0x39, 0x00 }, // select 1.5625Hz ODR,
87 #elif (ACCEL_ODR_HZ <= 6)
88  { MMA865x_CTRL_REG1, 0x31, 0x00 }, // select 6.25Hz ODR
89 #elif (ACCEL_ODR_HZ <= 12)
90  { MMA865x_CTRL_REG1, 0x29, 0x00 }, // select 12.5Hz ODR
91 #elif (ACCEL_ODR_HZ <= 50)
92  { MMA865x_CTRL_REG1, 0x21, 0x00 }, // select 50Hz ODR
93 #elif (ACCEL_ODR_HZ <= 100)
94  { MMA865x_CTRL_REG1, 0x19, 0x00 }, // select 100Hz ODR
95 #elif (ACCEL_ODR_HZ <= 200)
96  { MMA865x_CTRL_REG1, 0x11, 0x00 }, // select 200Hz ODR
97 #elif (ACCEL_ODR_HZ <= 400)
98  { MMA865x_CTRL_REG1, 0x09, 0x00 }, // select 400Hz ODR
99 #else
100  { MMA865x_CTRL_REG1, 0x01, 0x00 }, // select 800Hz ODR
101 #endif
103 };
104 
105 // All sensor drivers and initialization functions have the same prototype.
106 // sfg is a pointer to the master "global" sensor fusion structure.
107 // sensor = pointer to linked list element used by the sensor fusion subsystem to specify required sensors
108 
109 // sfg = pointer to top level (generally global) data structure for sensor fusion
110 int8_t MMA8652_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
111 {
112  int32_t status;
113  uint8_t reg;
114  status = Register_I2C_Read(sensor->bus_driver, &sensor->deviceInfo, sensor->addr, MMA865x_WHO_AM_I, 1, &reg);
115  if (status==SENSOR_ERROR_NONE) {
116  sfg->Accel.iWhoAmI = reg;
117  if (reg != MMA8652_WHOAMI_VALUE) return(SENSOR_ERROR_INIT);
118  } else {
119  return(status);
120  }
121 
122  status = Sensor_I2C_Write(sensor->bus_driver, &sensor->deviceInfo, sensor->addr, MMA8652_Initialization );
123  // Stash some needed constants in the SF data structure for this sensor
124  sfg->Accel.iCountsPerg = MMA8652_COUNTSPERG;
125  sfg->Accel.fgPerCount = 1.0F / MMA8652_COUNTSPERG;
126  sfg->Accel.fgPerCount = 1.0F / MMA8652_COUNTSPERG;
127 
128  sensor->isInitialized = F_USING_ACCEL;
129  sfg->Accel.isEnabled = true;
130 
131  return (status);
132 }
133 
134 int8_t MMA8652_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
135 {
136  uint8_t I2C_Buffer[6 * MMA8652_ACCEL_FIFO_SIZE]; // I2C read buffer
137  int8_t status; // I2C transaction status
138  int8_t j; // scratch
139  uint8_t sensor_fifo_count = 1;
140  int16_t sample[3];
141 
142  if(sensor->isInitialized != F_USING_ACCEL)
143  {
144  return SENSOR_ERROR_INIT;
145  }
146 
147  // read the F_STATUS register (mapped to STATUS) and extract number of measurements available (lower 6 bits)
148  status = Sensor_I2C_Read(sensor->bus_driver, &sensor->deviceInfo, sensor->addr, MMA8652_F_STATUS_READ, I2C_Buffer );
149  if (status==SENSOR_ERROR_NONE) {
150  sensor_fifo_count = I2C_Buffer[0] & 0x3F;
151  // return if there are no measurements in the sensor FIFO.
152  // this will only occur when the FAST_LOOP_HZ equals or exceeds ACCEL_ODR_HZ
153  if (sensor_fifo_count == 0) return SENSOR_ERROR_READ;
154  } else {
155  return(status);
156  }
157 
158  MMA8652_DATA_READ[0].readFrom = MMA865x_OUT_X_MSB;
159  MMA8652_DATA_READ[0].numBytes = 6 * sensor_fifo_count;
160  status = Sensor_I2C_Read(sensor->bus_driver, &sensor->deviceInfo, sensor->addr, MMA8652_DATA_READ, I2C_Buffer );
161 
162  if (status==SENSOR_ERROR_NONE) {
163  for (j = 0; j < sensor_fifo_count; j++)
164  {
165  sample[CHX] = (I2C_Buffer[6 * j ] << 8) | I2C_Buffer[6 * j + 1];
166  sample[CHY] = (I2C_Buffer[6 * j + 2] << 8) | I2C_Buffer[6 * j + 3];
167  sample[CHZ] = (I2C_Buffer[6 * j + 4] << 8) | I2C_Buffer[6 * j + 5];
168  conditionSample(sample); // truncate negative values to -32767
169  addToFifo((union FifoSensor*) &(sfg->Accel), ACCEL_FIFO_SIZE, sample);
170  }
171  }
172 
173  return (status);
174 }
175 
176 
177 // Each entry in a RegisterWriteList is composed of: register address, value to write, bit-mask to apply to write (0 enables)
178 const registerwritelist_t MMA8652_IDLE[] =
179 {
180  // Set ACTIVE = other bits unchanged
181  { MMA865x_CTRL_REG1, 0x00, 0x01 },
183 };
184 
185 // MMA8652_Idle places the sensor into SLEEP mode (wakeup time = 2/ODR+1ms)
186 int8_t MMA8652_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
187 {
188  int32_t status;
189  if(sensor->isInitialized == F_USING_ACCEL) {
190  status = Sensor_I2C_Write(sensor->bus_driver, &sensor->deviceInfo, sensor->addr, MMA8652_IDLE );
191  sensor->isInitialized = 0;
192  sfg->Accel.isEnabled = false;
193  } else {
194  return SENSOR_ERROR_INIT;
195  }
196  return status;
197 }
198 
199 #endif // F_USING_ACCEL
int32_t Sensor_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerreadlist_t *pReadList, uint8_t *pOutBuffer)
Read register data from a sensor.
void * bus_driver
should be of type (ARM_DRIVER_I2C* for I2C-based sensors, ARM_DRIVER_SPI* for SPI) ...
This structure defines the Write command List.
Definition: sensor_drv.h:68
int32_t status
#define F_USING_ACCEL
nominally 0x0001 if an accelerometer is to be used, 0x0000 otherwise
int8_t MMA8652_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
Provides function prototypes for driver level interfaces.
int32_t Register_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register.
An instance of PhysicalSensor structure type should be allocated for each physical sensors (combo dev...
int8_t MMA8652_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
void conditionSample(int16_t sample[3])
conditionSample ensures that we never encounter the maximum negative two&#39;s complement value for a 16-...
#define CHZ
Used to access Z-channel entries in various data data structures.
Definition: sensor_fusion.h:62
void addToFifo(union FifoSensor *sensor, uint16_t maxFifoSize, int16_t sample[3])
addToFifo is called from within sensor driver read functions
The sensor_drv.h file contains sensor state and error definitions.
#define __END_WRITE_DATA__
Definition: sensor_drv.h:45
The top level fusion structure.
#define CHY
Used to access Y-channel entries in various data data structures.
Definition: sensor_fusion.h:61
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define MMA8652_ACCEL_FIFO_SIZE
#define ACCEL_FIFO_SIZE
FXOS8700 (accel), MMA8652, FXLS8952 all have 32 element FIFO.
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor.
Definition: sensor_io_i2c.c:71
registerDeviceInfo_t deviceInfo
I2C device context.
int8_t MMA8652_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
The sensor_fusion.h file implements the top level programming interface.
#define __END_READ_DATA__
Definition: sensor_drv.h:51
SensorFusionGlobals sfg
uint16_t readFrom
Definition: sensor_drv.h:80
uint16_t isInitialized
Bitfields to indicate sensor is active (use SensorBitFields from build.h)
This structure defines the Read command List.
Definition: sensor_drv.h:78
#define CHX
Used to access X-channel entries in various data data structures.
Definition: sensor_fusion.h:60
The FifoSensor union allows us to use common pointers for Accel, Mag & Gyro logical sensor structures...
uint16_t addr
I2C address if applicable.
#define MMA8652_COUNTSPERG
#define MMA8652_WHOAMI_VALUE
Definition: mma865x.h:65
The sensor_io_i2c.h file declares low-level interface functions for reading and writing sensor regist...