ISSDK  1.8
IoT Sensing Software Development Kit
Functions
sensor_fusion.c File Reference

The sensor_fusion.c file implements the top level programming interface. More...

#include <stdio.h>
#include "sensor_fusion.h"
#include "magnetic.h"
#include "drivers.h"
#include "sensor_drv.h"
#include "status.h"
#include "control.h"
#include "fusion.h"
Include dependency graph for sensor_fusion.c:

Go to the source code of this file.

Functions

void setStatus (SensorFusionGlobals *sfg, fusion_status_t status)
 
void queueStatus (SensorFusionGlobals *sfg, fusion_status_t status)
 
void updateStatus (SensorFusionGlobals *sfg)
 
void testStatus (SensorFusionGlobals *sfg)
 
void initSensorFusionGlobals (SensorFusionGlobals *sfg, StatusSubsystem *pStatusSubsystem, ControlSubsystem *pControlSubsystem)
 utility function to insert default values in the top level structure More...
 
int8_t installSensor (SensorFusionGlobals *sfg, struct PhysicalSensor *pSensor, uint16_t addr, uint16_t schedule, void *bus_driver, registerDeviceInfo_t *busInfo, initializeSensor_t *initialize, readSensor_t *read)
 
int8_t initializeSensors (SensorFusionGlobals *sfg)
 
void processMagData (SensorFusionGlobals *sfg)
 
int8_t readSensors (SensorFusionGlobals *sfg, uint16_t read_loop_counter)
 
void conditionSensorReadings (SensorFusionGlobals *sfg)
 
void zeroArray (StatusSubsystem *pStatus, void *data, uint16_t size, uint16_t numElements, uint8_t check)
 
void clearFIFOs (SensorFusionGlobals *sfg)
 Function to clear FIFO at the end of each fusion computation. More...
 
void runFusion (SensorFusionGlobals *sfg)
 
void initializeFusionEngine (SensorFusionGlobals *sfg)
 
void conditionSample (int16_t sample[3])
 conditionSample ensures that we never encounter the maximum negative two's complement value for a 16-bit variable (-32768). More...
 
void addToFifo (union FifoSensor *sensor, uint16_t maxFifoSize, int16_t sample[3])
 addToFifo is called from within sensor driver read functions More...
 

Detailed Description

The sensor_fusion.c file implements the top level programming interface.

Definition in file sensor_fusion.c.

Function Documentation

◆ addToFifo()

void addToFifo ( union FifoSensor *  sensor,
uint16_t  maxFifoSize,
int16_t  sample[3] 
)

addToFifo is called from within sensor driver read functions

addToFifo is called from within sensor driver read functions to transfer new readings into the sensor structure corresponding to accel, gyro or mag. This function ensures that the software FIFOs are not overrun.

example usage: if (status==SENSOR_ERROR_NONE) addToFifo((FifoSensor*) &(sfg->Mag), MAG_FIFO_SIZE, sample);

Parameters
sensorpointer to structure of type AccelSensor, MagSensor or GyroSensor
maxFifoSizethe size of the software (not hardware) FIFO
samplethe sample to add

Definition at line 522 of file sensor_fusion.c.

References FifoSensor::Accel, CHX, CHY, CHZ, AccelSensor::iFIFOCount, AccelSensor::iFIFOExceeded, and AccelSensor::iGsFIFO.

Referenced by FXLS8471Q_Read(), FXOS8700_Init(), FXOS8700_ReadMagData(), and MAG3110_Read().

Here is the caller graph for this function:

◆ clearFIFOs()

void clearFIFOs ( SensorFusionGlobals *  sfg)

Function to clear FIFO at the end of each fusion computation.

Parameters
sfgGlobal data structure pointer

Definition at line 354 of file sensor_fusion.c.

References MagSensor::iFIFOCount, MagSensor::iFIFOExceeded, and SensorFusionGlobals::Mag.

Referenced by initializeFusionEngine(), initSensorFusionGlobals(), and runFusion().

Here is the caller graph for this function:

◆ conditionSample()

void conditionSample ( int16_t  sample[3])

conditionSample ensures that we never encounter the maximum negative two's complement value for a 16-bit variable (-32768).

conditionSample ensures that we never encounter the maximum negative two's complement value for a 16-bit variable (-32768). This value cannot be negated, because the maximum positive value is +32767. We need the ability to negate to gaurantee that subsequent HAL operations can be run successfully.

Parameters
sample16-bit register value from triaxial sensor read

Definition at line 510 of file sensor_fusion.c.

References CHX, CHY, and CHZ.

Referenced by FXLS8471Q_Read(), FXOS8700_Init(), FXOS8700_ReadMagData(), and MAG3110_Read().

Here is the caller graph for this function:

◆ conditionSensorReadings()

void conditionSensorReadings ( SensorFusionGlobals *  sfg)

conditionSensorReadings() transforms raw software FIFO readings into forms that can be consumed by the sensor fusion engine. This include sample averaging and (in the case of the gyro) integrations, applying hardware abstraction layers, and calibration functions. This function is normally involved via the "sfg." global pointer.

Parameters
sfgGlobal data structure pointer

Definition at line 296 of file sensor_fusion.c.

References MagSensor::isEnabled, SensorFusionGlobals::Mag, and processMagData().

Referenced by initSensorFusionGlobals().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ initializeFusionEngine()

void initializeFusionEngine ( SensorFusionGlobals *  sfg)

◆ initializeSensors()

int8_t initializeSensors ( SensorFusionGlobals *  sfg)

◆ initSensorFusionGlobals()

void initSensorFusionGlobals ( SensorFusionGlobals *  sfg,
StatusSubsystem *  pStatusSubsystem,
ControlSubsystem *  pControlSubsystem 
)

◆ installSensor()

int8_t installSensor ( SensorFusionGlobals *  sfg,
struct PhysicalSensor *  pSensor,
uint16_t  addr,
uint16_t  schedule,
void *  bus_driver,
registerDeviceInfo_t *  busInfo,
initializeSensor_t *  initialize,
readSensor_t *  read 
)

installSensor is used to instantiate a physical sensor driver into the sensor fusion system. This function is normally involved via the "sfg." global pointer.

Parameters
sfgtop level fusion structure
pSensorpointer to structure describing physical sensor
addrI2C address for sensor (if applicable)
scheduleParameter to control sensor sampling rate
bus_driverISSDK sensor bus driver (usually KSDK I2C bus)
busInfoinformation required for bus power management
initializepointer to sensor initialization function
readpointer to sensor read function

Definition at line 105 of file sensor_fusion.c.

References PhysicalSensor::addr, PhysicalSensor::bus_driver, PhysicalSensor::deviceInfo, registerDeviceInfo_t::deviceInstance, registerDeviceInfo_t::functionParam, registerDeviceInfo_t::idleFunction, PhysicalSensor::initialize, PhysicalSensor::next, spiSlaveSpecificParams_t::pReadPreprocessFN, SensorFusionGlobals::pSensors, spiSlaveSpecificParams_t::pTargetSlavePinID, spiSlaveSpecificParams_t::pWritePreprocessFN, PhysicalSensor::read, PhysicalSensor::schedule, PhysicalSensor::slaveParams, spiSlaveSpecificParams_t::spiCmdLen, and spiSlaveSpecificParams_t::ssActiveValue.

Referenced by initSensorFusionGlobals().

Here is the caller graph for this function:

◆ processMagData()

void processMagData ( SensorFusionGlobals *  sfg)

◆ queueStatus()

void queueStatus ( SensorFusionGlobals *  sfg,
fusion_status_t  status 
)

Poor man's inheritance for status subsystem queueStatus command. This function is normally involved via the "sfg." global pointer.

Definition at line 33 of file sensor_fusion.c.

References SensorFusionGlobals::pStatusSubsystem, and StatusSubsystem::queue.

Referenced by initSensorFusionGlobals().

Here is the caller graph for this function:

◆ readSensors()

int8_t readSensors ( SensorFusionGlobals *  sfg,
uint16_t  read_loop_counter 
)

readSensors traverses the linked list of physical sensors, calling the individual read functions one by one. This function is normally involved via the "sfg." global pointer.

Parameters
sfgpointer to global sensor fusion data structure
read_loop_countercurrent loop counter (used for multirate processing)

Definition at line 267 of file sensor_fusion.c.

References HARD_FAULT, PhysicalSensor::isInitialized, PhysicalSensor::next, SensorFusionGlobals::pSensors, PhysicalSensor::read, PhysicalSensor::schedule, SENSOR_ERROR_INIT, SensorFusionGlobals::setStatus, and status.

Referenced by initSensorFusionGlobals().

Here is the caller graph for this function:

◆ runFusion()

void runFusion ( SensorFusionGlobals *  sfg)

runFusion the top level call that actually runs the sensor fusion. This is a utility function which manages the various defines in build.h. You should feel free to drop down a level and implement only those portions of fFuseSensors() that your application needs. This function is normally involved via the "sfg." global pointer.

Definition at line 377 of file sensor_fusion.c.

References clearFIFOs(), fFuseSensors(), SensorFusionGlobals::Mag, and SensorFusionGlobals::MagCal.

Referenced by initSensorFusionGlobals().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ setStatus()

void setStatus ( SensorFusionGlobals *  sfg,
fusion_status_t  status 
)

Poor man's inheritance for status subsystem setStatus command This function is normally involved via the "sfg." global pointer.

Definition at line 26 of file sensor_fusion.c.

References SensorFusionGlobals::pStatusSubsystem, and StatusSubsystem::set.

Referenced by initSensorFusionGlobals().

Here is the caller graph for this function:

◆ testStatus()

void testStatus ( SensorFusionGlobals *  sfg)

Definition at line 45 of file sensor_fusion.c.

References SensorFusionGlobals::pStatusSubsystem, and StatusSubsystem::test.

Referenced by initSensorFusionGlobals().

Here is the caller graph for this function:

◆ updateStatus()

void updateStatus ( SensorFusionGlobals *  sfg)

Poor man's inheritance for status subsystem updateStatus command. This function is normally involved via the "sfg." global pointer.

Definition at line 40 of file sensor_fusion.c.

References SensorFusionGlobals::pStatusSubsystem, and StatusSubsystem::update.

Referenced by initSensorFusionGlobals().

Here is the caller graph for this function:

◆ zeroArray()

void zeroArray ( StatusSubsystem *  pStatus,
void *  data,
uint16_t  size,
uint16_t  numElements,
uint8_t  check 
)
Parameters
pStatusStatus subsystem pointer
datapointer to array to be zeroed
sizedata type size = 8, 16 or 32
numElementsnumber of elements to zero out
checktrue if you would like to verify writes, false otherwise

Definition at line 311 of file sensor_fusion.c.

References data, HARD_FAULT, and StatusSubsystem::set.