![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The pedometer_stepcount_mma8451.c file implements the ISSDK prdometer example using MMA8451 sensor as the acceleration source. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "pedometer.h"#include "mma845x_drv.h"
Go to the source code of this file.
Macros | |
| #define | RAW_ACCEL_DATA_SIZE (6) |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | mma845x_Config_Normal [] |
| const registerreadlist_t | mma845x_Data_Ready [] = {{.readFrom = MMA845x_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| const registerreadlist_t | mma845x_Output_Values [] |
The pedometer_stepcount_mma8451.c file implements the ISSDK prdometer example using MMA8451 sensor as the acceleration source.
Definition in file pedometer_stepcount_mma8451.c.
| #define RAW_ACCEL_DATA_SIZE (6) |
Definition at line 32 of file pedometer_stepcount_mma8451.c.
| int main | ( | void | ) |
Main function.
Initialize the MCU hardware
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the MMA845x sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the MMA845x sensor driver with Non FIFO mode.
Initialize the pedometer
Configure the pedometer
Read the data ready status from MMA845x
Read the raw sensor data from the MMA845x.
Convert the raw sensor data for display to the debug port.
Execute the pedometer Algorithm
Definition at line 85 of file pedometer_stepcount_mma8451.c.
References mma845x_acceldata_t::accel, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), MMA8451_WHO_AM_I_WHOAMI_VALUE, MMA845x_ACCEL_DATA_SIZE, MMA845x_I2C_ADDR, MMA845x_I2C_Configure(), MMA845x_I2C_Initialize(), MMA845x_I2C_ReadData(), MMA845x_I2C_SetIdleTask(), MMA845x_STATUS_ZYXDR_MASK, pedometer_configure(), pedometer_init(), pedometer_run(), rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), pedometer_t::status, status, and pedometer_t::pedometer_status_tag::stepcount.

| const registerwritelist_t mma845x_Config_Normal[] |
Prepare the register write list to configure MMA845x in poll mode.
Definition at line 39 of file pedometer_stepcount_mma8451.c.
| const registerreadlist_t mma845x_Data_Ready[] = {{.readFrom = MMA845x_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Prepare the register read list to read the Data Ready Status from MMA845x.
Definition at line 49 of file pedometer_stepcount_mma8451.c.
| const registerreadlist_t mma845x_Output_Values[] |
Prepare the register read list to read the raw Accel data from MMA845x.
Definition at line 52 of file pedometer_stepcount_mma8451.c.