44 #include "clock_config.h" 45 #include "fsl_debug_console.h" 48 #include "Driver_I2C.h" 51 #include "issdk_hal.h" 91 PRINTF(
"\r\n ISSDK FXAS21002 sensor driver example demonstration with poll mode\r\n");
95 if (ARM_DRIVER_OK != status)
97 PRINTF(
"\r\n I2C Initialization Failed\r\n");
102 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
103 if (ARM_DRIVER_OK != status)
105 PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
110 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
111 if (ARM_DRIVER_OK != status)
113 PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
122 PRINTF(
"\r\n Sensor Initialization Failed\r\n");
125 PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
134 PRINTF(
"\r\n FXAS21002 Sensor Configuration Failed, Err = %d\r\n", status);
137 PRINTF(
"\r\n Successfully Applied FXAS21002 Sensor Configuration\r\n");
150 if (ARM_DRIVER_OK != status)
152 PRINTF(
"\r\n Read Failed. \r\n");
157 rawData.
gyro[0] = ((int16_t)data[0] << 8) | data[1];
158 rawData.
gyro[1] = ((int16_t)data[2] << 8) | data[3];
159 rawData.
gyro[2] = ((int16_t)data[4] << 8) | data[5];
162 PRINTF(
"\r\n Gyro X = %d Y = %d Z = %d\r\n", rawData.
gyro[0], rawData.
gyro[1], rawData.
gyro[2]);
#define __END_WRITE_DATA__
const registerreadlist_t fxas21002_Output_Values[]
const registerwritelist_t fxas21002_Config_Normal[]
#define BOARD_BootClockRUN
#define FXAS21002_CTRL_REG1_DR_MASK
uint8_t data[FXLS8962_DATA_SIZE]
void BOARD_InitDebugConsole(void)
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
The fxas21002_drv.h file describes the fxas21002 driver interface and structures. ...
int main(void)
Main function.
#define __END_READ_DATA__
#define FXAS21002_DR_STATUS_ZYXDR_MASK
This structure defines the fxas21002 raw data buffer.
This defines the sensor specific information for I2C.
#define ASK_USER_TO_RESUME(x)
int32_t FXAS21002_I2C_ReadData(fxas21002_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
#define I2C_S_DEVICE_INDEX
#define FXAS21002_WHO_AM_I_WHOAMI_PROD_VALUE
#define FXAS21002_I2C_ADDR
int32_t FXAS21002_I2C_Configure(fxas21002_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
const registerreadlist_t fxas21002_DRDY[]
void FXAS21002_I2C_SetIdleTask(fxas21002_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
fxls8962_acceldataUser_t rawData
This structure defines the Write command List.
This structure defines the Read command List.
#define FXAS21002_GYRO_DATA_SIZE
The size of the FXAS21002 gyro data.
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define FXAS21002_CTRL_REG1_DR_12_5HZ
#define I2C_S_SIGNAL_EVENT
int32_t FXAS21002_I2C_Initialize(fxas21002_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.